Texas Instruments Technology for Innovators(tm)

SysLink 2.00.04.83 Release Notes

October 2011

This SysLink Release is targeted to SYS/BIOS 6-based platforms.

Introduction, Documentation, What's New, Upgrade Info, Compatibility Information, Device Support, Validation Info, Known Issues, Examples, Version Information, Technical Support.


Introduction

SysLink is runtime software that simplifies the development of embedded applications in which either General-Purpose microprocessors (GPP) or DSPs communicate with each other. The SysLink product provides software connectivity between multiple processors. Each processor may run either an HLOS (e.g. Linux) or an RTOS (e.g. SYS/BIOS). In addition, a processor may also be designated as the master for another slave processor, and may be responsible for controlling the slave processor's execution (including boot-loading the slave).

The SysLink product provides the following services to frameworks and applications:

SYS/BIOS operating system is expected to be running on the slaves with all of these platforms.


Documentation

The following documentation is available:

In addition, users are encouraged to monitor (and contribute to!) the TI Embedded Processors Wiki.

Release notes from previous releases are also available in the relnotes_archive directory.


What's New

The following significant changes have been made since 2.00

2.00.04.83
2.00.03.82
2.00.02.80
2.00.01.79
2.00.00.78


Upgrade Information

This SysLink release is not suitable for BIOS 5-based DVSDKs. DVSDK users should continue to use the BIOS 5-based DSP Link 1.x releases.

The SysLink packages are available in the "packages/" subdirectory of the product. If you have a previous release of the SysLink product, you can install this release next to it, and modify your build scripts/makefiles to use this newer release.

Compatibility Breaks!

Note, if you're upgrading from a release earlier than SysLink 2.00, be sure to review the Upgrade section for each of the releases between your current release and this one.


Device Support

This release supports the following devices:


Validation

This release was built and validated against using the following software components:

This release was validated using the following hardware platforms:


Known Issues

Consult the SDOWP database for open issues.


Version Information

This product's version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and b is an unrestricted set of digits used as an incrementing build counter.

To support multiple side-by-side installations of the product, the product version is encoded in the top level directory, ex. syslink_2_00_04_83.

Subsequent releases of patch upgrades will be identified by the patch number, ex. SysLink 2.00.01.XX with directory syslink_2_00_01_XX. Typically, these patches only include critical bug fixes.


Technical Support

For technical support, contact softwaresupport@ti.com

Check the following web site for updates: https://software-dl.ti.com/dsps/dsps_public_sw/sdo_sb/targetcontent/syslink/index.html


Last updated: October 27, 2011