module ti.sysbios.family.arm.f2838x.init.Boot |
 |
TMS320F2838X device Boot Support
The Boot module supports boot initialization for the CM core.
Two special Boot init functions are created based on the configuration
settings for this module. One function is an xdc.runtime.Reset
function (called early at boot prior to cinit processing), and the second
function is an xdc.runtime.Startup first function (called before main()).
[
more ... ]
#include <ti/sysbios/family/arm/f2838x/init/Boot.h>
Functions common to all target modules |
|
|
DETAILS
The Boot module supports boot initialization for the CM core.
Two special Boot init functions are created based on the configuration
settings for this module. One function is an xdc.runtime.Reset
function (called early at boot prior to cinit processing), and the second
function is an xdc.runtime.Startup first function (called before main()).
The code to support the boot module is placed in a separate section
named
".text:.bootCodeSection" to allow placement of this section in
the linker .cmd file if necessary. This section is a subsection of the
".text" section so this code will be placed into the .text section unless
explicitly placed, either through
Program.sectMap or through a linker
command file.
Module-Wide Built-Ins |
 |
// Get this module's unique id
Bool Boot_Module_startupDone();
// Test if this module has completed startup
// The heap from which this module allocates memory
Bool Boot_Module_hasMask();
// Test whether this module has a diagnostics mask
Bits16 Boot_Module_getMask();
// Returns the diagnostics mask for this module
Void Boot_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
var Boot = xdc.useModule('ti.sysbios.family.arm.f2838x.init.Boot');
module-wide constants & types
module-wide config parameters
metaonly struct Boot.ModuleView |
 |
var obj = new Boot.ModuleView;
obj.disableWatchdog = Bool ...
obj.configureFlashController = Bool ...
obj.configureFlashWaitStates = Bool ...
obj.enableFlashProgramCache = Bool ...
obj.enableFlashDataCache = Bool ...
obj.pllSourcedINTOSC = Bool ...
obj.bootFromFlash = Bool ...
metaonly config Boot.bootFromFlash // module-wide |
 |
Boot from Flash flag. Default is true
Boot.bootFromFlash = Bool true;
DETAILS
Set to true to enable booting CM from Flash.
metaonly config Boot.common$ // module-wide |
 |
Common module configuration parameters
DETAILS
All modules have this configuration parameter. Its name
contains the '$' character to ensure it does not conflict with
configuration parameters declared by the module. This allows
new configuration parameters to be added in the future without
any chance of breaking existing modules.
metaonly config Boot.configureFlashController // module-wide |
 |
Flash controller configuration flag, default is true
Boot.configureFlashController = Bool true;
DETAILS
Set to true to enable the configuration of the Flash controller
wait states, program and data cache.
metaonly config Boot.configureFlashWaitStates // module-wide |
 |
Flash controller wait states configuration flag, default is true
Boot.configureFlashWaitStates = Bool true;
DETAILS
Set to true to configure the Flash controller wait states. The number
of wait states is computed based upon the CPU frequency.
metaonly config Boot.disableWatchdog // module-wide |
 |
Watchdog disable configuration flag, default is false
Boot.disableWatchdog = Bool false;
DETAILS
Set to true to disable the watchdog.
metaonly config Boot.enableFlashDataCache // module-wide |
 |
Flash controller data cache enable flag, default is true
Boot.enableFlashDataCache = Bool true;
DETAILS
Set to true to enable the Flash controller's data cache.
metaonly config Boot.enableFlashProgramCache // module-wide |
 |
Flash controller program cache enable flag, default is true
Boot.enableFlashProgramCache = Bool true;
DETAILS
Set to true to enable the Flash controller's program cache.
metaonly config Boot.loadSegment // module-wide |
 |
Specifies where to load the Flash controller configuration function
Boot.loadSegment = String undefined;
DETAILS
If 'configureFlashController' is true, then this parameter
determines where the ".ti_sysbios_family_arm_f2838x_init_flashfuncs"
section gets loaded.
metaonly config Boot.pllSourcedINTOSC // module-wide |
 |
Internal OSCCLK configuration flag, default is true
Boot.pllSourcedINTOSC = Bool true;
DETAILS
Set to true to indicate PLLSYSCLK is derived from either INTOSC1 or
or INTOSC2, set to false if PLLSYSCLK is derived from an external
crystal (XTAL).
metaonly config Boot.rovViewInfo // module-wide |
 |
metaonly config Boot.runSegment // module-wide |
 |
Specifies where to run the Flash controller configuration function
Boot.runSegment = String undefined;
DETAILS
If 'configureFlashController' is true then this parameter
determines where the ".ti_sysbios_family_arm_f2838x_init_flashfuncs"
section gets executed at runtime.
generated on Thu, 23 May 2019 00:22:55 GMT