module ti.sysbios.family.arm.a15.TimestampProvider

A15 TimestampProvider

The source of the timestamps for the A15 TimestampProvider is the A15's internal PMC counter which counts CPU cycles. [ more ... ]
C synopsis target-domain sourced in ti/sysbios/family/arm/a15/TimestampProvider.xdc
DETAILS
The source of the timestamps for the A15 TimestampProvider is the A15's internal PMC counter which counts CPU cycles.
As this counter is only 32 bits in length, provision is made in the get64() API to test if an overflow has occurred since the last invocation of get64() and compensate the return value accordingly.
As it is possible for the 32 bit counter to roll over more than once between successive get64() calls, this module offers an auto refresh feature. If auto refresh is enabled (see autoRefreshEnable), this module will register a clock function with a period less than the amount of time it takes for the 32 bit counter to roll over. The clock function checks for an overflow and updates the upper 32 bits of the counter to guarantee coherency in successive timestamps.
NOTE
Auto refresh feature requires that the SYS/BIOS clock is enabled. If the SYS/BIOS clock is disabled (see BIOS.clockEnabled) then this feature cannot be enabled.

Calling Context

Function Hwi Swi Task Main Startup
get32 Y Y Y Y N
get64 Y Y Y Y N
getFreq Y Y Y Y N
Definitions:
  • Hwi: API is callable from a Hwi thread.
  • Swi: API is callable from a Swi thread.
  • Task: API is callable from a Task thread.
  • Main: API is callable during any of these phases:
    • In your module startup after this module is started (e.g. TimestampProvider_Module_startupDone() returns TRUE).
    • During xdc.runtime.Startup.lastFxns.
    • During main().
    • During BIOS.startupFxns.
  • Startup: API is callable during any of these phases:
    • During xdc.runtime.Startup.firstFxns.
    • In your module startup before this module is started (e.g. TimestampProvider_Module_startupDone() returns FALSE).
 
TimestampProvider_get32()  // module-wide

Return a 32-bit timestamp

C synopsis target-domain
Bits32 TimestampProvider_get32();
 
RETURNS
Returns a 32-bit timestamp value. Use getFreq to convert this value into units of real time.
Returns a 32-bit timestamp value. Use getFreq to convert this value into units of real time.
SEE
 
TimestampProvider_get64()  // module-wide

Return a 64-bit timestamp

C synopsis target-domain
Void TimestampProvider_get64(Types_Timestamp64 *result);
 
ARGUMENTS
result — pointer to 64-bit result
This parameter is a pointer to a structure representing a 64-bit wide timestamp value where the current timestamp is written.
If the underlying hardware does not support 64-bit resolution, the hi field of result is always set to 0; see xdc.runtime.Types.Timestamp64. So, it is possible for the lo field to wrap around without any change to the hi field. Use getFreq to convert this value into units of real time.
pointer to 64-bit result
This parameter is a pointer to a structure representing a 64-bit wide timestamp value where the current timestamp is written.
If the underlying hardware does not support 64-bit resolution, the hi field of result is always set to 0; see xdc.runtime.Types.Timestamp64. So, it is possible for the lo field to wrap around without any change to the hi field. Use getFreq to convert this value into units of real time.
SEE
 
TimestampProvider_getFreq()  // module-wide

Get the timestamp timer's frequency (in Hz)

C synopsis target-domain
Void TimestampProvider_getFreq(Types_FreqHz *freq);
 
ARGUMENTS
freq — pointer to a 64-bit result
This parameter is a pointer to a structure representing a 64-bit wide frequency value where the timer's frequency (in Hz) is written; see xdc.runtime.Types.FreqHz. This function provides a way of converting timestamp values into units of real time.
pointer to a 64-bit result
This parameter is a pointer to a structure representing a 64-bit wide frequency value where the timer's frequency (in Hz) is written; see xdc.runtime.Types.FreqHz. This function provides a way of converting timestamp values into units of real time.
SEE
Module-Wide Built-Ins

C synopsis target-domain
Types_ModuleId TimestampProvider_Module_id();
// Get this module's unique id
 
Bool TimestampProvider_Module_startupDone();
// Test if this module has completed startup
 
IHeap_Handle TimestampProvider_Module_heap();
// The heap from which this module allocates memory
 
Bool TimestampProvider_Module_hasMask();
// Test whether this module has a diagnostics mask
 
Bits16 TimestampProvider_Module_getMask();
// Returns the diagnostics mask for this module
 
Void TimestampProvider_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
 
Configuration settings sourced in ti/sysbios/family/arm/a15/TimestampProvider.xdc
 
metaonly config TimestampProvider.autoRefreshEnable  // module-wide

If this config param is set to true, this module will create a clock instance with a timeout that is less than the amount of time it takes for the PMU cycle counter to overflow. The clock handler function will check if the PMU cycle counter has overflowed and update the upper 32 bits of the timestamp so coherency of successive 64bit timestamps is guaranteed

Configuration settings
TimestampProvider.autoRefreshEnable = Bool true;
 
 
metaonly config TimestampProvider.common$  // module-wide

Common module configuration parameters

Configuration settings
TimestampProvider.common$ = Types.Common$ undefined;
 
DETAILS
All modules have this configuration parameter. Its name contains the '$' character to ensure it does not conflict with configuration parameters declared by the module. This allows new configuration parameters to be added in the future without any chance of breaking existing modules.
generated on Sat, 21 Dec 2013 00:08:55 GMT