The Swi module manages software interrupt service routines, which are
patterned after hardware interrupt service routines.
SYS/BIOS manages four distinct levels of execution threads: hardware
interrupt service routines, software interrupt routines, tasks, and
background idle functions. A software interrupt is an object that
encapsulates a function to be executed and a priority.
Software interrupts are prioritized, preempt tasks, and are preempted
by hardware interrupt service routines.
Each software interrupt has a priority level. A software interrupt
preempts any lower-priority software interrupt currently executing.
A target program uses an API call to post a Swi object. This causes the
Swi module to schedule execution of the software interrupt's function.
When a Swi is posted by an API call, the Swi object's function is not
executed immediately. Instead, the function is scheduled for execution.
SYS/BIOS uses the Swi's priority to determine whether to preempt the
thread currently running. Note that if a Swi is posted several times
before it begins running, (because Hwis and higher priority interrupts
are running,) when the Swi does eventually run, it will run only one time.
A Swi preempts any currently running Swi with a lower priority.
When multiple Swis of the same priority level have been posted,
their respective Swi functions are executed in the order the Swis
were posted.
Hwis in turn preempt any currently running Swi,
allowing the target to respond quickly to hardware peripherals.
Swi threads are executed using the ISR (or "Hwi") stack. Thus
they share the ISR stack with Hwi threads.
Sets of hook functions can be specified for the Swi module. Each set
contains these hook functions:
Hook functions can only be configured statically.
If you define more than one set of hook functions, all the functions
of a particular type will be run when a Swi triggers that type of
hook.
The create and delete functions are called whenever a Swi is created
or deleted. They are called with interrupts enabled (unless called
at boot time or from main()).
The ready, begin and end functions are all called with interrupts
enabled. The ready function is called when a Swi is posted and made
ready to run. The begin function is called right before the function
associated with the given Swi is run. The end function is called
right after this function returns.
typedef Swi_FuncPtr |
|
Swi function type definition
typedef Void (*Swi_FuncPtr)(UArg,UArg);
DETAILS
All Swi functions are passed two uninterpreted arguments of type
UArg and have no return value.
struct Swi_HookSet |
|
Swi hook set type definition
typedef struct Swi_HookSet {
Void (*registerFxn)(Int);
} Swi_HookSet;
DETAILS
This structure defines the set of hook functions that can be
specified for the Swi module.
See
Hook Functions for details.
config Swi_A_badPriority // module-wide |
|
Assertion raised if a Swi's priority is out of range
DETAILS
Swi priorities must be in the range of 0 and numPriorities-1.
config Swi_A_swiDisabled // module-wide |
|
Assertion raised if Swi_create is called and runtime Swi creation is
disabled
DETAILS
config Swi_LD_end // module-wide |
|
The event logged just after returning from a Swi's function
config Swi_LM_begin // module-wide |
|
The event logged just prior to invoking a Swi's function
config Swi_LM_post // module-wide |
|
The event logged when Swi_post() is called
config Swi_numPriorities // module-wide |
|
Number of Swi priorities supported
extern const UInt Swi_numPriorities;
DETAILS
The maximum number of priorities supported is
target-specific and depends on the number of
bits in a UInt data type. For 6x and ARM devices
the maximum number of priorities is therefore 32.
For 28x, 55x, and MSP430 devices, the maximum number of
priorities is 16.
Swi_disable() // module-wide |
|
Disable Swi Scheduling
RETURNS
opaque key for use with Swi_restore()
DETAILS
Swi_disable() and
Swi_restore() control Swi
scheduling.
Swi_disable() disables all Swi functions from running until
Swi_restore() is called. Hardware interrupts can still run.
Swi_disable() and Swi_restore() allow you to ensure that
statements that must be performed together during critical
processing are not preempted by other Swis or Tasks.
The value of the key returned by Swi_disable() is opaque to
applications and is meant to be passed to Swi_restore().
In the following example, the critical section cannot be preempted
by any Swis. Nor can it be pre-empted by other Tasks.
key = Swi_disable();
`critical section`
Swi_restore(key);
SIDE EFFECTS OF DISABLING THE SWI SCHEDULER
Swi_disable(), in addition to disabling Swis from
pre-empting the code which follows its invocation, has
the side effect of also disabling the Task scheduler.
Consequently, Task pre-emption and blocking is also disabled while
the Swi scheduler is disabled.
When
Swi_restore() is subsequently called, it will
re-enable and invoke the Task scheduler if the Task scheduler was not
already disabled prior to invoking Swi_disable().
The following code snippet:
key = Swi_disable();
...
Swi_post(swi); <-- 'swi' will not run
...
Swi_restore(key); <-- 'swi' runs now
Should be thought of as equivalent to this:
tasKey = Task_disable();
swiKey = Swi_disable();
...
Swi_post(swi); <-- 'swi' will not run
...
Swi_restore(swiKey); <-- 'swi' runs now
Task_restore(taskKey);
In the following example, even though the Semaphore_post() call
unblocks a task of higher priority, the local task is not pre-empted
until after the Swi_restore() call is made:
key = Swi_disable();
...
Swi_post(swi); <-- 'swi' will not run
Semaphore_post(sem); <-- readys a task of higher priority than current task
...
Swi_restore(key); <-- 'swi' runs now, then current task is pre-empted.
A common mistake that users make is to invoke a blocking
API such as Semaphore_pend() after calling Swi_disable().
This results in unrecoverable damage to the Task scheduler's internal
state and will lead to unpredictable and usually catastrophic behavior:
key = Swi_disable();
...
Semaphore_pend(sem, BIOS_WAIT_FOREVER); <-- !!! DO NOT DO THIS !!!
...
Swi_restore(key); <-- !!! System failure guaranteed to follow !!!
A more subtle variant of the above problem occurs when an API such
as GateMutex_enter() is invoked directly or indirectly while the
Swi scheduler
is disabled. If the GateMutex has already been entered by another thread,
the current thread should block until the other thread calls
GateMutex_leave().
But because the Task scheduler is disabled, the local thread returns
immediately from GateMutex_enter(), just as though it successfully
entered the GateMutex! This usually leads to catastrophic results.
Swi_getTrigger() // module-wide |
|
Return the trigger value of the currently executing Swi
RETURNS
trigger value
DETAILS
Swi_getTrigger returns the value that Swi's trigger had when the Swi
started running. SYS/BIOS saves the trigger value internally, so that
Swi_getTrigger can access it at any point within a Swi object's
function, and then automatically resets the trigger to its initial
value.
Swi_getTrigger should only be called within a function run by a Swi
object.
When called from within the context of a Swi, the value returned by
Swi_getTrigger is zero if the Swi was posted by a call to Swi_andn,
or Swi_dec. Therefore, Swi_getTrigger provides relevant information
only if the Swi was posted by a call to Swi_inc, Swi_or, Swi_orHook,
or Swi_post.
This API is called within a Swi object's function to use the trigger
value that caused the function to run. For example, if you use
Swi_or or Swi_inc to post a Swi, different trigger values can require
different processing.
swicount = Swi_getTrigger();
Swi_restore() // module-wide |
|
Restore Swi Scheduling state
Void Swi_restore(UInt key);
ARGUMENTS
key
key to restore previous Swi scheduler state
DETAILS
Swi_restore restores the Swi scheduler to the locked/unlocked state
it was in when Swi_disable was called. If the scheduler becomes
unlocked and Swis of sufficient priority have been made ready to
run by any of the posting APIs, then they are run at this time.
Swi_disable and Swi_restore control software interrupt processing.
Swi_disable disables all other Swi functions from running until
Swi_restore is called. Hardware interrupts can still run.
Swi_disable and Swi_restore allow you to ensure that statements that
must be performed together during critical processing are not
pre-empted by other Swis.
In the following example, the critical section cannot be preempted
by any Swis. Nor can it be pre-empted by other Tasks.
key = Swi_disable();
`critical section`
Swi_restore(key);
Read the discussion of the side effects of disabling the Swi
scheduler
here.
CONSTRAINTS
Swi_restore will also re-enable and invoke the Task
scheduler if the Task scheduler was not disabled prior to
invoking Swi_disable().
The
post discussion regarding global interrupts applies
to this API.
Swi_self() // module-wide |
|
Return address of currently executing Swi object
RETURNS
handle of currently running Swi
DETAILS
Swi_self returns the handle of the currently executing Swi.
For example, you can call Swi_self as follows if you want
a Swi to repost itself:
Module-Wide Built-Ins |
|
// Get this module's unique id
Bool Swi_Module_startupDone();
// Test if this module has completed startup
// The heap from which this module allocates memory
Bool Swi_Module_hasMask();
// Test whether this module has a diagnostics mask
Bits16 Swi_Module_getMask();
// Returns the diagnostics mask for this module
Void Swi_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
Instance Object Types |
|
typedef struct Swi_Object Swi_Object;
// Opaque internal representation of an instance object
// Client reference to an instance object
typedef struct Swi_Struct Swi_Struct;
// Opaque client structure large enough to hold an instance object
// Convert this instance structure pointer into an instance handle
// Convert this instance handle into an instance structure pointer
Instance Config Parameters |
|
typedef struct Swi_Params {
// Instance config-params structure
// Common per-instance configs
UArg arg0;
// Swi function argument 0
UArg arg1;
// Swi function argument 1
UInt priority;
// Swi priority
UInt trigger;
// Initial Swi trigger value
} Swi_Params;
// Initialize this config-params structure with supplier-specified defaults before instance creation
config Swi_arg0 // instance |
|
Swi function argument 0
DETAILS
The default value of this optional parameter is 0.
SEE
config Swi_arg1 // instance |
|
Swi function argument 1
DETAILS
The default value of this optional parameter is 0.
SEE
config Swi_priority // instance |
|
Swi priority
DETAILS
Each software interrupt has a priority level, 0 to
(
numPriorities - 1). A software interrupt
preempts any lower-priority software interrupt currently executing.
When multiple Swis of the same priority level have been posted,
their respective Swi functions are executed in the order the Swis
were posted.
The default value of this optional parameter is ~0, which yields a
Swi with the highest priority: (
numPriorities - 1).
config Swi_trigger // instance |
|
Initial Swi trigger value
DETAILS
The default value of this optional parameter is 0.
Each Swi object has a "trigger" used either to determine whether to
post the Swi or as a value that can be evaluated within the Swi's
function.
The
andn and
dec functions post the Swi
if the trigger value transitions to 0. The
or and
inc functions also modify the trigger value. (
or
sets bits, and
andn clears bits.)
Instance Creation |
|
// Allocate and initialize a new instance object and return its handle
// Initialize a new instance object inside the provided structure
ARGUMENTS
swiFxn
Swi Function
params
per-instance config params, or NULL to select default values (target-domain only)
eb
active error-handling block, or NULL to select default policy (target-domain only)
DETAILS
Swi_create creates a new Swi object.
The following C code sets Swi parameters and
creates two Swi objects:
Void main()
{
Swi_Params swiParams;
Swi_Params_init(&swiParams);
swiParams.arg0 = 1;
swiParams.arg1 = 0;
swiParams.priority = 2;
swiParams.trigger = 0;
swi0 = Swi_create(swi0Fxn, &swiParams, NULL);
swiParams.arg0 = 2;
swiParams.arg1 = 0;
swiParams.priority = 1;
swiParams.trigger = 3;
swi1 = Swi_create(swi1Fxn, &swiParams, NULL);
BIOS_start();
}
The following XDCscript statements set Swi parameters and
create two Swi objects:
var Swi = xdc.useModule('ti.sysbios.knl.Swi');
var swiParams = new Swi.Params();
swiParams.arg0 = 1;
swiParams.arg1 = 0;
swiParams.priority = 2;
swiParams.trigger = 0;
Program.global.swi0 = Swi.create('&swi0Fxn', swiParams);
swiParams.arg0 = 2;
swiParams.priority = 1;
swiParams.trigger = 3;
Program.global.swi1 = Swi.create('&swi1Fxn', swiParams);
Instance Deletion |
|
// Finalize and free this previously allocated instance object, setting the referenced handle to NULL
// Finalize the instance object inside the provided structure
Swi_andn() // instance |
|
Clear bits in Swi's trigger; post if trigger becomes 0
ARGUMENTS
handle
handle of a previously-created Swi instance object
mask
inverse value to be ANDed
DETAILS
Swi_andn is used to conditionally post a software interrupt.
Swi_andn clears the bits specified by a mask from Swi's internal
trigger. If the Swi's trigger becomes 0, Swi_andn posts the Swi.
The bitwise logical operation performed is:
trigger = trigger AND (NOT MASK)
If multiple conditions that all be met before a
Swi can run, you should use a different bit in the trigger for
each condition. When a condition is met, clear the bit for that
condition.
For example, if two events must happen before a Swi is to be
triggered, the initial trigger value of the Swi can be 3 (binary 0011).
One call to Swi_andn can have a mask value of 2 (binary 0010), and
another call to Swi_andn can have a mask value of 1 (binary 0001).
After both calls have been made, the trigger value will be 0.
Swi_andn(swi0, 2); // clear bit 1
Swi_andn(swi0, 1); // clear bit 0
Swi_andn results in a context switch if the Swi's trigger becomes
zero and the Swi has higher priority than the currently executing
thread.
You specify a Swi's initial trigger value at Swi creation time.
The trigger value is automatically reset when the Swi executes.
CONSTRAINTS
The
post discussion regarding global interrupts applies
to this API.
Swi_dec() // instance |
|
Decrement Swi's trigger value; post if trigger becomes 0
ARGUMENTS
handle
handle of a previously-created Swi instance object
DETAILS
Swi_dec is used to conditionally post a software interrupt. Swi_dec
decrements the value in Swi's trigger by 1. If Swi's trigger value
becomes 0, Swi_dec posts the Swi. You can increment a trigger value
by using Swi_inc, which always posts the Swi.
For example, you would use Swi_dec if you wanted to post a Swi after
a number of occurrences of an event.
// swi0's trigger is configured to start at 3
Swi_dec(swi0); // trigger = 2
Swi_dec(swi0); // trigger = 1
Swi_dec(swi0); // trigger = 0
You specify a Swi's initial trigger value at Swi creation time. The
trigger value is automatically reset when the Swi executes.
Swi_dec results in a context switch if the Swi's trigger becomes
zero and the Swi has higher priority than the currently executing
thread.
CONSTRAINTS
The
post discussion regarding global interrupts applies
to this API.
Swi_getAttrs() // instance |
|
Retrieve attributes of an existing Swi object
ARGUMENTS
handle
handle of a previously-created Swi instance object
swiFxn
pointer to a Swi_FuncPtr
params
pointer for returning Swi's Params
DETAILS
The 'handle' argument specifies the address of the Swi object whose
attributes are to be retrieved.
The 'swiFxn' argument is the address of a function pointer where the
the Swi function address is to be written to. If NULL is passed for
'swiFxn', no attempt is made to return the Swi function.
The 'params' argument is a pointer to a Swi_Params structure that will
contain the retrieved Swi attributes.
RELATED
Swi_getFunc() // instance |
|
Get Swi function and arguments
ARGUMENTS
handle
handle of a previously-created Swi instance object
arg0
pointer for returning Swi's first function argument
arg1
pointer for returning Swi's second function argument
RETURNS
Swi function
DETAILS
If either arg0 or arg1 is NULL, then the corresponding argument is not
returned.
RELATED
Swi_getHookContext() // instance |
|
Get hook instance's context pointer for a Swi
Ptr Swi_getHookContext(
Swi_Handle handle,
Int id);
ARGUMENTS
handle
handle of a previously-created Swi instance object
RETURNS
hook instance's context pointer for Swi
DETAILS
For example, this C code gets the HookContext, prints it,
and sets a new value for the HookContext.
Ptr pEnv;
Swi_Handle mySwi;
Int myHookSetId1;
pEnv = Swi_getHookContext(swi, myHookSetId1);
System_printf("myEnd1: pEnv = 0x%lx, time = %ld\n",
(ULong)pEnv, (ULong)Timestamp_get32());
Swi_setHookContext(swi, myHookSetId1, (Ptr)0xc0de1);
See
Hook Functions for more details.
Swi_getPri() // instance |
|
Return a Swi's priority
ARGUMENTS
handle
handle of a previously-created Swi instance object
RETURNS
Priority of Swi
DETAILS
Swi_getPri returns the priority of the Swi passed in as the
argument.
Swi_inc() // instance |
|
Increment Swi's trigger value and post the Swi
ARGUMENTS
handle
handle of a previously-created Swi instance object
DETAILS
Swi_inc increments the value in Swi's trigger by 1 and posts the Swi
regardless of the resulting trigger value. You can decrement a
trigger value using Swi_dec, which only posts the Swi if the
trigger value is 0.
If a Swi is posted several times before it has a chance to begin
executing (i.e. when Hwis or higher priority Swis are running) the Swi
only runs one time. If this situation occurs, you can use Swi_inc to
post the Swi. Within the Swi's function, you could then use
Swi_getTrigger to find out how many times this Swi has been posted
since the last time it was executed.
You specify a Swi's initial trigger value at Swi creation time.
The trigger value is automatically reset when the Swi executes.
To get the trigger value, use Swi_getTrigger.
Swi_inc results in a context switch if the Swi is higher priority
than the currently executing thread.
CONSTRAINTS
The
post discussion regarding global interrupts applies
to this API.
Swi_or() // instance |
|
Or mask with value contained in Swi's trigger and post the
Swi
ARGUMENTS
handle
handle of a previously-created Swi instance object
mask
value to be ORed
DETAILS
Swi_or is used to post a software interrupt. Swi_or sets the bits
specified by a mask in Swi's trigger. Swi_or posts the Swi
regardless of the resulting trigger value. The bitwise logical
operation performed on the trigger value is:
trigger = trigger OR mask
You specify a Swi's initial trigger value at Swi creation time.
The trigger value is automatically reset when the Swi executes.
To get the trigger value, use Swi_getTrigger.
For example, you might use Swi_or to post a Swi if any of three
events should cause a Swi to be executed, but you want the Swi's
function to be able to tell which event occurred. Each event
would correspond to a different bit in the trigger.
Swi_or results in a context switch if the Swi is higher priority
than the currently executing thread.
CONSTRAINTS
The
post discussion regarding global interrupts applies
to this API.
Swi_post() // instance |
|
Unconditionally post a software interrupt
ARGUMENTS
handle
handle of a previously-created Swi instance object
DETAILS
Swi_post is used to post a software interrupt regardless of the
trigger value. No change is made to the Swi object's trigger value.
Swi_post results in a context switch if the Swi is higher priority
than the currently executing thread.
CONSTRAINTS
Swis are ALWAYS run with interrupts enabled.
If a Swi is made ready to run as a consequence of this
API, interrupts will be globally enabled while the Swi function
executes, regardless of the prior globally enabled/disabled
state of interrupts.
Upon return from this API, the global interrupt enabled/disabled state
is restored to its previous value.
Swi_setAttrs() // instance |
|
Set the attributes of an existing Swi object
ARGUMENTS
handle
handle of a previously-created Swi instance object
swiFxn
address of the Swi function
params
pointer for returning Swi's Params
DETAILS
The 'handle' argument specifies the address of the Swi object whose
attributes are to be set.
The 'swiFxn' argument is the address of the function to be invoked
when the Swi runs. If 'swiFxn' is NULL, no change is made to the Swi
function.
The 'params' argument, which can be either NULL or a pointer to
a Swi_Params structure that contains attributes for the
Swi object, facilitates setting the attributes of the Swi object.
If 'params' is NULL, the Swi object is assigned a default set of
attributes.
Otherwise, the Swi object's attributes are set according the values
passed within 'params'.
CONSTRAINTS
Swi_setParams() must not be used on a Swi that is preempted
or is ready to run.
RELATED
Swi_setHookContext() // instance |
|
Set hook instance's context for a swi
Void Swi_setHookContext(
Swi_Handle handle,
Int id,
Ptr hookContext);
ARGUMENTS
handle
handle of a previously-created Swi instance object
id
hook instance's ID
hookContext
value to write to context
DETAILS
For example, this C code gets the HookContext, prints it,
and sets a new value for the HookContext.
Ptr pEnv;
Swi_Handle mySwi;
Int myHookSetId1;
pEnv = Swi_getHookContext(swi, myHookSetId1);
System_printf("myEnd1: pEnv = 0x%lx, time = %ld\n",
(ULong)pEnv, (ULong)Timestamp_get32());
Swi_setHookContext(swi, myHookSetId1, (Ptr)0xc0de1);
See
Hook Functions for more details.
Instance Built-Ins |
|
Int Swi_Object_count();
// The number of statically-created instance objects
// The handle of the i-th statically-created instance object (array == NULL)
// The handle of the first dynamically-created instance object, or NULL
// The handle of the next dynamically-created instance object, or NULL
// The heap used to allocate dynamically-created instance objects
// The label associated with this instance object
// The name of this instance object
struct Swi.HookSet |
|
Swi hook set type definition
var obj = new Swi.HookSet;
obj.registerFxn = Void(*)(Int) ...
DETAILS
This structure defines the set of hook functions that can be
specified for the Swi module.
See
Hook Functions for details.
C SYNOPSIS
config Swi.A_badPriority // module-wide |
|
Assertion raised if a Swi's priority is out of range
msg: "A_badPriority: An invalid Swi priority was used."
};
DETAILS
Swi priorities must be in the range of 0 and numPriorities-1.
C SYNOPSIS
config Swi.A_swiDisabled // module-wide |
|
Assertion raised if Swi_create is called and runtime Swi creation is
disabled
msg: "A_swiDisabled: Cannot create a Swi when Swi is disabled."
};
DETAILS
C SYNOPSIS
config Swi.LD_end // module-wide |
|
The event logged just after returning from a Swi's function
msg: "LD_end: swi: 0x%x"
};
C SYNOPSIS
config Swi.LM_begin // module-wide |
|
The event logged just prior to invoking a Swi's function
msg: "LM_begin: swi: 0x%x, func: 0x%x, preThread: %d"
};
C SYNOPSIS
config Swi.LM_post // module-wide |
|
The event logged when Swi_post() is called
msg: "LM_post: swi: 0x%x, func: 0x%x, pri: %d"
};
C SYNOPSIS
config Swi.numPriorities // module-wide |
|
Number of Swi priorities supported
Swi.numPriorities = UInt 16;
DETAILS
The maximum number of priorities supported is
target-specific and depends on the number of
bits in a UInt data type. For 6x and ARM devices
the maximum number of priorities is therefore 32.
For 28x, 55x, and MSP430 devices, the maximum number of
priorities is 16.
C SYNOPSIS
metaonly config Swi.common$ // module-wide |
|
Common module configuration parameters
DETAILS
All modules have this configuration parameter. Its name
contains the '$' character to ensure it does not conflict with
configuration parameters declared by the module. This allows
new configuration parameters to be added in the future without
any chance of breaking existing modules.
metaonly Swi.addHookSet() // module-wide |
|
Add hook functions to be called by the Swi scheduler
ARGUMENTS
hookSet
structure of type HookSet
DETAILS
This function is used in a config file to add a set of functions
that are called before or after significant points within the Swi
scheduler.
Configures a set of hook functions for the
Swi module. Each set contains these hook functions:
- Register: A function called before all statically-created Swis
are initialized at runtime.
- Create: A function that is called when a Swi is created.
This includes Swis that are created statically and those
created dynamically using create.
- Ready: A function that is called when any Swi becomes ready
to run.
- Begin: A function that is called just prior to running a Swi.
- End: A function that is called just after a Swi finishes.
- Delete: A function that is called when a Swi is deleted at
run-time with delete.
See
Hook Functions for more details.
HookSet structure elements may be omitted, in which case those
elements will not exist.
For example, the following configuration code defines a
HookSet:
// Hook Set 1
Swi.addHookSet({
registerFxn: '&myRegister1',
createFxn: '&myCreate1',
readyFxn: '&myReady1',
beginFxn: '&myBegin1',
endFxn: '&myEnd1',
deleteFxn: '&myDelete1'
});
Instance Config Parameters |
|
var params = new Swi.Params;
// Instance config-params object
params.arg0 = UArg 0;
// Swi function argument 0
params.arg1 = UArg 0;
// Swi function argument 1
params.priority = UInt ~0;
// Swi priority
params.trigger = UInt 0;
// Initial Swi trigger value
config Swi.arg0 // instance |
|
Swi function argument 0
var params = new Swi.Params;
...
params.arg0 = UArg 0;
DETAILS
The default value of this optional parameter is 0.
SEE
C SYNOPSIS
config Swi.arg1 // instance |
|
Swi function argument 1
var params = new Swi.Params;
...
params.arg1 = UArg 0;
DETAILS
The default value of this optional parameter is 0.
SEE
C SYNOPSIS
config Swi.priority // instance |
|
Swi priority
var params = new Swi.Params;
...
params.priority = UInt ~0;
DETAILS
Each software interrupt has a priority level, 0 to
(
numPriorities - 1). A software interrupt
preempts any lower-priority software interrupt currently executing.
When multiple Swis of the same priority level have been posted,
their respective Swi functions are executed in the order the Swis
were posted.
The default value of this optional parameter is ~0, which yields a
Swi with the highest priority: (
numPriorities - 1).
C SYNOPSIS
config Swi.trigger // instance |
|
Initial Swi trigger value
var params = new Swi.Params;
...
params.trigger = UInt 0;
DETAILS
The default value of this optional parameter is 0.
Each Swi object has a "trigger" used either to determine whether to
post the Swi or as a value that can be evaluated within the Swi's
function.
The
andn and
dec functions post the Swi
if the trigger value transitions to 0. The
or and
inc functions also modify the trigger value. (
or
sets bits, and
andn clears bits.)
C SYNOPSIS
Instance Creation |
|
// Allocate instance config-params
params.config = ...
// Assign individual configs
var inst = Swi.create(Void(*)(UArg,UArg) swiFxn, params);
// Create an instance-object
ARGUMENTS
swiFxn
Swi Function
params
per-instance config params, or NULL to select default values (target-domain only)
eb
active error-handling block, or NULL to select default policy (target-domain only)
DETAILS
Swi_create creates a new Swi object.
The following C code sets Swi parameters and
creates two Swi objects:
Void main()
{
Swi_Params swiParams;
Swi_Params_init(&swiParams);
swiParams.arg0 = 1;
swiParams.arg1 = 0;
swiParams.priority = 2;
swiParams.trigger = 0;
swi0 = Swi_create(swi0Fxn, &swiParams, NULL);
swiParams.arg0 = 2;
swiParams.arg1 = 0;
swiParams.priority = 1;
swiParams.trigger = 3;
swi1 = Swi_create(swi1Fxn, &swiParams, NULL);
BIOS_start();
}
The following XDCscript statements set Swi parameters and
create two Swi objects:
var Swi = xdc.useModule('ti.sysbios.knl.Swi');
var swiParams = new Swi.Params();
swiParams.arg0 = 1;
swiParams.arg1 = 0;
swiParams.priority = 2;
swiParams.trigger = 0;
Program.global.swi0 = Swi.create('&swi0Fxn', swiParams);
swiParams.arg0 = 2;
swiParams.priority = 1;
swiParams.trigger = 3;
Program.global.swi1 = Swi.create('&swi1Fxn', swiParams);