| module ti.sysbios.family.arm.a8.TimestampProvider |
 |
 |
A8 TimestampProvider
The source of the timestamps for the A8 TimestampProvider is
the A8's internal PMC counter which counts CPU cycles.
[
more ... ]
#include <ti/sysbios/family/arm/a8/TimestampProvider.h>
Functions common to all ITimestamp modules |
Bits32 | |
Void | |
Void | |
Functions common to all target modules |
|
|
DETAILS
The source of the timestamps for the A8 TimestampProvider is
the A8's internal PMC counter which counts CPU cycles.
As this counter is only 32 bits in length, provision is made
in the get64() API to test if an overflow has occurred since
the last invocation of get64() and compensate the return value
accordingly.
As it is possible for the 32 bit counter to roll over more
than once between successive get64() calls, it is up to the user
to call the get64() API often enough to guarantee coherency in
successive timestamps. A simple mechanism to do this would be
to add a Clock function that simply invokes get64():
var Clock = xdc.useModule('ti.sysbios.knl.Clock');
var TimestampProvider = xdc.useModule('ti.sysbios.family.arm.a8.TimestampProvider');
var clockParams = new Clock.Params();
clockParams.period = 1; // call every Clock tick
Clock.create($externModFxn(TimestampProvider.get64), 1, clockParams);
Calling Context
| Function | Hwi | Swi |
Task | Main | Startup |
| get32 | Y | Y |
Y | Y | N |
| get64 | Y | Y |
Y | Y | N |
| getFreq | Y | Y |
Y | Y | N |
Definitions:
- Hwi: API is callable from a Hwi thread.
- Swi: API is callable from a Swi thread.
- Task: API is callable from a Task thread.
- Main: API is callable during any of these phases:
- In your module startup after this module is started
(e.g. TimestampProvider_Module_startupDone() returns TRUE).
- During xdc.runtime.Startup.lastFxns.
- During main().
- During BIOS.startupFxns.
- Startup: API is callable during any of these phases:
- During xdc.runtime.Startup.firstFxns.
- In your module startup before this module is started
(e.g. TimestampProvider_Module_startupDone() returns FALSE).
|
| TimestampProvider_get32() // module-wide |
 |
Return a 32-bit timestamp
Bits32 TimestampProvider_get32();
RETURNS
Returns a 32-bit timestamp value.
Use
getFreq to convert this value into units of real time.
Returns a 32-bit timestamp value.
Use
getFreq to convert this value into units of real time.
SEE
| TimestampProvider_get64() // module-wide |
 |
Return a 64-bit timestamp
ARGUMENTS
result
pointer to 64-bit result
This parameter is a pointer to a structure representing a 64-bit
wide timestamp value where the current timestamp is written.
If the underlying hardware does not support 64-bit resolution, the
hi field of
result is always set to 0; see
xdc.runtime.Types.Timestamp64. So, it is possible for
the
lo field to wrap around without any change to the
hi field.
Use
getFreq to convert this value into units of real
time.
pointer to 64-bit result
This parameter is a pointer to a structure representing a 64-bit
wide timestamp value where the current timestamp is written.
If the underlying hardware does not support 64-bit resolution, the
hi field of
result is always set to 0; see
xdc.runtime.Types.Timestamp64. So, it is possible for
the
lo field to wrap around without any change to the
hi field.
Use
getFreq to convert this value into units of real
time.
SEE
| TimestampProvider_getFreq() // module-wide |
 |
Get the timestamp timer's frequency (in Hz)
ARGUMENTS
freq
pointer to a 64-bit result
This parameter is a pointer to a structure representing a 64-bit
wide frequency value where the timer's frequency (in Hz)
is written; see
xdc.runtime.Types.FreqHz.
This function provides a way of converting timestamp
values into units of real time.
pointer to a 64-bit result
This parameter is a pointer to a structure representing a 64-bit
wide frequency value where the timer's frequency (in Hz)
is written; see
xdc.runtime.Types.FreqHz.
This function provides a way of converting timestamp
values into units of real time.
SEE
| Module-Wide Built-Ins |
 |
// Get this module's unique id
Bool TimestampProvider_Module_startupDone();
// Test if this module has completed startup
// The heap from which this module allocates memory
Bool TimestampProvider_Module_hasMask();
// Test whether this module has a diagnostics mask
Bits16 TimestampProvider_Module_getMask();
// Returns the diagnostics mask for this module
Void TimestampProvider_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
var TimestampProvider = xdc.useModule('ti.sysbios.family.arm.a8.TimestampProvider');
module-wide config parameters
generated on Fri, 26 Jul 2013 18:18:35 GMT