module ti.sysbios.hal.Timer

Timer Manager Proxy

The ti.sysbios.hal.Timer module presents a standard interface for using the timer peripherals. This module is part of the Hardware Abstraction Layer (HAL) package, which hides target/device-specific characteristics of the hardware. [ more ... ]
C synopsis target-domain sourced in ti/sysbios/hal/Timer.xdc
#include <ti/sysbios/hal/Timer.h>
Functions
Void
Void
Void
Void
Functions common to all ITimer modules
UInt32 
Void 
UInt 
UInt32 
Void 
Void 
Bool 
Void 
Void 
Functions common to all target instances
Functions common to all target modules
Defines
#define
Typedefs
typedef Void 
typedef Timer_Object *
typedef struct
typedef struct
typedef enum
typedef enum
typedef enum
typedef enum
typedef struct
 
DETAILS
The ti.sysbios.hal.Timer module presents a standard interface for using the timer peripherals. This module is part of the Hardware Abstraction Layer (HAL) package, which hides target/device-specific characteristics of the hardware.
You can use this module to create a timer (that is, to mark a timer for use) and configure it to call a tickFxn when the timer expires. Use this module only if you do not need to do any custom configuration of the timer peripheral.
The timer can be configured as a one-shot or a continuous mode timer. The period can be specified in timer counts or microseconds.
The timer interrupt always uses the Hwi dispatcher. The Timer tickFxn runs in the context of a Hwi thread. The Timer module automatically creates a Hwi instance for the timer interrupt.
The actual implementations of the Timer module functions are provided by device/family-specific Timer modules. Additional, family-specific Timer module APIs may also be provided by your Timer module implementation. Follow the link below to determine which Timer implementation is used for your target:

Calling Context

Function Hwi Swi Task Main Startup
getNumTimers Y Y Y Y N
getStatus Y Y Y Y N
Params_init Y Y Y Y N
construct Y Y Y Y N
create N N Y Y N
delete N N Y Y N
destruct Y Y Y Y N
getFreq Y Y Y Y N
getPeriod Y Y Y Y N
setPeriod Y Y Y Y N
setPeriodMicroSecs Y Y Y Y N
start Y Y Y N N
stop Y Y Y N N
Definitions:
  • Hwi: API is callable from a Hwi thread.
  • Swi: API is callable from a Swi thread.
  • Task: API is callable from a Task thread.
  • Main: API is callable during any of these phases:
    • In your module startup after this module is started (e.g. Timer_Module_startupDone() returns TRUE).
    • During xdc.runtime.Startup.lastFxns.
    • During main().
    • During BIOS.startupFxns.
  • Startup: API is callable during any of these phases:
    • During xdc.runtime.Startup.firstFxns.
    • In your module startup before this module is started (e.g. Timer_Module_startupDone() returns FALSE).
 
const Timer_ANY

Const used to specify any timer

C synopsis target-domain
#define Timer_ANY (UInt)~0
 
 
enum Timer_PeriodType

Timer period units

C synopsis target-domain
typedef enum Timer_PeriodType {
    Timer_PeriodType_MICROSECS,
    // period in microsecs
    Timer_PeriodType_COUNTS
    // period in counts
} Timer_PeriodType;
 
VALUES
PeriodType_MICROSECS — Period value is in microseconds.
PeriodType_COUNTS — Period value is in counts.
 
enum Timer_RunMode

Timer Run Modes

C synopsis target-domain
typedef enum Timer_RunMode {
    Timer_RunMode_CONTINUOUS,
    // periodic and continuous
    Timer_RunMode_ONESHOT,
    // one-shot
    Timer_RunMode_DYNAMIC
    // dynamically reprogrammed (available on subset of devices)
} Timer_RunMode;
 
VALUES
RunMode_CONTINUOUS — Timer is periodic and runs continuously.
RunMode_ONESHOT — Timer runs for a single period value and stops.
RunMode_DYNAMIC — Timer is dynamically reprogrammed for the next required tick.
 
enum Timer_StartMode

Timer Start Modes

C synopsis target-domain
typedef enum Timer_StartMode {
    Timer_StartMode_AUTO,
    // timer starts automatically
    Timer_StartMode_USER
    // timer will be started by user
} Timer_StartMode;
 
VALUES
StartMode_AUTO — Statically created/constructed Timers will be started in BIOS_start(). Dynamically created Timers will start at create() time. This includes timers created before BIOS_start().
StartMode_USER — Timer will be started by the user using start().
 
enum Timer_Status

Timer Status

C synopsis target-domain
typedef enum Timer_Status {
    Timer_Status_INUSE,
    // timer in use
    Timer_Status_FREE
    // timer is free
} Timer_Status;
 
VALUES
Status_INUSE — Timer is in use. A timer is marked in use from the time it gets created to the time it gets deleted.
Status_FREE — Timer is free and can be acquired using create.
 
typedef Timer_FuncPtr

Timer tick function prototype

C synopsis target-domain
typedef Void (*Timer_FuncPtr)(UArg);
 
 
Timer_getNumTimers()  // module-wide

Returns number of timer peripherals on the platform

C synopsis target-domain
UInt Timer_getNumTimers();
 
RETURNS
Number of timer peripherals.
 
Timer_getStatus()  // module-wide

Returns timer status (free or in use)

C synopsis target-domain
ITimer_Status Timer_getStatus(UInt id);
 
RETURNS
timer status
Module-Wide Built-Ins

C synopsis target-domain
Types_ModuleId Timer_Module_id();
// Get this module's unique id
 
Bool Timer_Module_startupDone();
// Test if this module has completed startup
 
IHeap_Handle Timer_Module_heap();
// The heap from which this module allocates memory
 
Bool Timer_Module_hasMask();
// Test whether this module has a diagnostics mask
 
Bits16 Timer_Module_getMask();
// Returns the diagnostics mask for this module
 
Void Timer_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
Instance Object Types

C synopsis target-domain
typedef struct Timer_Object Timer_Object;
// Opaque internal representation of an instance object
 
typedef Timer_Object *Timer_Handle;
// Client reference to an instance object
 
typedef struct Timer_Struct Timer_Struct;
// Opaque client structure large enough to hold an instance object
 
Timer_Handle Timer_handle(Timer_Struct *structP);
// Convert this instance structure pointer into an instance handle
 
Timer_Struct *Timer_struct(Timer_Handle handle);
// Convert this instance handle into an instance structure pointer
Instance Config Parameters

C synopsis target-domain
typedef struct Timer_Params {
// Instance config-params structure
    IInstance_Params *instance;
    // Common per-instance configs
    UArg arg;
    // Argument for tick function
    Types_FreqHz extFreq;
    // Timer frequency
    UInt32 period;
    // Period of a tick
    ITimer_PeriodType periodType;
    // Period type
    ITimer_RunMode runMode;
    // Timer run mode
    ITimer_StartMode startMode;
    // Timer start mode
} Timer_Params;
 
Void Timer_Params_init(Timer_Params *params);
// Initialize this config-params structure with supplier-specified defaults before instance creation
 
config Timer_arg  // instance

Argument for tick function

C synopsis target-domain
struct Timer_Params {
      ...
    UArg arg;
 
DETAILS
Default is null.
 
config Timer_extFreq  // instance

Timer frequency

C synopsis target-domain
struct Timer_Params {
      ...
    Types_FreqHz extFreq;
 
DETAILS
This parameter is meaningfull only on platforms where the timer's input clock can be changed. If value is left at zero, then input clock to the timer clock is assumed.
This value is used to convert timer ticks to real time units; seconds, milliseconds, etc.
 
config Timer_period  // instance

Period of a tick

C synopsis target-domain
struct Timer_Params {
      ...
    UInt32 period;
 
DETAILS
The period can be specified in timer counts or microseconds and its default value is 0.
The implementation of ITimer will support a period of UInt32 timer counts and use pre-scalars if necessary.
 
config Timer_periodType  // instance

Period type

C synopsis target-domain
struct Timer_Params {
      ...
    ITimer_PeriodType periodType;
 
DETAILS
Default is PeriodType_MICROSECS
 
config Timer_runMode  // instance

Timer run mode

C synopsis target-domain
struct Timer_Params {
      ...
    ITimer_RunMode runMode;
 
DETAILS
Default is RunMode_CONTINUOUS.
 
config Timer_startMode  // instance

Timer start mode

C synopsis target-domain
struct Timer_Params {
      ...
    ITimer_StartMode startMode;
 
DETAILS
Default is StartMode_AUTO.
Instance Creation

C synopsis target-domain
Timer_Handle Timer_create(Int id, Timer_FuncPtr tickFxn, const Timer_Params *params, Error_Block *eb);
// Allocate and initialize a new instance object and return its handle
 
Void Timer_construct(Timer_Struct *structP, Int id, Timer_FuncPtr tickFxn, const Timer_Params *params, Error_Block *eb);
// Initialize a new instance object inside the provided structure
ARGUMENTS
id — Timer id ranging from 0 to a platform specific value
tickFxn — function that runs upon timer expiry.
params — per-instance config params, or NULL to select default values (target-domain only)
eb — active error-handling block, or NULL to select default policy (target-domain only)
DETAILS
Create could fail if timer peripheral is unavailable. To request any available timer use ANY as the id. TimerId's are logical ids. The family-specific implementations map the ids to physical peripherals.
Instance Deletion

C synopsis target-domain
Void Timer_delete(Timer_Handle *handleP);
// Finalize and free this previously allocated instance object, setting the referenced handle to NULL
 
Void Timer_destruct(Timer_Struct *structP);
// Finalize the instance object inside the provided structure
 
Timer_getCount()  // instance

Read timer counter register

C synopsis target-domain
UInt32 Timer_getCount(Timer_Handle handle);
 
ARGUMENTS
handle — handle of a previously-created Timer instance object
RETURNS
timer counter value
 
Timer_getFreq()  // instance

Return timer frequency in Hz

C synopsis target-domain
Void Timer_getFreq(Timer_Handle handle, Types_FreqHz *freq);
 
ARGUMENTS
handle — handle of a previously-created Timer instance object
freq — frequency in Hz
DETAILS
This is the effective frequency of the clock incrementing the timer counter register after all scaling factors are taken into account. (including pre-scalars).
 
Timer_getFunc()  // instance

Get Timer function and arg

C synopsis target-domain
ITimer_FuncPtr Timer_getFunc(Timer_Handle handle, UArg *arg);
 
ARGUMENTS
handle — handle of a previously-created Timer instance object
arg — pointer for returning Timer's function argument
RETURNS
Timer's function
 
Timer_getPeriod()  // instance

Get timer period in timer counts

C synopsis target-domain
UInt32 Timer_getPeriod(Timer_Handle handle);
 
ARGUMENTS
handle — handle of a previously-created Timer instance object
RETURNS
period in timer counts
 
Timer_setFunc()  // instance

Overwrite Timer function and arg

C synopsis target-domain
Void Timer_setFunc(Timer_Handle handle, ITimer_FuncPtr fxn, UArg arg);
 
ARGUMENTS
handle — handle of a previously-created Timer instance object
fxn — pointer to function
arg — argument to function
DETAILS
Replaces a Timer object's tickFxn function originally provided in create.
 
Timer_setPeriod()  // instance

Set timer period specified in timer counts

C synopsis target-domain
Void Timer_setPeriod(Timer_Handle handle, UInt32 period);
 
ARGUMENTS
handle — handle of a previously-created Timer instance object
period — period in timer counts
DETAILS
Timer_setPeriod() invokes Timer_stop() prior to setting the period and leaves the timer in the stopped state.
To dynamically change the period of a timer you must protect against re-entrancy by disabling interrupts. Use the following call sequence to guarantee proper results:
  // disable interrupts if an interrupt could lead to
  // another call to Timer_start().
  key = Hwi_disable();
  Timer_setPeriod(period);
  Timer_start();
  Hwi_restore(key);
ITimer implementation must support UInt32 and use pre-scalars whenever necessary
SIDE EFFECTS
Calls Timer_stop(), and disables the timer's interrupt.
 
Timer_setPeriodMicroSecs()  // instance

Set timer period specified in microseconds

C synopsis target-domain
Bool Timer_setPeriodMicroSecs(Timer_Handle handle, UInt32 microsecs);
 
ARGUMENTS
handle — handle of a previously-created Timer instance object
period — period in microseconds
DETAILS
A best-effort method will be used to set the period register. There might be a slight rounding error based on resolution of timer period register. If the timer frequency cannot support the requested period, i.e. the timer period register cannot support the requested period, then this function returns false.
Timer_setPeriodMicroSecs() invokes Timer_stop() prior to setting the period and leaves the timer in the stopped state.
To dynamically change the period of a timer you must protect against re-entrancy by disabling interrupts. Use the following call sequence to guarantee proper results:
  // disable interrupts if an interrupt could lead to
  // another call to Timer_start().
  key = Hwi_disable();
  Timer_setPeriodMicroSecs(period);
  Timer_start();
  Hwi_restore(key);
 
Timer_start()  // instance

Reload and start the timer

C synopsis target-domain
Void Timer_start(Timer_Handle handle);
 
ARGUMENTS
handle — handle of a previously-created Timer instance object
DETAILS
Thread safety must be observed when using the start and stop APIs to avoid possible miss- configuration of the timers and unintended behaviors. To protect against re-entrancy, surround the start/stop invocations with Hwi_disable() and Hwi_restore() calls:
  // disable interrupts if an interrupt could lead to
  // another call to Timer_start().
  key = Hwi_disable();
  Timer_stop();
  ...
  Timer_start();
  Hwi_restore(key);
SIDE EFFECTS
Enables the timer's interrupt.
 
Timer_stop()  // instance

Stop the timer

C synopsis target-domain
Void Timer_stop(Timer_Handle handle);
 
ARGUMENTS
handle — handle of a previously-created Timer instance object
DETAILS
Thread safety must be observed when using the start and stop APIs to avoid possible miss- configuration of the timers and unintended behaviors. To protect against re-entrancy, surround the start/stop invocations with Hwi_disable() and Hwi_restore() calls:
  // disable interrupts if an interrupt could lead to
  // another call to Timer_start().
  key = Hwi_disable();
  Timer_stop();
  ...
  Timer_start();
  Hwi_restore(key);
SIDE EFFECTS
Disables the timer's interrupt.
Instance Convertors

C synopsis target-domain
ITimer_Handle Timer_Handle_upCast(Timer_Handle handle);
// unconditionally move one level up the inheritance hierarchy
 
Timer_Handle Timer_Handle_downCast(ITimer_Handle handle);
// conditionally move one level down the inheritance hierarchy; NULL upon failure
Instance Built-Ins

C synopsis target-domain
Int Timer_Object_count();
// The number of statically-created instance objects
 
Timer_Handle Timer_Object_get(Timer_Object *array, Int i);
// The handle of the i-th statically-created instance object (array == NULL)
 
Timer_Handle Timer_Object_first();
// The handle of the first dynamically-created instance object, or NULL
 
Timer_Handle Timer_Object_next(Timer_Handle handle);
// The handle of the next dynamically-created instance object, or NULL
 
IHeap_Handle Timer_Object_heap();
// The heap used to allocate dynamically-created instance objects
 
Types_Label *Timer_Handle_label(Timer_Handle handle, Types_Label *buf);
// The label associated with this instance object
 
String Timer_Handle_name(Timer_Handle handle);
// The name of this instance object
 
XDCscript usage meta-domain sourced in ti/sysbios/hal/Timer.xdc
var Timer = xdc.useModule('ti.sysbios.hal.Timer');
module-wide constants & types
 
 
    values of type Timer.RunMode// Timer Run Modes
        const Timer.RunMode_ONESHOT// one-shot;
 
    values of type Timer.StartMode// Timer Start Modes
 
    values of type Timer.Status// Timer Status
        const Timer.Status_INUSE// timer in use;
        const Timer.Status_FREE// timer is free;
module-wide config parameters
per-instance config parameters
    var params = new Timer.Params// Instance config-params object;
        params.arg// Argument for tick function = UArg null;
        params.extFreq// Timer frequency = Types.FreqHz {
            lo: 0,
            hi: 0
        };
        params.period// Period of a tick = UInt32 0;
per-instance creation
    var inst = Timer.create// Create an instance-object(Int id, Void(*)(UArg) tickFxn, params);
 
 
const Timer.ANY

Const used to specify any timer

XDCscript usage meta-domain
const Timer.ANY = ~0;
 
C SYNOPSIS
 
enum Timer.PeriodType

Timer period units

XDCscript usage meta-domain
values of type Timer.PeriodType
    const Timer.PeriodType_MICROSECS;
    // period in microsecs
    const Timer.PeriodType_COUNTS;
    // period in counts
 
VALUES
PeriodType_MICROSECS — Period value is in microseconds.
PeriodType_COUNTS — Period value is in counts.
C SYNOPSIS
 
enum Timer.RunMode

Timer Run Modes

XDCscript usage meta-domain
values of type Timer.RunMode
    const Timer.RunMode_CONTINUOUS;
    // periodic and continuous
    const Timer.RunMode_ONESHOT;
    // one-shot
    const Timer.RunMode_DYNAMIC;
    // dynamically reprogrammed (available on subset of devices)
 
VALUES
RunMode_CONTINUOUS — Timer is periodic and runs continuously.
RunMode_ONESHOT — Timer runs for a single period value and stops.
RunMode_DYNAMIC — Timer is dynamically reprogrammed for the next required tick.
C SYNOPSIS
 
enum Timer.StartMode

Timer Start Modes

XDCscript usage meta-domain
values of type Timer.StartMode
    const Timer.StartMode_AUTO;
    // timer starts automatically
    const Timer.StartMode_USER;
    // timer will be started by user
 
VALUES
StartMode_AUTO — Statically created/constructed Timers will be started in BIOS_start(). Dynamically created Timers will start at create() time. This includes timers created before BIOS_start().
StartMode_USER — Timer will be started by the user using start().
C SYNOPSIS
 
enum Timer.Status

Timer Status

XDCscript usage meta-domain
values of type Timer.Status
    const Timer.Status_INUSE;
    // timer in use
    const Timer.Status_FREE;
    // timer is free
 
VALUES
Status_INUSE — Timer is in use. A timer is marked in use from the time it gets created to the time it gets deleted.
Status_FREE — Timer is free and can be acquired using create.
C SYNOPSIS
 
metaonly config Timer.common$  // module-wide

Common module configuration parameters

XDCscript usage meta-domain
Timer.common$ = Types.Common$ undefined;
 
DETAILS
All modules have this configuration parameter. Its name contains the '$' character to ensure it does not conflict with configuration parameters declared by the module. This allows new configuration parameters to be added in the future without any chance of breaking existing modules.
Instance Config Parameters

XDCscript usage meta-domain
var params = new Timer.Params;
// Instance config-params object
    params.arg = UArg null;
    // Argument for tick function
    params.extFreq = Types.FreqHz {
    // Timer frequency
        lo: 0,
        hi: 0
    };
    params.period = UInt32 0;
    // Period of a tick
    params.periodType = ITimer.PeriodType ITimer.PeriodType_MICROSECS;
    // Period type
    params.runMode = ITimer.RunMode ITimer.RunMode_CONTINUOUS;
    // Timer run mode
    params.startMode = ITimer.StartMode ITimer.StartMode_AUTO;
    // Timer start mode
 
config Timer.arg  // instance

Argument for tick function

XDCscript usage meta-domain
var params = new Timer.Params;
  ...
params.arg = UArg null;
 
DETAILS
Default is null.
C SYNOPSIS
 
config Timer.extFreq  // instance

Timer frequency

XDCscript usage meta-domain
var params = new Timer.Params;
  ...
params.extFreq = Types.FreqHz {
    lo: 0,
    hi: 0
};
 
DETAILS
This parameter is meaningfull only on platforms where the timer's input clock can be changed. If value is left at zero, then input clock to the timer clock is assumed.
This value is used to convert timer ticks to real time units; seconds, milliseconds, etc.
C SYNOPSIS
 
config Timer.period  // instance

Period of a tick

XDCscript usage meta-domain
var params = new Timer.Params;
  ...
params.period = UInt32 0;
 
DETAILS
The period can be specified in timer counts or microseconds and its default value is 0.
The implementation of ITimer will support a period of UInt32 timer counts and use pre-scalars if necessary.
C SYNOPSIS
 
config Timer.periodType  // instance

Period type

XDCscript usage meta-domain
var params = new Timer.Params;
  ...
 
DETAILS
Default is PeriodType_MICROSECS
C SYNOPSIS
 
config Timer.runMode  // instance

Timer run mode

XDCscript usage meta-domain
var params = new Timer.Params;
  ...
 
DETAILS
Default is RunMode_CONTINUOUS.
C SYNOPSIS
 
config Timer.startMode  // instance

Timer start mode

XDCscript usage meta-domain
var params = new Timer.Params;
  ...
 
DETAILS
Default is StartMode_AUTO.
C SYNOPSIS
Instance Creation

XDCscript usage meta-domain
var params = new Timer.Params;
// Allocate instance config-params
params.config =   ...
// Assign individual configs
 
var inst = Timer.create(Int id, Void(*)(UArg) tickFxn, params);
// Create an instance-object
ARGUMENTS
id — Timer id ranging from 0 to a platform specific value
tickFxn — function that runs upon timer expiry.
params — per-instance config params, or NULL to select default values (target-domain only)
eb — active error-handling block, or NULL to select default policy (target-domain only)
DETAILS
Create could fail if timer peripheral is unavailable. To request any available timer use ANY as the id. TimerId's are logical ids. The family-specific implementations map the ids to physical peripherals.
generated on Thu, 11 Oct 2012 23:22:32 GMT