Every library, executable, and repository added to the package is
automatically added to the default release.
struct PackageContents.Attrs |
|
Package-level attributes
XDCscript usage |
meta-domain |
var obj = new PackageContents.Attrs;
obj.profile = String ...
// select appropriate ITarget.OptionSet
obj.aopts = String ...
// assembly language options
obj.copts = String ...
// C/C++ compiler options
obj.defs = String ...
// -D options common to C/C++/asm
obj.incs = String ...
// -I options common to C/C++/asm
obj.tcopts = String ...
// tconf options, deprecated
obj.xsopts = String ...
// xs options
obj.lopts = String ...
// linker options
obj.exportDoc = Bool ...
// if true, export generated docs
obj.exportExe = Bool ...
// if true, export executables
obj.exportCfg = Bool ...
// if true, export program cfg scripts
obj.exportSrc = Bool ...
// if true, export all package sources
obj.exportAll = Bool ...
// if true, export all non-gen'd files
obj.relScript = String ...
// release files post-processing script
obj.compress = Bool ...
// if true, compress package release archives
obj.archiver = String ...
// "tar" or "zip"; defaults to "tar"
FIELDS
profile
This string names a profile defined by the
executable's target. A profile specifies a set of compiler,
linker, and archiver options that are to be used when
compiling and linking code. Note that these tool options are
in addition to any options specified via aopts, copts,
etc.
If this field is not specified or set to null, the
"release" profile will be used.
incs
This string contains include path options used by
the compiler (or assembler) to locate include files; e.g.,
"-I ../../include -I ../c55xx". Note that the syntax of
this string may be target dependent.
defs
This string contains options used by the
compiler (or assembler) to define macros; e.g.,
"-D_C6xxx -DDEBUG=1". Note that the syntax of
this string may be target dependent.
aopts
This string contains options used by the assembler
to produce object files; e.g., "-mP1". Note that the syntax
of this string may be target dependent.
copts
This string contains options used by the C/C++
compiler to produce object files; e.g., "-o3 -mi1". Note
that the syntax of this string may be target dependent.
lopts
This string contains options used by the linker
produce object files; e.g., "-l mylib.lib". Note
that the syntax of this string may be target dependent.
tcopts
This string contains options passed to tconf
Deprecated, use xsopts instead.
xsopts
This string contains options passed to xs
when running configuration scripts; e.g., to turn on the
reporting of warnings this string can be set to "-js -w",
or to define the name-value pair "FOO=bar" available via
the environment hash-table xsopts should be set to
"-DFOO=bar".
exportCfg
If this field is set to true, configuration
scripts will, by default, be part of the releases created
by this package.
exportDoc
If this field is set to true, generated
documentation will, by default, be part of the releases
created by this package.
exportSrc
If this field is set to true, the sources
used to build this package will, by default, be part of the
releases created by this package.
exportExe
If this field is set to true, the executables
created in this package will, by default, be part of the
releases created by this package.
exportAll
If this field is set to true, all files
in this package that are not known to be generated are in
the release. If it is unspecified (or set to null) these
files will not be added to this release. See
xdc.bld.Release.Attrs for more information about
this option.
relScript
If this field is non-null, the string names a
"release script" that is run to post-process the
files that are part of a release. Like configuration scripts,
the string names a script file that is searched for first in
the in package's base directory, and then along the package
path.
compress
If this field is set to true, the package release
archive files will be, by default, compressed; otherwise, the
archives will not be compressed
archiver
This field names the archiver to use when creating a
release. Two archivers are currently supported:
"tar" and "zip". If the archiver is set to "zip"
the Attrs.compress field is implicitly set to
true.
DETAILS
These attributes provide package-level defaults for attributes that
provide control over the code generation tools, the configuration
tool, and release options.
SEE
config PackageContents.attrs // module-wide |
|
Package attributes
XDCscript usage |
meta-domain |
DETAILS
These attributes are "inherited" by all executables and libraries
added to this package set.
SEE
config PackageContents.cfgDir // module-wide |
|
The directory where all intermediate program files are placed
XDCscript usage |
meta-domain |
PackageContents.cfgDir = String "package/cfg/";
DETAILS
During configuration, several files are generated (a C++ source file,
a linker command file, etc.) these generated files are placed in
the directory specified by this parameter.
config PackageContents.defaultRelease // module-wide |
|
The default release for this package
XDCscript usage |
meta-domain |
DETAILS
If this configuration parameter is defined, it is taken to be the
default release instance; otherwise a default instance is created
with the appropriate defaults.
If this release's label attribute is undefined or null, it is
set to "default" before the release is generated; otherwise the
label attribute is unchanged from what the user specified for this
instance.
The implicitly created default release is created as follows:
PackageContents.addRelease(name, {label: "default"})
where name is the package's name with all '.'s replaced with '_'.
config PackageContents.docDir // module-wide |
|
The directory where generated docs are placed
XDCscript usage |
meta-domain |
PackageContents.docDir = String undefined;
DETAILS
If set to a non-null value, package documentation will be
automatically generated and placed in this directory. If
it is not set or set to null, no docs will be generated for
this package.
If you set
exportDoc or
exportAll
to
true the generated docs will be included in the appropriate
releases of the package.
config PackageContents.generatedFiles // module-wide |
|
Array of generated files
XDCscript usage |
meta-domain |
PackageContents.generatedFiles = String[] undefined;
DETAILS
This is an array of arbitrary file names that are to be removed
during a clean of this package. File names that end with the '/'
character are assumed to be directories; in this case, the directory
and all of its contents are removed during the clean.
Only those files that are not already directly (or indirectly)
named by adding executables or libraries to this package set need
to appear in this array.
config PackageContents.imports // module-wide |
|
An array of required packages (and their version) for this package
XDCscript usage |
meta-domain |
PackageContents.imports = String[] undefined;
READONLY
This parameter is an array of all prerequisite packages
required by this package. Each string is of the form:
<packageName>{<packageCompatibilityKey>
where <packageName> is the name of the required package and
<packageCompatibilityKey> is the compatibility key specified in the
requires statement of this package. If no compatibility key is
specified in package.xdc, <packageCompatibilityKey> is "".
If the package specifies that a requirement is "internal", the
package name is prefixed with a '*' character. In other words, the
string is of the form:
*<packageName>{<packageCompatibilityKey>
config PackageContents.interfaces // module-wide |
|
An array of interface names provided by this package
XDCscript usage |
meta-domain |
PackageContents.interfaces = String[] undefined;
READONLY
This parameter is an array of all interface names
defined by this package.
config PackageContents.libDir // module-wide |
|
The directory where all intermediate library directories are placed
XDCscript usage |
meta-domain |
PackageContents.libDir = String "package/lib/";
DETAILS
Each object file for a library is placed in a sub-directory of this
directory that has a name that matches the name specified in the
addLibrary() function.
config PackageContents.libTemplate // module-wide |
|
Template of a common C-file archived into every library
XDCscript usage |
meta-domain |
PackageContents.libTemplate = String null;
DETAILS
This template can be used to embed package-specific meta-information
into each library produced by the package. For example, it can be
used to add package version infomation to each library.
This template is expanded just once in the Build model during
makefile generation. Thus, the contents of the resulting C-file can
not be library specific.
The template is found using xdc.findFile() and, as a result,
libTemplate may refer to a template in either the current package
or even in another package.
During expansion of the template, the this pointer is the
PackageContents module object; i.e., the object that the global
variable Pkg references.
The expanded template may refer to the following pre-defined macros:
- __xdc_PKGVERS
-
the package compatibility key declared in package.xdc; e.g.
"1, 2, 3"
- __xdc_PKGNAME
-
the package's name; e.g., xdc.bld
- __xdc_PKGPREFIX
-
the package's prefix; e.g., for the package xdc.bld the
prefix would be xdc_bld_
config PackageContents.makeEpilogue // module-wide |
|
String to add to the end of the generated makefile
XDCscript usage |
meta-domain |
PackageContents.makeEpilogue = String "";
DETAILS
Similar to makePrologue except that this string is placed at
the very end of the generated makefile.
config PackageContents.makePrologue // module-wide |
|
String to add to the beginning of the generated makefile
XDCscript usage |
meta-domain |
PackageContents.makePrologue = String "";
DETAILS
This string is placed at the very beginning of the package's
generated makefile. This allows one to extend the build
environment using any facility available to GNU make.
config PackageContents.modules // module-wide |
|
An array of module names provided by this package
XDCscript usage |
meta-domain |
PackageContents.modules = String[] undefined;
READONLY
This parameter is an array of all module names
implemented in this package.
config PackageContents.name // module-wide |
|
Name of this package
XDCscript usage |
meta-domain |
PackageContents.name = String undefined;
READONLY
This parameter is the name of this package as
specified by the package.xdc package specification file
config PackageContents.otherFiles // module-wide |
|
Array of files to include this package
XDCscript usage |
meta-domain |
PackageContents.otherFiles = String[] undefined;
DETAILS
This is an array of arbitrary file names that are to be included
in the package.
Only those files that are not already directly (or indirectly)
named by adding executables or libraries to this package set need
to appear in this array.
config PackageContents.otherSrcs // module-wide |
|
Array of source files to include this package
XDCscript usage |
meta-domain |
PackageContents.otherSrcs = String[] undefined;
DETAILS
Like otherFiles except that the file names listed here are to be
post-processed by the xdc document preparation tools. This array
only needs to specify files that are not implicitly specidied via
any of the addObjects function; e.g., script files, hand-creafted
headers, etc.
config PackageContents.relDir // module-wide |
|
The directory where all intermediate release files are placed
XDCscript usage |
meta-domain |
PackageContents.relDir = String "package/rel/";
DETAILS
Release specific files for a release are placed in a sub-directory of
this directory that has a name that matches the name specified in the
addRelease() function.
config PackageContents.releasePrefix // module-wide |
|
A prefix appended to the name of each release archive
XDCscript usage |
meta-domain |
PackageContents.releasePrefix = String "";
DETAILS
This configuration parameter allows one to generate release archives
somewhere other than inside the package being built. releasePrefix
is prepended to the name of the release name to form the name of the
release archive.
For example, setting releasePrefix to "../" implies that a
release named "exports/foo" generates an archive file named
foo.tar in the directory "../exports".
releasePrefix must be a relative path that is relative to the
package's "base" directory; i.e., the directory containing the
package's specification file package.xdc.
This prefix can be overridden on a per release basis; see
xdc.bld.Release.Attrs.
NOTE
If this parameter starts with "..", the resulting archive
file will not be removed as part of a package clean.
config PackageContents.uses // module-wide |
|
Array of directory suffixes used to locate files
XDCscript usage |
meta-domain |
PackageContents.uses = String[] undefined;
DETAILS
This array of directory suffixes is used to locate package files
that are referenced (e.g., via #include) without the package name.
This array names package directory suffixes (found along the
package path) that:
- contain headers included by this package's sources which
are included *without* using the package name, or
- contain JavaScript "import" files which are included (via
utils.importFile()) *without* using the package name.
This mechanism is used to support legacy code that does not
explicitly name the package in the #include statements, and *only*
affects the compiler's -I options (not the package path) and the
configuration tool's import path (config.importPath).
Strings in the Pkg.uses array must not be absolute paths. Each string
in the Pkg.uses array must point to an existing directory that can be
located along the package path. The generated makefiles create an
absolute path by simply appending the string from uses[] to each
directory name in the package path until an existing directory is
found. The resulting absolute path is then passed to the compiler in
a -I option, for example.
The directories named in this array may include sub-directories of
any package in the package path.
The strings in this array should use '/' to separate directories;
even on Windows systems. Since Windows supports '/' as a directory
separator, the use of '/' ensures host platform independence.
EXAMPLE
The following example allows sources in the current package to
"#include <tsk.h>" and have the compiler find tsk.h in the
sub-directory ti/bios/include which is contained in some repository
named in the package path (XDCPATH):
var Pkg = xdc.useModule('xdc.bld.PackageContents');
Pkg.uses = ["ti/bios/include", "ti/xdais/legacy"];
config PackageContents.version // module-wide |
|
The package version string
XDCscript usage |
meta-domain |
PackageContents.version = String undefined;
READONLY
This parameter is a version string that comes from the
package.xdc specification.
PackageContents.addExecutable( ) // module-wide |
|
Add specified executable to this package
XDCscript usage |
meta-domain |
ARGUMENTS
name
executable base name; this name is used to create
the file name of the output executable and has the
form:
where
<suffix> is the suffix specified by
the target argument below.
See NOTE in
xdc.bld for filename rules.
target
target (xdc.bld.ITarget) for each built
object linked into the executable.
platform
string name of the platform; this is the name of a
platform package
DETAILS
The name of the executable file is
<name>.x<target_suffix>,
where
<name> is the name parameter (which may contain a directory
prefix) and
<target_suffix> is the suffix specified by the target
parameter (
xdc.bld.ITarget.suffix).
This name is also used to create a sub-directory in the package's
"cfgDir" directory (
xdc.bld.PackageContents.cfgDir) to
contain files generated for the benefit of creating the executable.
Thus, the name parameter names *both* an executable file and a
sub-directory (in
PackageContents.cfgDir) that contains the objects
linked into the executable.
When the executable is added to the package, a
xdc.bld.Test
is implicitly added to the executable; thus, every executable has at
least one
Test. Attributes for this test can be specified via
exeAttrs.
RETURNS
Returns the
xdc.bld.Executable instance
object created.
THROWS
XDCException exceptions are thrown for fatal
errors. The following error codes are
reported in the exception message:
- xdc.bld.INVALID_TARGET
-
This error is reported when a package is being
built for an unknown target. Ensure that the
correct targets are mentioned in the package's
build script.
- xdc.bld.EXECUTABLE_EXISTS
-
This error is reported when a package's build
script specifies multiple executables with the
same name. Ensure that the names of the
executables to be built are unique.
- xdc.bld.PARAMETER_MISMATCH
-
This error is reported whenever parameters with
the wrong type are passed to the method. Ensure
that the parameters passed have the right type.
PackageContents.addLibrary( ) // module-wide |
|
Add specified library to this package
XDCscript usage |
meta-domain |
ARGUMENTS
name
library base name; this name is used to create
*both* an archive and a sub-directory in the
package's "libDir" directory which
will contain the target-specific object files.
See NOTE in xdc.bld for filename rules.
target
target (a module implementing the
xdc.bld.ITarget interface) for each built
object in the library
DETAILS
The name of the library archive file is
<name>.a<target_suffix>,
where
<name> is the name parameter (which may contain a directory
prefix) and
<target_suffix> is the suffix specified by the target
parameter (
xdc.bld.ITarget.suffix).
The individual objects of each library are located in the directory
<libDir>/<name>, where
<name> is the name parameter and
<libDir>
is the configurable parameter
xdc.bld.PackageContents.libDir.
Thus, the name parameter names *both* an archive file and a
sub-directory (in
PackageContents.libDir) that contains the objects
in the archive.
RETURNS
Returns the
xdc.bld.Library instance
object created.
THROWS
XDCException exceptions are thrown for fatal
errors. The following error codes are
reported in the exception message:
- xdc.bld.INVALID_TARGET
-
This error is reported when a package is being
built for an unknown target. Ensure that the
correct targets are mentioned in the package's
build script.
- xdc.bld.LIBRARY_EXISTS
-
This error is reported when a package's build
script specifies multiple libraries with the
same name. Ensure that the names of the
libraries to be built are unique.
- xdc.bld.PARAMETER_MISMATCH
-
This error is reported whenever parameters with
the wrong type are passed to the method. Ensure
that the parameters passed have the right type.
SEE
PackageContents.addRelease( ) // module-wide |
|
Add specified release to this package
XDCscript usage |
meta-domain |
ARGUMENTS
name
release base name; this name is used to create
the file name of the output file and has the
form:
<name>.tar
See NOTE in xdc.bld for filename rules.
RETURNS
Returns the
xdc.bld.Release instance object
created.
THROWS
XDCException exceptions are thrown for fatal
errors. The following error codes are
reported in the exception message:
- xdc.bld.RELEASE_EXISTS
-
This error is reported whenever a package's build
script specifies multiple releases with the same
name. Ensure that the names of the releases
specified in the build script are unique.
- xdc.bld.INVALID_RELEASE_PREFIX
-
This error is reported whenever a release prefix
is specified by its absolute path in the package's
build script. The release prefix has to be
relative to the package's base directory.
- xdc.bld.INVALID_RELEASE_NAME
-
This error is reported whenever a release name is
specified by its absolute path in the package's
build script. The release name has to be relative
to the package's base directory.
PackageContents.addRepository( ) // module-wide |
|
Add a repository to this package
XDCscript usage |
meta-domain |
ARGUMENTS
DETAILS
A repository is a directory that contains packages. Repositories are
typically named in the user's XDCPATH environment variable and contain
a set of packages that are managed as a group.
This method allows one to bundle several packages together into a
single release (of the package that contains this repository).
RETURNS
Returns the
xdc.bld.Repository
instance object created.
THROWS
XDCException exceptions are thrown for fatal
errors. The following error codes are
reported in the exception message:
- xdc.bld.REPOSITORY_EXISTS
-
This error is reported whenever a package's build
script specifies multiple repositories with the
same name. Ensure that the names of the
repositories specified in the build script are
unique.
PackageContents.addScript( ) // module-wide |
|
Add a script to this package
XDCscript usage |
meta-domain |
ARGUMENTS
name
name of the script to add to this package. Script
names are simply the script's filename relative to
the package's base directory. Scripts can have any
extension, but if the extension is ".sh" or ".ksh"
a Korn shell compatible shell is used to run the
script's tests; otherwise it is assumed to be an
XDCscript file and any tests will be run by the
XDCscript interpreter xs.
DETAILS
Both XDCscript and Korn shell scripts can be added to package. This
not only allows one to add script utilities to a package, it
also makes it easy to create scripted regression tests. As with
Executables, it is possible to add
xdc.bld.Tests to a
Script; see
xdc.bld.Script.addTest.
RETURNS
Returns the
xdc.bld.Script instance
object created.
THROWS
XDCException exceptions are thrown for fatal
errors. The following error codes are
reported in the exception message:
- xdc.bld.SCRIPT_EXISTS
-
This error is reported whenever a package's build
script specifies multiple user scripts with the
same name. Ensure that the names of the user
scripts are unique.