![]() |
![]() |
Collaboration diagram for DREC:
Data Fields | |
uint | Type |
Type of socket. For V4 this could be SOCK_STREAM, SOCK_STREAMNC, SOCK_DGRAM But for V6 this can only be SOCK_STREAM and SOCK_DGRAM. | |
IPN | LocalAddress |
Local V4 Address to which the socket is bound to For most cases this is passed as INADDR_ANY. | |
IP6N | LocalV6Address |
Local V6 address to which the socket is bound to For most cases this is passed as IPV6_UNSPECIFIED_ADDRESS. | |
uint | LocalPort |
Local Port to which the daemon will be bound to This cannot be NULL. | |
int(* | pCb )(SOCKET, UINT32) |
Call back function which is invoked when data is received on the registered daemon. | |
uint | Priority |
Priority of the child task. | |
uint | StackSize |
Stack size of the child task. | |
UINT32 | Argument |
Argument which is to passed to the call back routine. | |
uint | MaxSpawn |
Maximum number of tasks which can be spawned to handle the daemon. | |
SOCKET | s |
Internal socket created by the daemon for use. | |
uint | TasksSpawned |
Number of tasks spawned to handle the daemon. | |
_child * | pC |
Pointer to children. |