![]() |
![]() |
Functions | |
uint | VLANReceivePacket (PBM_Handle hPkt) |
int | VLANAddDevice (uint index, UINT16 vlan_id, UINT8 default_priority, UINT8 prio_mapping[MAX_PRIO_VAL]) |
int | VLANDelDevice (UINT16 dev_index) |
void | VLANInit (void) |
void | VLANDeinit (void) |
int VLANAddDevice | ( | uint | index, | |
UINT16 | vlan_id, | |||
UINT8 | default_priority, | |||
UINT8 | prio_mapping[MAX_PRIO_VAL] | |||
) |
Description
The API is available to user applications to be able to create a VLAN virtual device on a source interface
[in] | index | Source Interface Index on which the VLAN device is created |
[in] | vlan_id | VLAN Identifier associated with the VLAN device |
[in] | default_priority | Default User Priority configured in the VLAN packet if no packet priority is defined. |
[in] | prio_mapping | The mapping which maps the packet priority to the VLAN user priority which is a part of the VLAN header. |
Index | of the new VLAN device - Success | |
<0 | - Error |
void VLANDeinit | ( | void | ) |
Description
The function is used to deinitialize the VLAN module. The function is called to close and shutdown all the VLAN enabled NIMU Network Interface objects which exist in the System
This is for *internal* NDK Stack Usage.
Not | Applicable. |
int VLANDelDevice | ( | UINT16 | dev_index | ) |
Description
The API is available to user applications to be able to delete a previously created VLAN device.
[in] | dev_index | Index of the VLAN NIMU Interface Object which is to be deleted. This should be the same as the returned value from VLANAddDevice. |
0 | - Success | |
<0 | - Error |
void VLANInit | ( | void | ) |
Description
The function is used to initialize the VLAN module in the NDK core stack
This is for *internal* NDK Stack Usage.
Not | Applicable. |
uint VLANReceivePacket | ( | PBM_Handle | hPkt | ) |
Description
The function is called by the NIMU Receive function when a VLAN packet is received. The function validates the packet and ensures that there is a valid VLAN node on the system which can process the packet.
This is for *internal* NDK Stack Usage.
[in] | hPkt | Handle to the packet which needs to be sent |
Encapsulated | Protocol - Success | |
0xFFFF | - Error |