![]() |
![]() |
#include <udpif.h>
Data Fields | |
UINT32 | RcvTotal |
Total UDP datagrams received. | |
UINT32 | RcvShort |
Number UDP packets received with length shorter than UDP header length. | |
UINT32 | RcvBadLen |
Number of UDP packets received with length larger than the packet size. | |
UINT32 | RcvBadSum |
Number of UDP packets received with checksum errs. | |
UINT32 | RcvFull |
Number of UDP Packets dropped because of the receiver socket queue being full. | |
UINT32 | RcvNoPort |
Number of UDP packets received that are destined to a port on the host on which there exists no listening socket/application. | |
UINT32 | RcvNoPortB |
Number of UDP multicast/broadcast packets received that are destined to a port on the host stack on which there exists no listening socket/application. | |
UINT32 | SndTotal |
Total UDP packets sent. | |
UINT32 | SndNoPacket |
Packets dropped because of memory allocation problems. |
This structure is used to hold various stats and counters by the UDP module. A separate copy of this stats is maintained by the IPv4 and IPv6 stacks.