![]() |
![]() |
Data Structures | |
struct | ICMPV6STATS |
The structure describes the ICMPv6 Statistics Block. More... | |
Functions | |
_extern void | ICMPv6Init (void) |
_extern int | ICMPv6RxPacket (PBM_Pkt *pPkt, IPV6HDR *ptr_ipv6hdr) |
_extern int | ICMPv6RecvNS (PBM_Pkt *pPkt, IPV6HDR *ptr_ipv6hdr) |
_extern int | ICMPv6RecvNA (PBM_Pkt *pPkt, IPV6HDR *ptr_ipv6hdr) |
_extern int | ICMPv6RecvRA (PBM_Pkt *pPkt, IPV6HDR *ptr_ipv6hdr) |
_extern int | ICMPv6RecvRedirect (PBM_Pkt *pPkt, IPV6HDR *ptr_ipv6hdr) |
_extern int | ICMPv6RecvRS (PBM_Pkt *pPkt, IPV6HDR *ptr_ipv6hdr) |
_extern int | ICMPv6SendDstUnreachable (UINT8 Code, PBM_Pkt *pOrgPkt) |
_extern int | ICMPv6SendTimeExceeded (UINT8 Code, PBM_Pkt *pOrgPkt) |
_extern int | ICMPv6SendParameterProblem (UINT8 Code, PBM_Pkt *pOrgPkt, UINT32 Pointer) |
_extern int | ICMPv6SendNS (NETIF_DEVICE *ptr_device, IP6N DstAddress, IP6N SrcAddress, IP6N TargetAddress) |
_extern int | ICMPv6SendNA (NETIF_DEVICE *ptr_device, IP6N DstAddress, IP6N SrcAddress, IP6N TargetAddress, UINT8 Flags) |
_extern int | ICMPv6SendRS (NETIF_DEVICE *ptr_device, IP6N SrcAddress) |
_extern void ICMPv6Init | ( | void | ) |
Description
The function is used to initialize the ICMPv6 Protocol stack.
This is for *internal* NDK Stack Usage.
Not | Applicable. |
_extern int ICMPv6RecvNA | ( | PBM_Pkt * | pPkt, | |
IPV6HDR * | ptr_ipv6hdr | |||
) |
Description
The function handles the ICMPv6 Neighbour Advertisment Message
[in] | pPkt | Pointer to the entire ICMPv6 Packet. |
[in] | ptr_ipv6hdr | Pointer to the IPv6 Header. |
0 | - Success | |
<0 | - Error |
_extern int ICMPv6RecvNS | ( | PBM_Pkt * | pPkt, | |
IPV6HDR * | ptr_ipv6hdr | |||
) |
Description
The function handles the ICMPv6 Neighbour Solicitation Message
[in] | pPkt | Pointer to the entire ICMPv6 Packet. |
[in] | ptr_ipv6hdr | Pointer to the IPv6 Header. |
0 | - Success | |
<0 | - Error |
_extern int ICMPv6RecvRA | ( | PBM_Pkt * | pPkt, | |
IPV6HDR * | ptr_ipv6hdr | |||
) |
Description
The function handles the ICMPv6 Router Advertisment Message
[in] | pPkt | Pointer to the entire ICMPv6 Packet. |
[in] | ptr_ipv6hdr | Pointer to the IPv6 Header. |
0 | - Success | |
<0 | - Error |
_extern int ICMPv6RecvRedirect | ( | PBM_Pkt * | pPkt, | |
IPV6HDR * | ptr_ipv6hdr | |||
) |
Description
The function handles the ICMPv6 Redirect Message
[in] | pPkt | Pointer to the entire ICMPv6 Packet. |
[in] | ptr_ipv6hdr | Pointer to the IPv6 Header. |
0 | - Success | |
<0 | - Error |
_extern int ICMPv6RecvRS | ( | PBM_Pkt * | pPkt, | |
IPV6HDR * | ptr_ipv6hdr | |||
) |
Description
The function handles the ICMPv6 Router Solicitation Message
[in] | pPkt | Pointer to the entire ICMPv6 Packet. |
[in] | ptr_ipv6hdr | Pointer to the IPv6 Header. |
0 | - Success | |
<0 | - Error |
_extern int ICMPv6RxPacket | ( | PBM_Pkt * | pPkt, | |
IPV6HDR * | ptr_ipv6hdr | |||
) |
Description
The function handles the ICMPv6 Packets.
[in] | pPkt | Pointer to the entire ICMPv6 Packet. |
[in] | ptr_ipv6hdr | Pointer to the IPv6 Header. |
Not | Applicable. |
_extern int ICMPv6SendDstUnreachable | ( | UINT8 | Code, | |
PBM_Pkt * | pOrgPkt | |||
) |
Description
The function sends a destination unreachable message. The function accepts Code as a parameter and can be used to send different messages.
[in] | Code | Code to be added to the ICMPv6 Destination Unreachable message Valid Values range from 0 - 4 as specified in RFC 2463. |
[in] | pOrgPkt | The offending packet which causes the packet to be sent out. |
0 | - Success | |
<0 | - Error |
_extern int ICMPv6SendNA | ( | NETIF_DEVICE * | ptr_device, | |
IP6N | DstAddress, | |||
IP6N | SrcAddress, | |||
IP6N | TargetAddress, | |||
UINT8 | Flags | |||
) |
Description
The function is used to send out a Neighbor Advertisment.
This is for *internal* NDK Stack Usage.
[in] | ptr_device | The Network Interface object on which the packet is to be transmitted. |
[in] | DstAddress | The destination address to which the NA packet is directed too. |
[in] | SrcAddress | The Source address of the interface |
[in] | TargetAddress | The Target address to which the NA message is being transmitted. |
[in] | Flags | The value of the (R)eserved, (S)olicited and (O)verride flags. |
0 | - Success | |
<0 | - Error |
_extern int ICMPv6SendNS | ( | NETIF_DEVICE * | ptr_device, | |
IP6N | DstAddress, | |||
IP6N | SrcAddress, | |||
IP6N | TargetAddress | |||
) |
Description
The function is used to send out a Neighbor solicitation
This is for *internal* NDK Stack Usage.
[in] | ptr_device | The Network Interface object on which the packet is to be transmitted. |
[in] | DstAddress | The destination address to which the NS packet is directed too. As per RFC 2461; this can either be the Solicted Node Multicast Address or the the target address. |
[in] | SrcAddress | The Source address of the interface; this can either be UNSPECIFIED i.e. :: if the NS is being sent for DAD or it will be the address of the source interface. |
[in] | TargetAddress | The Target address to which the NS message is being transmitted. |
0 | - Success | |
<0 | - Error |
_extern int ICMPv6SendParameterProblem | ( | UINT8 | Code, | |
PBM_Pkt * | pOrgPkt, | |||
UINT32 | Pointer | |||
) |
Description
The function sends the Parameter Problem message. The function accepts Code as a parameter and can be used to send different messages.
[in] | Code | Code to be added to the ICMPv6 Time Exceeded message Valid Values range from 0 - 2 as specified in RFC 2463. |
[in] | pOrgPkt | The offending packet which causes the packet to be sent out. |
[in] | Pointer | Identifies the Code Offset within the packet where the error occurred. |
0 | - Success | |
<0 | - Error |
_extern int ICMPv6SendRS | ( | NETIF_DEVICE * | ptr_device, | |
IP6N | SrcAddress | |||
) |
Description
The function is used to send out a Router solicitation. All RS messages are sent to the ALL_ROUTER Destination Address.
This is for *internal* NDK Stack Usage.
[in] | ptr_device | The Network Interface object on which the packet is to be transmitted. |
[in] | SrcAddress | The Source address of the interface; this could be set to the UNSPECIFIED address. If the Source address is UNSPECIFIED; the function does not append the SOURCE_LL Option to the RS packet. |
0 | - Success | |
<0 | - Error |
_extern int ICMPv6SendTimeExceeded | ( | UINT8 | Code, | |
PBM_Pkt * | pOrgPkt | |||
) |
Description
The function sends a Time Exceeded message. The function accepts Code as a parameter and can be used to send different messages.
[in] | Code | Code to be added to the ICMPv6 Time Exceeded message Valid Values range from 0 - 1 as specified in RFC 2463. |
[in] | pOrgPkt | The offending packet which causes the packet to be sent out. |
0 | - Success | |
<0 | - Error |