![]() |
![]() |
Functions | |
int | TCP6PrAttach (HANDLE h, HANDLE *phTcp) |
int | TCP6PrListen (HANDLE h, HANDLE hTcp) |
void | TCP6PrInherit (HANDLE hParent, HANDLE hTcpParent, HANDLE hChild, HANDLE hTcpChild) |
uint | TCP6ValidateMetrics (TCPPROT *pt, uint rcvmss) |
void | TCP6Close (TCPPROT *pt) |
void | TCP6Drop (TCPPROT *pt, int Error) |
int | TCP6PrDetach (HANDLE hSock, HANDLE *phTcp, int fatal) |
int | TCP6PrConnect (HANDLE h, HANDLE hTcp) |
int | TCP6PrDisconnect (HANDLE hSock, HANDLE hTcp) |
int | TCP6PrRecv (HANDLE h, HANDLE hTcp) |
int | TCP6PrSend (HANDLE h, HANDLE hTcp, UINT8 *pBuf, INT32 Size, INT32 *pRetSize) |
int | TCP6PrSendOOB (HANDLE h, HANDLE hTcp, UINT8 *pBuf, INT32 Size, INT32 *pRetSize) |
uint | TCP6PrGetState (HANDLE hParent, HANDLE hTcp) |
void | TCP6PrCtlError (HANDLE h, HANDLE hTcp, uint Code, int Error) |
int | TCP6PrSetOption (HANDLE h, HANDLE hTcp, int Prop, void *pBuf, int size) |
int | TCP6PrGetOption (HANDLE h, HANDLE hTcp, int Prop, void *pBuf, int *psize) |
void TCP6Close | ( | TCPPROT * | pt | ) |
Description
The function is called to close down the TCP Protocol block.
[in] | pt | Pointer to the TCP Protocol Information block. |
Not | Applicable. |
void TCP6Drop | ( | TCPPROT * | pt, | |
int | Error | |||
) |
Description
The function drops a TCP side "socket" with ABORT
[in] | pt | Handle to the TCP protocol information |
[in] | Error | Error Code. |
Not | applicable. |
int TCP6PrAttach | ( | HANDLE | h, | |
HANDLE * | phTcp | |||
) |
Description
The function is used to create a new TCP socket and is called from the SOCK6 module.
[in] | h | Handle to the socket being created. |
[out] | phTcp | The TCP Protocol information which is populated. |
Success | - 0 | |
Error | - Non Zero |
int TCP6PrConnect | ( | HANDLE | h, | |
HANDLE | hTcp | |||
) |
Description
The function requests a connection for a TCP6 socket.
[in] | h | Handle to the socket. |
[in] | hTcp | Handle to the TCP Protocol Information block. |
Always | returns 0. |
void TCP6PrCtlError | ( | HANDLE | h, | |
HANDLE | hTcp, | |||
uint | Code, | |||
int | Error | |||
) |
Description
The function is called to indicate there is an error detected by the reception of an error ICMPv6 packet.
[in] | h | Handle to the socket. |
[in] | hTcp | Handle to the TCP Protocol Information block. |
[in] | Code | Obsolete |
[in] | Error | Error Code. |
Not | Applicable |
int TCP6PrDetach | ( | HANDLE | hSock, | |
HANDLE * | phTcp, | |||
int | fatal | |||
) |
Description
The function closes the TCP side "socket", detaches and free resources
[in] | hSock | Handle to the socket. |
[in] | phTcp | Handle to the TCP Protocol Information block. |
[in] | fatal | Status flag which if set to 1 indicates that the socket should be closed immediately and if set to 0 indicates that the TCP close state machine is invoked. |
Always | returns 0. |
int TCP6PrDisconnect | ( | HANDLE | hSock, | |
HANDLE | hTcp | |||
) |
Description
The function disconnects a TCP side "socket" - performs "half close"
[in] | hSock | Handle to the socket. |
[in] | hTcp | Handle to the TCP Protocol Information block. |
Always | returns 0. |
int TCP6PrGetOption | ( | HANDLE | h, | |
HANDLE | hTcp, | |||
int | Prop, | |||
void * | pBuf, | |||
int * | psize | |||
) |
Description
The function is used to get the TCP options.
[in] | h | Handle to the socket. |
[in] | hTcp | Handle to the TCP Protocol Information block. |
[in] | Prop | The Property which needs to be configured. |
[out] | pBuf | Data buffer where the value of property will be copied. |
[out] | psize | Size of the Data buffer |
Success | - 0 | |
Error | - Non Zero |
uint TCP6PrGetState | ( | HANDLE | hParent, | |
HANDLE | hTcp | |||
) |
Description
The function returns the TCP State
[in] | hParent | Handle to the socket. |
[in] | hTcp | Handle to the TCP Protocol Information Block. |
TCP | State |
void TCP6PrInherit | ( | HANDLE | hParent, | |
HANDLE | hTcpParent, | |||
HANDLE | hChild, | |||
HANDLE | hTcpChild | |||
) |
Description
The function is called to inherit TCP protocol properties from parent to child.
[in] | hParent | Handle to the parent socket. |
[in] | hTcpParent | Handle to the parent TCP protocol information |
[in] | hChild | Handle to the child socket. |
[in] | hTcpChild | Handle to the child TCP protocol information |
Not | Applicable |
int TCP6PrListen | ( | HANDLE | h, | |
HANDLE | hTcp | |||
) |
Description
The function is called by the SOCKET Layer to indicate that the socket has been marked as LISTENING. This internally implies that the socket can no longer be used for data reception and transmission so the function clears the internal protocol resources.
[in] | h | Handle to the socket |
[in] | hTcp | Handle to the TCP protocol information |
Always | returns 0. |
int TCP6PrRecv | ( | HANDLE | h, | |
HANDLE | hTcp | |||
) |
Description
The function deals with Rx data being removed from buffer
[in] | h | Handle to the socket. |
[in] | hTcp | Handle to the TCP Protocol Information block. |
Always | returns 0. |
int TCP6PrSend | ( | HANDLE | h, | |
HANDLE | hTcp, | |||
UINT8 * | pBuf, | |||
INT32 | Size, | |||
INT32 * | pRetSize | |||
) |
Description
The function sends data
[in] | h | Handle to the socket. |
[in] | hTcp | Handle to the TCP Protocol Information block. |
[in] | pBuf | Pointer to the data Buffer to be transmitted. |
[in] | Size | Size of the data buffer. |
[out] | pRetSize | Number of bytes sent out. |
Always | returns 0. |
int TCP6PrSendOOB | ( | HANDLE | h, | |
HANDLE | hTcp, | |||
UINT8 * | pBuf, | |||
INT32 | Size, | |||
INT32 * | pRetSize | |||
) |
Description
The function sends OOB data
[in] | h | Handle to the socket. |
[in] | hTcp | Handle to the TCP Protocol Information block. |
[in] | pBuf | Pointer to the data Buffer to be transmitted. |
[in] | Size | Size of the data buffer. |
[out] | pRetSize | Number of bytes sent out. |
Always | returns 0. |
int TCP6PrSetOption | ( | HANDLE | h, | |
HANDLE | hTcp, | |||
int | Prop, | |||
void * | pBuf, | |||
int | size | |||
) |
Description
The function is used to set the TCP options.
[in] | h | Handle to the socket. |
[in] | hTcp | Handle to the TCP Protocol Information block. |
[in] | Prop | The Property which needs to be configured. |
[in] | pBuf | Data buffer where the value of property is present |
[in] | size | Size of the Data buffer |
Success | - 0 | |
Error | - Non Zero |
uint TCP6ValidateMetrics | ( | TCPPROT * | pt, | |
uint | rcvmss | |||
) |
Description
The function is called to update the TCP Information based on the socket route.
[in] | pt | Handle to the TCP protocol information |
[in] | rcvmss | Received MSS. |
Current | MSS to advertise. |