![]() |
![]() |
Functions | |
void | IGMPLeaveHostGroup (IPN IpAddr, uint IfIdx) |
int | IGMPJoin (HANDLE hSock, struct ip_mreq *ptr_ipmreq) |
int | IGMPLeave (HANDLE hSock, struct ip_mreq *ptr_ipmreq) |
int IGMPJoin | ( | HANDLE | hSock, | |
struct ip_mreq * | ptr_ipmreq | |||
) |
Description
The function is called from the setsockopt to join a multicast group. This function was added to make the IGMP Join behavior similar to the standard 'socket' interface via the IP_ADD_MEMBERSHIP socket option.
[in] | hSock | Handle to the socket on which the multicast group is being joined. |
[in] | ptr_ipmreq | Multicast Request structure populated by the application which contains the Multicast group address and the address of the interface on which the group is being joined. |
0 | - Success | |
Non | Zero - Error |
int IGMPLeave | ( | HANDLE | hSock, | |
struct ip_mreq * | ptr_ipmreq | |||
) |
Description
The function is called from the setsockopt to leave a multicast group. This function was added to make the IGMP Leave behavior similar to the standard 'socket' interface via the IP_DROP_MEMBERSHIP socket option.
[in] | hSock | Handle to the socket on which the multicast group is leaving. |
[in] | ptr_ipmreq | Multicast Request structure populated by the application which contains the Multicast group address and the address of the interface on which the group will be left. |
0 | - Success | |
Non | Zero - Error |
void IGMPLeaveHostGroup | ( | IPN | IpAddr, | |
uint | IfIdx | |||
) |
Description
The function is called to LEAVE a multicast group on the specific interface. The function leaves the multicast group on the interface list and kicks the IGMP membership state machine to send out the LEAVE reports.
This is the OLD API which was used to LEAVE multicast groups but has now been obsoleted. Users are advised to use the well defined setsockopt with the IP_DROP_MEMBERSHIP to acheive the needful.
This function is now called only from *kernel* context
[in] | IpAddr | Multicast group IP address which is being joined. |
[in] | IfIdx | Interface Index on which the group is being joined. |
Not | Applicable. |