NDK  2.23.01.01
 All Files Functions Pages
Functions
sntp.h File Reference

Detailed Description

This is a 'beta' release of SNTP client.

The SNTP client uses the Network Time Protocol (NTP) to provide a continuous service of maintaining system time by periodically sychronizing with one or more NTP servers.

To implement the SNTP client service, the user is required to provide two system time keeping functions, as well as a list of NTP server IP addresses.

The time keeping functions are called by the SNTP client in order to get or set the current time in the system ("gettime" and "settime"). For example, these could be APIs which set or get the value of a Real Time Clock (RTC). The "gettime" and "settime" functions should have the following format and should be passed into the SNTP_start() function:

uint32_t (*GetTimeFxn)(void);
void (*SetTimeFxn)(uint32_t newtime);

The "gettime" function should return the number of seconds since the Epoch (January 1, 1970). The "settime" function sets the time to the value that is passed to it. The SNTP client uses the "gettime" function to write the current system time into a request to an NTP server. The "settime" function is used to set the system time to a new value received from the NTP server. The SNTP client handles the conversion of NTP time (time since Janary 1, 1900) to the local system's time (number of seconds since January 1, 1970).

The list of NTP servers should consist of socket address structures which contain the unicast addresses of the servers (as well as some additional information). Both IPv4 and IPv6 unicast server addresses are supported (host names are not supported). Structures of type 'struct sockaddr_in' must be used for IPv4 server addresses and of type 'struct sockaddr_in6' for IPv6 server addresses. These structures must be written to a contiguous block of memory and then passed to the SNTP_setservers() function.

The SNTP client may be stopped by calling SNTP_stop(). Calling this function will cause the SNTP client Task to exit and all of the resources used by it to be freed.

Example Usage

The SNTP module is part of the NDK nettools library. An application should include its header file as follows:

Setting The Time Functions And Starting The SNTP Client Service

The SNTP client should be initialized by calling the SNTP_start() function. Pointers to the set and get time functions should be passed as arguments, as well as the stack size to be used for the client Task, if desired. The following example code passes pointers to some existing time functions 'gettime' and 'settime'. A value of 0 is passed as the last argument, which specifies that the default stack size for the SNTP client Task should be used:

SNTP_start(gettime, settime, 0);

Initializing The List Of Servers Using Socket Address Structures

The server list should be initialized and passed to the SNTP module via the SNTP_setservers() API. The following code uses socket address structs to store the IPv4 and IPv6 addresses of some (imaginary) NTP servers. Note that in addition to the addresses, it is necessary to set the size of the address structure, as this is required by the SNTP module to cycle through the server list. The family, port, and scope ID (for IPv6 only) must also be correctly set:

#include <ti/ndk/inc/netmain.h>
#include <ti/ndk/inc/_stack.h>
struct sockaddr_in ipv4addr;
struct sockaddr_in6 ipv6addr;
ipv4addr.sin_len = sizeof(struct sockaddr_in);
ipv4addr.sin_family = AF_INET;
ipv4addr.sin_port = htons(123);
ipv4addr.sin_addr.s_addr = inet_addr("192.168.1.100");
ipv6addr.sin6_len = sizeof(struct sockaddr_in6);
ipv6addr.sin6_family = AF_INET6;
ipv6addr.sin6_port = htons(123);
IPv6StringToIPAddress("fe80::dbff:b21b:fe78:20b",
(IP6N *)&ipv6addr.sin6_addr);
ipv6addr.sin6_scope_id = 1;

Storing The Server List In A Contiguous Block Of Memory

Once the address structures are properly initialized, they need to be written into a contiguous block of memory. This can be done copying the address structures into a byte array:

#define SIZE (sizeof(struct sockaddr_in) + sizeof(struct sockaddr_in6))
unsigned char ntpServers[SIZE];
int currPos = 0;
memcpy((ntpServers + currPos), &ipv4addr, sizeof(struct sockaddr_in));
currPos += sizeof(struct sockaddr_in);
memcpy((ntpServers + currPos), &ipv6addr, sizeof(struct sockaddr_in6));
currPos += sizeof(struct sockaddr_in6);

Passing The Server List To The SNTP Module

To set the list of NTP servers, call SNTP_setservers(), passing the server list and the number of servers in the list as arguments. Note that the server list is cast to the generic type of 'struct sockaddr *':

SNTP_setservers((struct sockaddr *)ntpServers, 2);

Stopping The SNTP Client Service

To stop the SNTP client, the SNTP_stop() function is called:


#include <xdc/std.h>
Include dependency graph for sntp.h:

Go to the source code of this file.

Functions

int SNTP_start (uint32_t(*get)(void), void(*set)(uint32_t newtime), size_t stacksize)
 Initialize and start the SNTP client Task.
void SNTP_stop (void)
 Stops the SNTP client Task and frees resources used by the module.
void SNTP_setservers (struct sockaddr *servers, unsigned int numservers)
 Initializes or updates the list of NTP servers to communicate with.

Function Documentation

int SNTP_start ( uint32_t(*)(void)  get,
void(*)(uint32_t newtime)  set,
size_t  stacksize 
)

Initialize and start the SNTP client Task.

Called to create and start SNTP client Task and Semaphores. User must pass in pointers to functions for getting and setting the current time.

The SNTP client Task's stacksize is configurable via the stacksize parameter.

Passing a value of 0 for the stack parameter causes the Task to be created with a default value. Passing a value > 0 causes the Task to be created using that value for the stack size. When a value > 0 is passed, it is the application developer's responsiblity to choose an appropriate stack size. If this is not done, stack overflow or other undesirable behavior may occur.

The priority of SNTP_synctime is set to 1 and is not configurable.

Parameters:
getA pointer to a function that returns the number of seconds since January 1, 1970
setA pointer to a function that sets the time to the supplied value
stacksizeStack size to use for the SNTP client Task. Passing a value of 0 allows a default to be used.
Returns:
0 on failure and 1 on success
void SNTP_stop ( void  )

Stops the SNTP client Task and frees resources used by the module.

void SNTP_setservers ( struct sockaddr *  servers,
unsigned int  numservers 
)

Initializes or updates the list of NTP servers to communicate with.

Must call SNTP_start() first. This function is used to set the list of NTP servers initially, or to update the list of servers at a later point in the application run.

Parameters:
serversA pointer to a contiguous block of memory which contains a list of sockaddr_in and/or sockaddr_in6 structures
numserversThe number of servers (structs) contained in the server list
Copyright 2013, Texas Instruments Incorporated