TI-RTOS Drivers
tidrivers_cc13xx_cc26xx_2_16_01_13
|
CCamera_Config | Camera Global configuration |
CCamera_FxnTable | The definition of a Camera function table that contains the required set of functions to control a specific Camera driver implementation |
CCamera_Params | Camera Parameters |
CClockP_FreqHz | Frequency-in-hertz struct |
CClockP_Params | Basic ClockP Parameters |
CCryptoCC26XX_AESCCM_Transaction | CryptoCC26XX AES-CCM Transaction |
CCryptoCC26XX_AESECB_Transaction | CryptoCC26XX AES-ECB Transaction |
CCryptoCC26XX_Config | CryptoCC26XX Global Configuration |
CCryptoCC26XX_HWAttrs | CryptoCC26XX Hardware Attributes |
CCryptoCC26XX_Object | CryptoCC26XX Object |
CCryptoCC26XX_Params | CryptoCC26XX Parameters |
CCryptoCC26XX_Transaction | CryptoCC26XX Transaction |
CDIR | |
Cdiskio_fxns | |
CDisplay_Config | Display Global configuration |
CDisplay_FxnTable | The definition of a Display function table that contains the required set of functions to control a specific Display driver implementation |
CDisplay_Params | Display Parameters |
CDisplayDogm1286_HWAttrs | |
CDisplayDogm1286_Object | |
CDisplayGrLib_Object | |
CDisplayLog_Object | |
CDisplaySharp_HWAttrs | |
CDisplaySharp_Object | |
CDisplaySharpColor_t | Foreground and background color struct, compatible with GrLib |
CDisplayUart_HWAttrs | |
CDisplayUart_Object | |
CEMAC_Config | EMAC Global configuration |
CEMAC_FxnTable | EMAC Function table structure |
CExtFlashInfo_t | |
CFATFS | |
CFIL | |
CFILINFO | |
CGPIOCC26XX_Config | GPIO device specific driver configuration structure |
CHwiP_Params | Basic HwiP Parameters |
CI2C_Config | I2C Global configuration |
CI2C_FxnTable | The definition of a I2C function table that contains the required set of functions to control a specific I2C driver implementation |
CI2C_Params | I2C Parameters |
CI2C_Transaction | I2C transaction |
CI2CCC26XX_HWAttrsV1 | I2CCC26XX Hardware attributes |
CI2CCC26XX_I2CPinCfg | I2CCC26XX Pin Configuration |
CI2CCC26XX_Object | I2CCC26XX Object |
CI2S_BufDesc | I2S buffer descriptor for issue/reclaim mode |
CI2S_Config | I2S Global configuration |
CI2S_FxnTable | The definition of a I2S function table that contains the required set of functions to control a specific I2S driver implementation |
CI2S_Params | Basic I2S Parameters |
CLCD_Buffer | LCD_Buffer used to store data to be printed on the LCD display |
CLCD_Command | Format of LCD commands used by the LCD controller |
CLCD_Config | The LCD_Config structure contains a set of pointers used to characterize the LCD driver implementation |
CLCD_HWAttrs | LCD Hardware attributes |
CLCD_Object | LCD Object |
CLCD_Params | LCD Parameters are used to with the LCD_open() call. Default values for these parameters are set using LCD_Params_init() |
CList_Elem | |
CList_List | |
CMutexP_Params | Basic MutexP Parameters |
CNVS_Attrs | NVS attributes |
CNVS_Config | NVS Global configuration |
CNVS_FxnTable | The definition of an NVS function table that contains the required set of functions to control a specific NVS driver implementation |
CNVS_Params | NVS Parameters |
CNVSCC26XX_CmdSetCopyBlockArgs | NVSCC26XX command structure for setting copy block |
CNVSCC26XX_HWAttrs | NVSCC26XX attributes |
CNVSCC26XX_Object | |
CPDMCC26XX_BufferRequest | A PDMCC26XX_BufferRequest data structure is used with PDMCC26XX_requestBuffer() |
CPDMCC26XX_Config | The PDMCC26XX_Config structure contains a set of pointers used to characterize the PDMCC26XX driver implementation |
CPDMCC26XX_HWAttrs | PDMCC26XX Hardware attributes |
CPDMCC26XX_I2S_AudioClockConfig | PDMCC26XX_I2S Audio Clock configuration |
CPDMCC26XX_I2S_AudioFormatConfig | PDMCC26XX_I2S Hardware configuration |
CPDMCC26XX_I2S_AudioPinConfig | PDMCC26XX_I2S Audio Pin configuration |
CPDMCC26XX_I2S_BufferRelease | A PDMCC26XX_I2S_BufferRelease data structure is used with PDMCC26XX_I2S_releaseBuffer() |
CPDMCC26XX_I2S_BufferRequest | A PDMCC26XX_I2S_BufferRequest data structure is used with PDMCC26XX_I2S_requestBuffer() |
CPDMCC26XX_I2S_Config | The PDMCC26XX_I2S_Config structure contains a set of pointers used to characterize the PDMCC26XX_I2S driver implementation |
CPDMCC26XX_I2S_HWAttrs | PDMCC26XX_I2S Hardware attributes |
CPDMCC26XX_I2S_Object | PDMCC26XX_I2S Object |
CPDMCC26XX_I2S_Params | PDMCC26XX I2S Parameters are used when calling PDMCC26XX_I2S_open() |
CPDMCC26XX_I2S_StreamNotification | A PDMCC26XX_I2S_StreamNotification data structure is used with PDMCC26XX_I2S_CallbackFxn(). Provides notification about available buffers and potential errors |
CPDMCC26XX_metaData | Metadata associated with an array of PCM data |
CPDMCC26XX_Object | PDMCC26XX Object |
CPDMCC26XX_Params | PDMCC26XX Parameters are used to with the PDMCC26XX_open() call. Default values for these parameters are set using PDMCC26XX_Params_init() |
CPDMCC26XX_pcmBuffer | PCM buffer pointed to in a PDMCC26XX_BufferRequest |
CPDMCC26XX_StreamNotification | A PDMCC26XX_StreamNotification data structure is used with PDMCC26XX_CallbackFxn(). Provides notification about available buffers and potential errors |
CPIN_State_s | Underlying data structure for type PIN_State |
CPINCC26XX_HWAttrs | PINCC26XX Hardware attributes |
CPower_NotifyObj | Power notify object structure |
CPowerCC26XX_Config | Global configuration structure |
CPowerCC26XX_ModuleState | Internal module state |
CPowerCC26XX_ResourceRecord | Power resource database record format |
CPWM_Config | PWM Global configuration |
CPWM_FxnTable | The definition of a PWM function table that contains the required set of functions to control a specific PWM driver implementation |
CPWM_Params | PWM Parameters |
CPWMTimerCC26XX_HWAttrs | PWMTimerCC26XX Hardware attributes |
CPWMTimerCC26XX_Object | PWMTimerCC26XX Object |
CPWMTimerCC26XX_PWMPinCfg | PWMTimerCC26XX PWM Pin Configuration |
CRF_InfoVal | RF_getParamsVal used to input and return RF driver paramters with RF_getParams() |
CRF_Mode | Struct defining operating mode of RF driver |
CRF_Object | Struct used to store RF client state and configuration Pointer to an RF_Object is used as handles (RF_Handle) in interactions with the RF driver |
CRF_Params | RF parameter struct RF parameters are used with the RF_open() and RF_Params_init() call |
CRF_RadioSetup | Union of the different flavors of RADIO_SETUP commands |
CRFCC26XX_HWAttrs | RF Hardware attributes |
CRingBuf_Object | |
CSDSPI_Config | SDSPI Global configuration |
CSDSPI_FxnTable | The definition of a SDSPI function table that contains the required set of functions to control a specific SDSPI driver implementation |
CSDSPI_Params | SDSPI Parameters |
CSemaphoreP_Params | Basic SemaphoreP Parameters |
CSPI_Config | SPI Global configuration |
CSPI_FxnTable | The definition of a SPI function table that contains the required set of functions to control a specific SPI driver implementation |
CSPI_Params | SPI Parameters |
CSPI_Transaction | A SPI_Transaction data structure is used with SPI_transfer(). It indicates how many SPI_FrameFormat frames are sent and received from the buffers pointed to txBuf and rxBuf. The arg variable is an user-definable argument which gets passed to the SPI_CallbackFxn when the SPI driver is in SPI_MODE_CALLBACK |
CSPICC26XXDMA_HWAttrsV1 | SPICC26XXDMA Hardware attributes |
CSPICC26XXDMA_Object | SPICC26XXDMA Object |
CtContext | |
CtDisplay | This structure defines the characteristics of a display driver |
CtDisplayFxns | This structure defines the implementation of a display driver |
CtFont | This structure describes a font used for drawing text onto the screen |
CtFontEx | |
CtImage | This structure defines the characteristics of a Bitmap Image |
CtRectangle | |
CUART_Config | UART Global configuration |
CUART_FxnTable | The definition of a UART function table that contains the required set of functions to control a specific UART driver implementation |
CUART_Params | UART Parameters |
CUARTCC26XX_HWAttrsV1 | UARTCC26XX Hardware attributes |
CUARTCC26XX_Object | UARTCC26XX Object |
CUDMACC26XX_Config | UDMACC26XX Global configuration |
CUDMACC26XX_HWAttrs | UDMACC26XX hardware attributes |
CUDMACC26XX_Object | UDMACC26XX object |
CUSBMSCHFatFs_Config | USBMSCHFatFs Global configuration |
CUSBMSCHFatFs_FxnTable | The definition of a USBMSCHFatFs function table that contains the required set of functions to control a specific USBMSCHFatFs driver implementation |
CUSBMSCHFatFs_Params | USBMSCHFatFs Parameters |
CWatchdog_Config | Watchdog Global configuration |
CWatchdog_FxnTable | The definition of a Watchdog function table that contains the required set of functions to control a specific Watchdog driver implementation |
CWatchdog_Params | Watchdog Parameters |
CWiFi_Config | WiFi Global configuration |
CWiFi_FxnTable | The definition of a WiFi function table that contains the required set of functions to control a specific WiFi driver implementation |
CWiFi_Params | WiFi Parameters |