256 #ifndef ti_drivers_crypto_CryptoCC26XX__include
257 #define ti_drivers_crypto_CryptoCC26XX__include
266 #include <driverlib/crypto.h>
296 #define CRYPTOCC26XX_TIMEOUT 20
298 #define CRYPTOCC26XX_STATUS_SUCCESS 0
299 #define CRYPTOCC26XX_STATUS_ERROR -1
300 #define CRYPTOCC26XX_STATUS_UNDEFINEDCMD -2
302 #define CRYPTOCC26XX_OP_AES_CCM 0
303 #define CRYPTOCC26XX_OP_AES_CCM_NOCRYPT 1
304 #define CRYPTOCC26XX_OP_AES_CCMINV 2
305 #define CRYPTOCC26XX_OP_AES_CCMINV_NOCRYPT 3
306 #define CRYPTOCC26XX_OP_AES_ECB 4
307 #define CRYPTOCC26XX_OP_AES_ECB_NOCRYPT 5
310 #define OP_TYPE(x) ((x)&0xFE)
312 #define DO_CRYPT(x) ((x)&0x01?false:true)
318 #define ti_sysbios_family_arm_m3_Hwi__nolocalnames
319 #include <ti/sysbios/family/arm/m3/Hwi.h>
320 #include <ti/sysbios/knl/Semaphore.h>
515 ti_sysbios_family_arm_m3_Hwi_Struct
hwi;
719 #undef ti_sysbios_family_arm_m3_Hwi__nolocalnames
int CryptoCC26XX_allocateKey(CryptoCC26XX_Handle handle, CryptoCC26XX_KeyLocation keyLocation, const uint32_t *keySrc)
Function that allocates key, writes key into key store RAM and returns a handle to CryptoCC26XX Key...
CryptoCC26XX Transaction.
Definition: CryptoCC26XX.h:401
Semaphore_Struct waitSem
Definition: CryptoCC26XX.h:517
CryptoCC26XX Global Configuration.
Definition: CryptoCC26XX.h:521
CryptoCC26XX_Transaction * currentTransact
Definition: CryptoCC26XX.h:505
void CryptoCC26XX_Params_init(CryptoCC26XX_Params *params)
Function to initialize the CryptoCC26XX_Params struct to its defaults.
CryptoCC26XX AES-CCM Transaction.
Definition: CryptoCC26XX.h:413
struct CryptoCC26XX_Object CryptoCC26XX_Object
CryptoCC26XX Object.
CryptoCC26XX_Operation opType
Definition: CryptoCC26XX.h:435
int CryptoCC26XX_close(CryptoCC26XX_Handle handle)
Function to closes a given CryptoCC26XX peripheral specified by the CryptoCC26XX handle.
void * msgOut
Definition: CryptoCC26XX.h:422
struct CryptoCC26XX_AESCCM_Transaction CryptoCC26XX_AESCCM_Transaction
CryptoCC26XX AES-CCM Transaction.
CryptoCC26XX_Transaction * tailPtr
Definition: CryptoCC26XX.h:509
CryptoCC26XX Parameters.
Definition: CryptoCC26XX.h:381
uint8_t keyIndex
Definition: CryptoCC26XX.h:437
CryptoCC26XX_Operation opType
Definition: CryptoCC26XX.h:414
Definition: CryptoCC26XX.h:367
uint8_t CryptoCC26XX_Operation
CryptoCC26XX Operation Type.
Definition: CryptoCC26XX.h:357
uint8_t fieldLength
Definition: CryptoCC26XX.h:423
Definition: CryptoCC26XX.h:370
CryptoCC26XX_Operation opType
Definition: CryptoCC26XX.h:402
uint8_t data[]
Definition: CryptoCC26XX.h:404
Definition: CryptoCC26XX.h:338
CryptoCC26XX_Transaction * headPtr
Definition: CryptoCC26XX.h:508
void * msgOut
Definition: CryptoCC26XX.h:439
uint8_t keyIndex
Definition: CryptoCC26XX.h:416
char * nonce
Definition: CryptoCC26XX.h:419
struct CryptoCC26XX_Config CryptoCC26XX_Config
CryptoCC26XX Global Configuration.
void CryptoCC26XX_Transac_init(CryptoCC26XX_Transaction *trans, CryptoCC26XX_Operation opType)
Function to initialize the CryptoCC26XX_Transaction struct to its defaults.
int CryptoCC26XX_releaseKey(CryptoCC26XX_Handle handle, int *keyIndex)
Function that releases the specified CryptoCC26XX Key.
Definition: CryptoCC26XX.h:373
char * header
Definition: CryptoCC26XX.h:421
CryptoCC26XX Hardware Attributes.
Definition: CryptoCC26XX.h:473
Power_NotifyObj cryptoNotiObj
Definition: CryptoCC26XX.h:512
int openCnt
Definition: CryptoCC26XX.h:502
ti_sysbios_family_arm_m3_Hwi_Struct hwi
Definition: CryptoCC26XX.h:515
Definition: CryptoCC26XX.h:372
void const * hwAttrs
Definition: CryptoCC26XX.h:526
uint16_t headerLength
Definition: CryptoCC26XX.h:425
Definition: CryptoCC26XX.h:344
uint16_t msgInLength
Definition: CryptoCC26XX.h:424
struct CryptoCC26XX_Params CryptoCC26XX_Params
CryptoCC26XX Parameters.
struct CryptoCC26XX_Config * CryptoCC26XX_Handle
A handle that is returned from a CryptoCC26XX_open() call.
Definition: CryptoCC26XX.h:325
void * msgIn
Definition: CryptoCC26XX.h:438
Power notify object structure.
Definition: Power.h:112
uint32_t timeout
Definition: CryptoCC26XX.h:503
Definition: CryptoCC26XX.h:374
CryptoCC26XX_Mode
CryptoCC26XX Mode Settings.
Definition: CryptoCC26XX.h:333
CryptoCC26XX AES-ECB Transaction.
Definition: CryptoCC26XX.h:434
char * msgIn
Definition: CryptoCC26XX.h:420
void CryptoCC26XX_init(void)
Function to initializes bios modules needed by CryptoCC26XX module.
uint8_t intPriority
Crypto Peripheral's interrupt priority.
Definition: CryptoCC26XX.h:492
int CryptoCC26XX_transact(CryptoCC26XX_Handle handle, CryptoCC26XX_Transaction *transaction)
Function to do a Crypto operation (encryption or decryption) in blocking mode.
CryptoCC26XX_KeyStore keyStore
Definition: CryptoCC26XX.h:504
int powerMngrId
Definition: CryptoCC26XX.h:477
void * object
Definition: CryptoCC26XX.h:523
Semaphore_Struct transSem
Definition: CryptoCC26XX.h:516
Definition: CryptoCC26XX.h:375
Definition: CryptoCC26XX.h:369
uint8_t CryptoCC26XX_KeyStore
CryptoCC26XX Key.
Definition: CryptoCC26XX.h:390
CryptoCC26XX_Handle CryptoCC26XX_open(unsigned int index, bool exclusiveAccess, CryptoCC26XX_Params *params)
Function to initialize a given CryptoCC26XX peripheral specified by the particular index value...
CryptoCC26XX_Mode mode
Definition: CryptoCC26XX.h:436
CryptoCC26XX_KeyLocation
CryptoCC26XX Key Store Location.
Definition: CryptoCC26XX.h:365
int intNum
Definition: CryptoCC26XX.h:479
struct CryptoCC26XX_HWAttrs CryptoCC26XX_HWAttrs
CryptoCC26XX Hardware Attributes.
CryptoCC26XX_Mode mode
Definition: CryptoCC26XX.h:403
Definition: CryptoCC26XX.h:371
struct CryptoCC26XX_Transaction CryptoCC26XX_Transaction
CryptoCC26XX Transaction.
uint32_t timeout
Definition: CryptoCC26XX.h:382
CryptoCC26XX Object.
Definition: CryptoCC26XX.h:500
CryptoCC26XX_Mode mode
Definition: CryptoCC26XX.h:415
uint32_t baseAddr
Definition: CryptoCC26XX.h:475
struct CryptoCC26XX_AESECB_Transaction CryptoCC26XX_AESECB_Transaction
CryptoCC26XX AES-ECB Transaction.
Definition: CryptoCC26XX.h:368
int CryptoCC26XX_transactPolling(CryptoCC26XX_Handle handle, CryptoCC26XX_Transaction *transaction)
Function to do a Crypto transaction operation (encryption or decryption) in polling mode...
int CryptoCC26XX_transactCallback(CryptoCC26XX_Handle handle, CryptoCC26XX_Transaction *transaction)
Function to do a Crypto transaction operation (encryption or decryption) in callback mode...
uint8_t authLength
Definition: CryptoCC26XX.h:417
Definition: CryptoCC26XX.h:366