Defines | Typedefs | Enumerations | Functions

VICP Manager

Defines

#define VICP_VERSION   0x01000000
#define VICP_NUMRESOURCES   6

Typedefs

typedef enum VICP_Status VICP_Status
 Status codes for VICP API return values.
typedef enum VICP_ResourceType VICP_ResourceType
 Resource types to be used for all APIs.
typedef enum VICP_InterruptLine VICP_InterruptLine
 Source of VICP resource interrupt.
typedef enum VICP_InterruptType VICP_InterruptType
 Type of ARM interrupt support.

Enumerations

enum  VICP_Status {
  VICP_OK = 0,
  VICP_EFAIL,
  VICP_ENOCHANNEL,
  VICP_ENOINIT
}
 

Status codes for VICP API return values.

More...
enum  VICP_ResourceType {
  VICP_IMX0,
  VICP_IMX1,
  VICP_MJCP,
  VICP_NSF,
  VICP_HDVICP0,
  VICP_HDVICP1
}
 

Resource types to be used for all APIs.

More...
enum  VICP_InterruptLine {
  VICP_FIXED,
  VICP_FLEXIBLE
}
 

Source of VICP resource interrupt.

More...
enum  VICP_InterruptType {
  VICP_IRQ,
  VICP_FIQ
}
 

Type of ARM interrupt support.

More...

Functions

int VICP_init (void)
 VICP initialization API.
int VICP_exit (void)
 VICP finalization API.
VICP_Status VICP_register (VICP_ResourceType resource, VICP_InterruptLine intrLine, VICP_InterruptType intrType)
 Registers resource with requested interrupt type.
VICP_Status VICP_unregister (VICP_ResourceType resource)
 Frees previously requested resource.
VICP_Status VICP_wait (VICP_ResourceType resource)
 Waits for the transfer corresponding to this resource to complete.
VICP_Status VICP_done (VICP_ResourceType resource, int *done)
 Checks if the transfer corresponding to this resource is complete.

Detailed Description

This is the API for the VICP Manager.


Define Documentation

#define VICP_VERSION   0x01000000
#define VICP_NUMRESOURCES   6

Typedef Documentation

typedef enum VICP_Status VICP_Status

Status codes for VICP API return values.

Resource types to be used for all APIs.

Source of VICP resource interrupt.

Remarks:
VICP_FIXED tells the IRQ driver to use the interrupt that's dedicated for use with the particular VICP_ResourceType.
VICP_FLEXIBLE tells the IRQ driver to use the "flexible" VICP interrupt, which can be driven by all VICP_ResourceType except VICP_MJCP.

Type of ARM interrupt support.


Enumeration Type Documentation

Status codes for VICP API return values.

Enumerator:
VICP_OK 

OK

VICP_EFAIL 

general failure

VICP_ENOCHANNEL 

no channels available

VICP_ENOINIT 

VICP_init() not called

Resource types to be used for all APIs.

Enumerator:
VICP_IMX0 
VICP_IMX1 
VICP_MJCP 
VICP_NSF 
VICP_HDVICP0 
VICP_HDVICP1 

Source of VICP resource interrupt.

Remarks:
VICP_FIXED tells the IRQ driver to use the interrupt that's dedicated for use with the particular VICP_ResourceType.
VICP_FLEXIBLE tells the IRQ driver to use the "flexible" VICP interrupt, which can be driven by all VICP_ResourceType except VICP_MJCP.
Enumerator:
VICP_FIXED 
VICP_FLEXIBLE 

Type of ARM interrupt support.

Enumerator:
VICP_IRQ 
VICP_FIQ 

Function Documentation

int VICP_init ( void   )

VICP initialization API.

int VICP_exit ( void   )

VICP finalization API.

VICP_Status VICP_register ( VICP_ResourceType  resource,
VICP_InterruptLine  intrLine,
VICP_InterruptType  intrType 
)

Registers resource with requested interrupt type.

VICP_Status VICP_unregister ( VICP_ResourceType  resource )

Frees previously requested resource.

VICP_Status VICP_wait ( VICP_ResourceType  resource )

Waits for the transfer corresponding to this resource to complete.

VICP_Status VICP_done ( VICP_ResourceType  resource,
int *  done 
)

Checks if the transfer corresponding to this resource is complete.

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2011, Texas Instruments Incorporated