Linux Utils Application Programming Interface (API)  linuxutils-n01
 All Data Structures Files Functions Variables Typedefs Groups Pages
Data Structures | Macros | Typedefs | Functions | Variables
Contiguous Memory Manager

Describes the interface to the contiguous memory allocator. More...

Data Structures

struct  CMEM_AllocParams
 Parameters for CMEM_alloc(), CMEM_alloc2(), CMEM_allocPool(), CMEM_allocPool2(), CMEM_free(). More...
 
struct  CMEM_BlockAttrs
 

Macros

#define CMEM_VERSION   0x04000300U
 
#define MAX_POOLS   32
 
#define CMEM_CMABLOCKID   -1
 
#define CMEM_WB   0x00010000
 
#define CMEM_INV   0x00020000
 
#define CMEM_HEAP   0x00040000
 
#define CMEM_POOL   0x00000000
 
#define CMEM_CACHED   0x00080000
 
#define CMEM_NONCACHED   0x00000000
 
#define CMEM_PHYS   0x00100000
 
#define CMEM_IOCMAGIC   0x0000fe00
 
#define CMEM_IOCALLOC   1
 
#define CMEM_IOCALLOCHEAP   2
 
#define CMEM_IOCFREE   3
 
#define CMEM_IOCGETPHYS   4
 
#define CMEM_IOCGETSIZE   5
 
#define CMEM_IOCGETPOOL   6
 
#define CMEM_IOCCACHE   7
 
#define CMEM_IOCGETVERSION   8
 
#define CMEM_IOCGETBLOCK   9
 
#define CMEM_IOCREGUSER   10
 
#define CMEM_IOCGETNUMBLOCKS   11
 
#define CMEM_IOCCACHEWBINVALL   12
 
#define CMEM_IOCCACHEWBINV   CMEM_IOCCACHE | CMEM_WB | CMEM_INV
 
#define CMEM_IOCCACHEWB   CMEM_IOCCACHE | CMEM_WB
 
#define CMEM_IOCCACHEINV   CMEM_IOCCACHE | CMEM_INV
 
#define CMEM_IOCALLOCCACHED   CMEM_IOCALLOC | CMEM_CACHED
 
#define CMEM_IOCALLOCHEAPCACHED   CMEM_IOCALLOCHEAP | CMEM_CACHED
 
#define CMEM_IOCFREEHEAP   CMEM_IOCFREE | CMEM_HEAP
 
#define CMEM_IOCFREEPHYS   CMEM_IOCFREE | CMEM_PHYS
 
#define CMEM_IOCFREEHEAPPHYS   CMEM_IOCFREE | CMEM_HEAP | CMEM_PHYS
 
#define CMEM_IOCCMDMASK   0x000000ff
 

Typedefs

typedef struct CMEM_AllocParams CMEM_AllocParams
 Parameters for CMEM_alloc(), CMEM_alloc2(), CMEM_allocPool(), CMEM_allocPool2(), CMEM_free(). More...
 
typedef struct CMEM_BlockAttrs CMEM_BlockAttrs
 

Functions

int CMEM_init (void)
 Initialize the CMEM module. Must be called before other API calls. More...
 
int CMEM_getPool (unsigned long long size)
 Find the pool that best fits a given buffer size and has a buffer available. More...
 
int CMEM_getPool2 (int blockid, unsigned long long size)
 Find the pool in memory block blockid that best fits a given buffer size and has a buffer available. More...
 
void * CMEM_allocPool (int poolid, CMEM_AllocParams *params)
 Allocate memory from a specified pool. More...
 
void * CMEM_allocPool2 (int blockid, int poolid, CMEM_AllocParams *params)
 Allocate memory from a specified pool in a specified memory block. More...
 
void * CMEM_alloc (size_t size, CMEM_AllocParams *params)
 Allocate memory of a specified size. More...
 
void * CMEM_alloc2 (int blockid, size_t size, CMEM_AllocParams *params)
 Allocate memory of a specified size from a specified memory block. More...
 
off_t CMEM_allocPoolPhys (int poolid, CMEM_AllocParams *params)
 Allocate unmapped memory from a specified pool. More...
 
off_t CMEM_allocPoolPhys2 (int blockid, int poolid, CMEM_AllocParams *params)
 Allocate unmapped memory from a specified pool in a specified memory block. More...
 
off64_t CMEM_allocPoolPhys64 (int blockid, int poolid, CMEM_AllocParams *params)
 Allocate unmapped memory from a specified pool in a specified memory block (Android only). More...
 
off_t CMEM_allocPhys (size_t size, CMEM_AllocParams *params)
 Allocate unmapped memory of a specified size. More...
 
off_t CMEM_allocPhys2 (int blockid, size_t size, CMEM_AllocParams *params)
 Allocate unmapped memory of a specified size from a specified memory block. More...
 
off64_t CMEM_allocPhys64 (int blockid, size_t size, CMEM_AllocParams *params)
 Allocate unmapped memory of a specified size from a specified memory block (Android only) More...
 
void * CMEM_registerAlloc (off_t physp)
 Register shared usage of an already-allocated buffer. More...
 
void * CMEM_registerAlloc64 (off64_t physp)
 Register shared usage of an already-allocated buffer using mmap64 (Android only) More...
 
int CMEM_free (void *ptr, CMEM_AllocParams *params)
 Free a buffer previously allocated with CMEM_alloc()/CMEM_allocPool(). More...
 
int CMEM_freePhys (off_t physp, CMEM_AllocParams *params)
 Free an unmapped buffer previously allocated with CMEM_allocPhys()/CMEM_allocPoolPhys(). More...
 
int CMEM_freePhys64 (off64_t physp, CMEM_AllocParams *params)
 Free an unmapped buffer previously allocated with CMEM_allocPhys64()/CMEM_allocPoolPhys64() (Android only). More...
 
int CMEM_unregister (void *ptr, CMEM_AllocParams *params)
 Unregister use of a buffer previously registered with CMEM_registerAlloc(). More...
 
off_t CMEM_getPhys (void *ptr)
 Get the physical address of a contiguous buffer. More...
 
off64_t CMEM_getPhys64 (void *ptr)
 Get the physical address of a contiguous buffer (Android only). More...
 
int CMEM_cacheWbInvAll (void)
 Do a cache writeback/invalidate of the whole cache. More...
 
int CMEM_cacheWb (void *ptr, size_t size)
 Do a cache writeback of the block pointed to by ptr/size. More...
 
void * CMEM_map (off_t physp, size_t size)
 Map allocated memory. More...
 
void * CMEM_map64 (off64_t physp, size_t size)
 Map allocated memory using mmap64 (Android only) More...
 
int CMEM_unmap (void *userp, size_t size)
 Unmap allocated memory. More...
 
int CMEM_cacheInv (void *ptr, size_t size)
 Do a cache invalidate of the block pointed to by ptr/size. More...
 
int CMEM_cacheWbInv (void *ptr, size_t size)
 Do a cache writeback/invalidate of the block pointed to by ptr/size. More...
 
int CMEM_getVersion (void)
 Retrieve version from CMEM driver. More...
 
int CMEM_getBlock (off_t *pphys_base, unsigned long long *psize)
 Retrieve memory block bounds from CMEM driver. More...
 
int CMEM_getBlockAttrs (int blockid, CMEM_BlockAttrs *pattrs)
 Retrieve extended memory block attributes from CMEM driver. More...
 
int CMEM_getNumBlocks (int *pnblocks)
 Retrieve number of blocks configured into CMEM driver. More...
 
int CMEM_exit (void)
 Finalize the CMEM module. More...
 

Variables

CMEM_AllocParams CMEM_DEFAULTPARAMS
 

Detailed Description

Describes the interface to the contiguous memory allocator.

The cmem user interface library wraps file system calls to an associated kernel module (cmemk.ko), which needs to be loaded in order for calls to this library to succeed.

The CMEM kernel module accepts blocks of physical memory and a pool geometry within those blocks. The blocks and pools can be specified either in the traditional command line method, or with the new DT (Device Tree) method. The DT method is the prefered method due to its control by a system integrator.

Command line block and pool specification

The following is an example of installing the cmem kernel module using the traditional command line block and pool parameters (a DT example is shown below):

/sbin/insmod cmemk.ko pools=4x30000,2x500000 phys_start=0x0 phys_end=0x3000000 

This particular command creates 2 pools. The first pool is created with 4 buffers of size 30000 bytes and the second pool is created with 2 buffers of size 500000 bytes. The CMEM pool buffers start at 0x0 and end at 0x2FFFFFF (max).

There is also support for a 2nd, 3rd, or 4th contiguous memory block to be specified, with all the same features supported for those blocks as with the 1st. This 2nd block is specified with *_1 parameters (and 3rd block with *_2, 4th block with *_3). The following example expands upon the first example above:

/sbin/insmod cmemk.ko pools=4x30000,2x500000 phys_start=0x0 phys_end=0x3000000
   pools_1=4x65536 phys_start_1=0x80000000 phys_end_1=0x80010000 

This particular command, in addition to the pools explained above, creates 1 pool (with 4 buffers of size 64KB) in a 2nd memory block which starts at 0x80000000 and ends at 0x8000FFFF (specified as "end + 1" on the insmod command).

In order to access blocks beyond the 1st block, new APIs have been added to CMEM which allow specification of the block ID.

There is another configuration "switch" for the cmemk.ko kernel module, which can be specified on the 'insmod' (or 'modprobe') command lines: useHeapIfPoolUnavailable=[0|1]

'useHeapIfPoolUnavailable', when set to 1, will cause pool-based allocations to fallback to a heap-based allocation if no pool buffer of sufficient size is available (the CMEM heap is described below).

Pool buffers are aligned on a module-dependent boundary, and their sizes are rounded up to this same boundary. This applies to each buffer within a pool. The total space used by an individual pool will therefore be greater than (or equal to) the exact amount requested in the installation of the module.

The poolid used in the driver calls would be 0 for the first pool and 1 for the second pool.

Pool allocations can be requested explicitly by pool number, or more generally by just a size. For size-based allocations, the pool which best fits the requested size is automatically chosen. Some CMEM APIs (newer ones) accept a blockid as a parameter, in order to specify which of the multiple blocks to operate on. For 'legacy' APIs (ones that existed before the support for multiple blocks) where a blockid is still needed, block 0 is assumed.

There is also support for a general purpose heap. In addition to the 2 pools described above, a general purpose heap block is created from which allocations of any size can be requested. Internally, allocation sizes are rounded up to a module-dependent boundary and allocation addresses are aligned either to this same boundary or to the requested alignment (whichever is greater).

The size of the heap block is the amount of CMEM memory remaining after all pool allocations. If more heap space is needed than is available after pool allocations, you must reduce the amount of CMEM memory granted to the pools.

Buffer allocation is tracked at the file descriptor level by way of a 'registration' list. The initial allocator of a buffer (the process that calls CMEM_alloc()) is automatically added to the registration list, and further processes can become registered for the same buffer by way of the CMEM_registerAlloc() API (and unregister with the CMEM_unregister() API). This registration list for each buffer allows for buffer ownership tracking and cleanup on a per-file-descriptor basis, so that when a process exits or dies without having explicitly freed/unregistered its buffers, they get automatically unregistered (and freed when no more registered file descriptors exist). Only when the last registered file descriptor frees a buffer (either explictily, or by auto-cleanup) does a buffer actually get freed back to the kernel module.

Block and pool specification using Device Tree (DT)

The Device Tree can be used to specify physical memory blocks and pool geometry within those blocks, with the same capabilities as the command line specification. DT specification is preferred over command line specification for a number of reasons:

CMEM allows both DT-specified and command line specified blocks. Each block is assigned a number that can be later used for allocations in order to direct the allocation to a particular block. This allows some blocks to be defined in the DT and other blocks to be later defined on the CMEM command line. If a particular block number is assigned in DT and also specified on the CMEM command line then the DT specification takes precedence and the command line specification is ignored.

The following DT example snippet illustrates the syntax...

* // Specify reserved physical blocks, using "no-map" to keep Linux away.
* // The "reg" property is the base address and size in 32-bit ints.
* // This is the generic "reserved-memory" node that might also contain
* // other non-CMEM entries.
*
* reserved-memory {
* #address-cells = <1>;
* #size-cells = <1>;
* ranges;
* ...
* cmem_block_mem_0: cmem_block_mem@a0000000 {
* reg = <0xa0000000 0x10000000>;
* no-map;
* status = "okay";
* };
*
* cmem_block_mem_1: cmem_block_mem@b0000000 {
* reg = <0xb0000000 0x02000000>;
* no-map;
* status = "okay";
* };
* };
*
* // The CMEM node is specified below, and can be named arbitrarily ("cmem"
* // name chosen here). The node's "compatible" property must contain
* // "ti,cmem" in order for CMEM to process it.
*
* cmem {
* compatible = "ti,cmem"; // must be "ti,cmem"
* #address-cells = <1>;
* #size-cells = <0>;
*
* status = "okay";
*
* // CMEM block specifications along with pool geometry.
* //
* // The "reg" property is the block identifier, and each child of the
* // cmem node must specify a different "reg" value. The domain of
* // the block identifier is 0 -> <nblocks - 1>, where nblocks is the
* // total amount of DT-specified and command line-specified blocks.
* // CMEM currently supports up to 4 blocks (although that can be increased
* // by simple comment-directed modifications in cmemk.c).
* //
* // The "memory-region" property points to the phandle of the
* // reserved-memory area.
* //
* // The "cmem-buf-pools" property contains a variable number of comma-
* // separated pools, with each pool specifying the number of buffers and
* // the size of each buffer in <n size> format.
*
* cmem_block_0: cmem_block@0 {
* reg = <0>;
* memory-region = <&cmem_block_mem_0>;
* cmem-buf-pools = <1 0x0c000000>, <4 0x01000000>; // 1x256MB, 4x16MB pools
* };
*
* cmem_block_1: cmem_block@1 {
* reg = <1>;
* memory-region = <&cmem_block_mem_1>;
* cmem-buf-pools = <1 0x02000000>; // 1x32MB pool, remaining carveout is heap.
* };
* };
*

Decoupled allocation & memory mapping

For every CMEM_alloc*() API, there is a corresponding "Phys" API that returns the physical address of the allocation and does not do the user-space memory mapping (mmap()). There is also a corresponding CMEM_freePhys() to be used for freeing allocations performed by the "Phys" APIs. The user-space memory mapping is performed with the CMEM_map()/CMEM_unmap() APIs. This allows large buffer allocations without the burden of using up a large portion of the application's virtual address space for the duration of the allocation's existence. A mapping performed by CMEM_map() doesn't have to be for the whole of the allocated buffer, it can be for just portions of the buffer (but must not be larger than the allocated buffer).

CMEM_map() can be called multiple times for the same physical allocation. Each invocation of CMEM_map() will allocate a new user virtual address range for the same physical allocation.

CMA access

On systems with CMA (Contiguous Memory Allocator) support, CMEM can be used to allocate CMA buffers. Both heap and pool allocations are supported. A special block ID, CMEM_CMABLOCKID, is used for these allocations, and therefore the block-based CMEM APIs must be used (the ones ending in "2", such as CMEM_alloc2()), where the 'blockid' parameter is CMEM_CMABLOCKID (instead of 0 or 1).

CMA always contains, at the minimum, a global area that can be accessed by any device driver. CMEM treats this global area as a heap, which means that heap-based allocations can be performed on CMEM_CMABLOCKID. See the Linux CMA documentation for details on specifying this global area. Keep in mind that other Linux kernel entities can (and will) also allocate memory from this global area, so you never really know how much is available for allocations by CMEM.

To achieve pool-based allocations from CMA, a special CMEM stub must be builtin to the kernel, and CMEM must be built with CMEM_KERNEL_STUB=1 for the 'make' command (which turns into -DCMEM_KERNEL_STUB on the compile command). This stub processes a kernel command line parameter named "cmem_cma_pools=..." in the same fashion as the standard CMEM "pools=...". A separate CMA region (area) is created for each of the separate "cmem_cma_pools" (where each pool/region is one element of the comma- separated list).

The CMEM builtin kernel stub is located in .../src/cmem/module/kernel/drivers/cmem/cmemk_stub.c You don't need this stub if you want to allocate only from the CMA global area. Please see comments at the head of the above file for instructions on how to incorporate it into your kernel.

In supporting the pool model of CMEM, a separate CMA region is created for each pool. A pool consists of n buffers of size s, resulting in a region that is sized accordingly. CMA places no restrictions on the size of an allocation from a region, so the buffer size 's' becomes more of a convention than a hard rule. Given enough free space, any pool can be used to allocate a buffer of any size, but it is recommended to partition regions (or, in this case, pools) according to the size of buffers that will be allocated in order to reduce fragmentation and wasted memory due to size-based alignment padding. In other words, if your system will be allocating 10 buffers of size 4096, 8 of size 131072, and 4 of size 1048576, create pools of cmem_cma_pools=10x4096,8x131072,4x1048576 and perform allocations from the respective pool.

An application doesn't need to know the pool IDs that correspond to the respective sizes of that pool's buffers. The CMEM_alloc2() API decides which pool to use according to the requested size of allocation, and will choose the one that fits most efficiently. Unlike non-CMA pool allocations where, when the "best fit" pool has no remaining buffers it will choose a pool with larger available buffers, CMEM_alloc2() won't "promote" a CMA-based pool allocation to a pool with buffers larger than the the best fit.

CMEM supports a kernel command line parameter named "cmem_cma_heapsize". When assigned, a CMA region of size "cmem_cma_heapsize" is created for use by CMEM heap allocations for the CMA "block". This heap is then used for CMEM CMA heap allocations, and the CMA global area is no longer used by CMEM. This allows CMEM to have full usage of the CMEM CMA heap without possible allocations by non-CMEM entities in the kernel.

Macro Definition Documentation

#define CMEM_VERSION   0x04000300U
#define MAX_POOLS   32
#define CMEM_CMABLOCKID   -1
#define CMEM_WB   0x00010000
#define CMEM_INV   0x00020000
#define CMEM_HEAP   0x00040000

operation applies to heap

#define CMEM_POOL   0x00000000

operation applies to a pool

#define CMEM_CACHED   0x00080000

allocated buffer is cached

#define CMEM_NONCACHED   0x00000000

allocated buffer is not cached

#define CMEM_PHYS   0x00100000
#define CMEM_IOCMAGIC   0x0000fe00
#define CMEM_IOCALLOC   1
#define CMEM_IOCALLOCHEAP   2
#define CMEM_IOCFREE   3
#define CMEM_IOCGETPHYS   4
#define CMEM_IOCGETSIZE   5
#define CMEM_IOCGETPOOL   6
#define CMEM_IOCCACHE   7
#define CMEM_IOCGETVERSION   8
#define CMEM_IOCGETBLOCK   9
#define CMEM_IOCREGUSER   10
#define CMEM_IOCGETNUMBLOCKS   11
#define CMEM_IOCCACHEWBINVALL   12
#define CMEM_IOCCACHEWBINV   CMEM_IOCCACHE | CMEM_WB | CMEM_INV
#define CMEM_IOCCACHEWB   CMEM_IOCCACHE | CMEM_WB
#define CMEM_IOCCACHEINV   CMEM_IOCCACHE | CMEM_INV
#define CMEM_IOCALLOCCACHED   CMEM_IOCALLOC | CMEM_CACHED
#define CMEM_IOCALLOCHEAPCACHED   CMEM_IOCALLOCHEAP | CMEM_CACHED
#define CMEM_IOCFREEHEAP   CMEM_IOCFREE | CMEM_HEAP
#define CMEM_IOCFREEPHYS   CMEM_IOCFREE | CMEM_PHYS
#define CMEM_IOCFREEHEAPPHYS   CMEM_IOCFREE | CMEM_HEAP | CMEM_PHYS
#define CMEM_IOCCMDMASK   0x000000ff

Typedef Documentation

Function Documentation

int CMEM_init ( void  )

Initialize the CMEM module. Must be called before other API calls.

Returns
0 for success or -1 for failure.
See Also
CMEM_exit
int CMEM_getPool ( unsigned long long  size)

Find the pool that best fits a given buffer size and has a buffer available.

Parameters
sizeThe buffer size for which a pool is needed.
Returns
A poolid that can be passed to CMEM_allocPool(), or -1 for error.
Precondition
Must have called CMEM_init()
See Also
CMEM_allocPool()
CMEM_allocPool2()
CMEM_free()
CMEM_getPool2()
int CMEM_getPool2 ( int  blockid,
unsigned long long  size 
)

Find the pool in memory block blockid that best fits a given buffer size and has a buffer available.

Parameters
blockidBlock number
sizeThe buffer size for which a pool is needed.
Returns
A poolid that can be passed to CMEM_allocPool2(), or -1 for error.
Precondition
Must have called CMEM_init()
See Also
CMEM_allocPool()
CMEM_allocPool2()
CMEM_free()
CMEM_getPool()
void* CMEM_allocPool ( int  poolid,
CMEM_AllocParams params 
)

Allocate memory from a specified pool.

Parameters
poolidThe pool from which to allocate memory.
paramsAllocation parameters.
Remarks
params->type is ignored - a pool will always be used.
params->alignment is unused, since pool buffers are already aligned to specific boundaries.
Returns
A pointer to the allocated buffer, or NULL for failure.
Precondition
Must have called CMEM_init()
See Also
CMEM_alloc()
CMEM_alloc2()
CMEM_allocPool2()
CMEM_registerAlloc()
CMEM_unregister()
CMEM_free()
void* CMEM_allocPool2 ( int  blockid,
int  poolid,
CMEM_AllocParams params 
)

Allocate memory from a specified pool in a specified memory block.

Parameters
blockidThe memory block from which to allocate.
poolidThe pool from which to allocate memory.
paramsAllocation parameters.
Remarks
params->type is ignored - a pool will always be used.
params->alignment is unused, since pool buffers are already aligned to specific boundaries.
Returns
A pointer to the allocated buffer, or NULL for failure.
Precondition
Must have called CMEM_init()
See Also
CMEM_alloc()
CMEM_alloc2()
CMEM_allocPool()
CMEM_registerAlloc()
CMEM_unregister()
CMEM_free()
void* CMEM_alloc ( size_t  size,
CMEM_AllocParams params 
)

Allocate memory of a specified size.

Parameters
sizeThe size of the buffer to allocate.
paramsAllocation parameters.
Remarks
Used to allocate memory from either a pool, the heap, or the CMA global area. If doing a pool allocation, the pool that best fits the requested size will be selected. Use CMEM_allocPool() to allocate from a specific pool. Allocation will be cached or noncached, as specified by params. params->alignment valid only for heap allocation.
Returns
A pointer to the allocated buffer, or NULL for failure.
Precondition
Must have called CMEM_init()
See Also
CMEM_allocPool()
CMEM_allocPool2()
CMEM_alloc2()
CMEM_registerAlloc()
CMEM_unregister()
CMEM_free()
void* CMEM_alloc2 ( int  blockid,
size_t  size,
CMEM_AllocParams params 
)

Allocate memory of a specified size from a specified memory block.

Parameters
blockidThe memory block from which to allocate.
sizeThe size of the buffer to allocate.
paramsAllocation parameters.
Remarks
Used to allocate memory from either a pool, the heap, or the CMA global area. If doing a pool allocation, the pool that best fits the requested size will be selected. Use CMEM_allocPool() to allocate from a specific pool.
Allocation will be cached or noncached, as specified by params. params->alignment valid only for heap allocation.
Returns
A pointer to the allocated buffer, or NULL for failure.
Precondition
Must have called CMEM_init()
See Also
CMEM_allocPool()
CMEM_allocPool2()
CMEM_alloc()
CMEM_registerAlloc()
CMEM_unregister()
CMEM_free()
off_t CMEM_allocPoolPhys ( int  poolid,
CMEM_AllocParams params 
)

Allocate unmapped memory from a specified pool.

Parameters
poolidThe pool from which to allocate memory.
paramsAllocation parameters.
Remarks
params->type is ignored - a pool will always be used.
params->alignment is unused, since pool buffers are already aligned to specific boundaries.
Returns
The physical address of the allocated buffer, or NULL for failure.
Precondition
Must have called CMEM_init()
See Also
CMEM_allocPhys()
CMEM_allocPhys2()
CMEM_allocPoolPhys2()
CMEM_freePhys()
CMEM_map()
off_t CMEM_allocPoolPhys2 ( int  blockid,
int  poolid,
CMEM_AllocParams params 
)

Allocate unmapped memory from a specified pool in a specified memory block.

Parameters
blockidThe memory block from which to allocate.
poolidThe pool from which to allocate memory.
paramsAllocation parameters.
Remarks
params->type is ignored - a pool will always be used.
params->alignment is unused, since pool buffers are already aligned to specific boundaries.
Returns
The physical address of the allocated buffer, or NULL for failure.
Precondition
Must have called CMEM_init()
See Also
CMEM_allocPhys()
CMEM_allocPhys2()
CMEM_allocPoolPhys()
CMEM_freePhys()
CMEM_map()
off64_t CMEM_allocPoolPhys64 ( int  blockid,
int  poolid,
CMEM_AllocParams params 
)

Allocate unmapped memory from a specified pool in a specified memory block (Android only).

Parameters
blockidThe memory block from which to allocate.
poolidThe pool from which to allocate memory.
paramsAllocation parameters.
Remarks
params->type is ignored - a pool will always be used.
params->alignment is unused, since pool buffers are already aligned to specific boundaries.
Returns
The physical address of the allocated buffer, or NULL for failure.
Precondition
Must have called CMEM_init()
See Also
CMEM_allocPhys()
CMEM_allocPhys2()
CMEM_allocPoolPhys()
CMEM_freePhys()
CMEM_map()
off_t CMEM_allocPhys ( size_t  size,
CMEM_AllocParams params 
)

Allocate unmapped memory of a specified size.

Parameters
sizeThe size of the buffer to allocate.
paramsAllocation parameters.
Remarks
Used to allocate memory from either a pool, the heap, or the CMA global area. If doing a pool allocation, the pool that best fits the requested size will be selected. Use CMEM_allocPool() to allocate from a specific pool. Allocation will be cached or noncached, as specified by params. params->alignment valid only for heap allocation.
Returns
The physical address of the allocated buffer, or NULL for failure.
Precondition
Must have called CMEM_init()
See Also
CMEM_allocPoolPhys()
CMEM_allocPoolPhys2()
CMEM_allocPhys2()
CMEM_freePhys()
CMEM_map()
off_t CMEM_allocPhys2 ( int  blockid,
size_t  size,
CMEM_AllocParams params 
)

Allocate unmapped memory of a specified size from a specified memory block.

Parameters
blockidThe memory block from which to allocate.
sizeThe size of the buffer to allocate.
paramsAllocation parameters.
Remarks
Used to allocate memory from either a pool, the heap, or the CMA global area. If doing a pool allocation, the pool that best fits the requested size will be selected. Use CMEM_allocPool() to allocate from a specific pool.
Allocation will be cached or noncached, as specified by params. params->alignment valid only for heap allocation.
Returns
The physical address of the allocated buffer, or NULL for failure.
Precondition
Must have called CMEM_init()
See Also
CMEM_allocPoolPhys()
CMEM_allocPoolPhys2()
CMEM_allocPhys()
CMEM_freePhys()
CMEM_map()
off64_t CMEM_allocPhys64 ( int  blockid,
size_t  size,
CMEM_AllocParams params 
)

Allocate unmapped memory of a specified size from a specified memory block (Android only)

Parameters
blockidThe memory block from which to allocate.
sizeThe size of the buffer to allocate.
paramsAllocation parameters.
Remarks
Used to allocate memory from either a pool, the heap, or the CMA global area. If doing a pool allocation, the pool that best fits the requested size will be selected. Use CMEM_allocPool() to allocate from a specific pool.
Allocation will be cached or noncached, as specified by params. params->alignment valid only for heap allocation.
Returns
The physical address of the allocated buffer, or NULL for failure.
Precondition
Must have called CMEM_init()
See Also
CMEM_allocPoolPhys()
CMEM_allocPoolPhys2()
CMEM_allocPhys()
CMEM_freePhys()
CMEM_map()
void* CMEM_registerAlloc ( off_t  physp)

Register shared usage of an already-allocated buffer.

Parameters
physpPhysical address of the already-allocated buffer.
Remarks
Used to register the calling process for usage of an already-allocated buffer, for the purpose of shared usage of the buffer.
Allocation properties (such as cached/noncached or heap/pool) are inherited from original allocation call.
Returns
A process-specific pointer to the allocated buffer, or NULL for failure.
Precondition
Must have called some form of CMEM_alloc*()
See Also
CMEM_allocPool()
CMEM_allocPool2()
CMEM_alloc()
CMEM_free()
CMEM_unregister()
void* CMEM_registerAlloc64 ( off64_t  physp)

Register shared usage of an already-allocated buffer using mmap64 (Android only)

Parameters
physpPhysical address of the already-allocated buffer.
Remarks
Used to register the calling process for usage of an already-allocated buffer, for the purpose of shared usage of the buffer.
Allocation properties (such as cached/noncached or heap/pool) are inherited from original allocation call.
Returns
A process-specific pointer to the allocated buffer, or NULL for failure.
Precondition
Must have called some form of CMEM_alloc*()
See Also
CMEM_allocPool()
CMEM_allocPool2()
CMEM_alloc()
CMEM_free()
CMEM_unregister()
int CMEM_free ( void *  ptr,
CMEM_AllocParams params 
)

Free a buffer previously allocated with CMEM_alloc()/CMEM_allocPool().

Parameters
ptrThe pointer to the buffer.
paramsAllocation parameters.
Remarks
Use the same CMEM_AllocParams as was used for the allocation. params->flags is "don't care". params->alignment is "don't care".
Returns
0 for success or -1 for failure.
Precondition
Must have called CMEM_init()
See Also
CMEM_alloc()
CMEM_alloc2()
CMEM_allocPool()
CMEM_allocPool2()
CMEM_registerAlloc()
CMEM_unregister()
int CMEM_freePhys ( off_t  physp,
CMEM_AllocParams params 
)

Free an unmapped buffer previously allocated with CMEM_allocPhys()/CMEM_allocPoolPhys().

Parameters
physpThe physical address of the buffer.
paramsAllocation parameters.
Remarks
Use the same CMEM_AllocParams as was used for the allocation. params->flags is "don't care". params->alignment is "don't care".
Returns
0 for success or -1 for failure.
Precondition
Must have called CMEM_init()
See Also
CMEM_allocPhys()
CMEM_allocPhys2()
CMEM_allocPoolPhys()
CMEM_allocPoolPhys2()
CMEM_unmap()
int CMEM_freePhys64 ( off64_t  physp,
CMEM_AllocParams params 
)

Free an unmapped buffer previously allocated with CMEM_allocPhys64()/CMEM_allocPoolPhys64() (Android only).

Parameters
physpThe physical address of the buffer.
paramsAllocation parameters.
Remarks
Use the same CMEM_AllocParams as was used for the allocation. params->flags is "don't care". params->alignment is "don't care".
Returns
0 for success or -1 for failure.
Precondition
Must have called CMEM_init()
See Also
CMEM_allocPhys()
CMEM_allocPhys2()
CMEM_allocPoolPhys()
CMEM_allocPoolPhys2()
CMEM_unmap()
int CMEM_unregister ( void *  ptr,
CMEM_AllocParams params 
)

Unregister use of a buffer previously registered with CMEM_registerAlloc().

Parameters
ptrThe pointer to the buffer.
paramsAllocation parameters.
Remarks
Use the same CMEM_AllocParams as was used for the allocation. params->flags is "don't care". params->alignment is "don't care".
Returns
0 for success or -1 for failure.
Precondition
Must have called CMEM_init()
See Also
CMEM_alloc()
CMEM_alloc2()
CMEM_allocPool()
CMEM_allocPool2()
CMEM_registerAlloc()
CMEM_free()
off_t CMEM_getPhys ( void *  ptr)

Get the physical address of a contiguous buffer.

Parameters
ptrThe pointer to the buffer.
Returns
The physical address of the buffer or 0 for failure.
Precondition
Must have called CMEM_init()
off64_t CMEM_getPhys64 ( void *  ptr)

Get the physical address of a contiguous buffer (Android only).

Parameters
ptrThe pointer to the buffer.
Returns
The physical address of the buffer or 0 for failure.
Precondition
Must have called CMEM_init()
int CMEM_cacheWbInvAll ( void  )

Do a cache writeback/invalidate of the whole cache.

Returns
Success/failure boolean value
Precondition
Must have called CMEM_init()
See Also
CMEM_cacheWb()
CMEM_cacheInv()
CMEM_cacheWbInv()
int CMEM_cacheWb ( void *  ptr,
size_t  size 
)

Do a cache writeback of the block pointed to by ptr/size.

Parameters
ptrPointer to block to writeback
sizeSize in bytes of block to writeback.
Returns
Success/failure boolean value
Precondition
Must have called CMEM_init()
See Also
CMEM_cacheInv()
CMEM_cacheWbInv()
CMEM_cacheWbInvAll()
void* CMEM_map ( off_t  physp,
size_t  size 
)

Map allocated memory.

Parameters
physpPhysical address of the already-allocated buffer.
sizeSize in bytes of block to map.
Returns
A pointer to the mapped buffer, or NULL for failure.
Precondition
Must have called CMEM_init()
See Also
CMEM_allocPhys()
CMEM_allocPoolPhys()
CMEM_unmap()
void* CMEM_map64 ( off64_t  physp,
size_t  size 
)

Map allocated memory using mmap64 (Android only)

Parameters
physpPhysical address of the already-allocated buffer.
sizeSize in bytes of block to map.
Returns
A pointer to the mapped buffer, or NULL for failure.
Precondition
Must have called CMEM_init()
See Also
CMEM_allocPhys()
CMEM_allocPoolPhys()
CMEM_unmap()
int CMEM_unmap ( void *  userp,
size_t  size 
)

Unmap allocated memory.

Parameters
userpUser virtual address of the mapped buffer.
sizeSize in bytes of block to unmap.
Returns
Success/failure boolean value
Precondition
Must have called CMEM_init()
See Also
CMEM_freePhys()
CMEM_map()
int CMEM_cacheInv ( void *  ptr,
size_t  size 
)

Do a cache invalidate of the block pointed to by ptr/size.

Parameters
ptrPointer to block to invalidate
sizeSize in bytes of block to invalidate
Returns
Success/failure boolean value
Precondition
Must have called CMEM_init()
See Also
CMEM_cacheWb()
CMEM_cacheWbInv()
CMEM_cacheWbInvAll()
int CMEM_cacheWbInv ( void *  ptr,
size_t  size 
)

Do a cache writeback/invalidate of the block pointed to by ptr/size.

Parameters
ptrPointer to block to writeback/invalidate
sizeSize in bytes of block to writeback/invalidate
Returns
Success/failure boolean value
Precondition
Must have called CMEM_init()
See Also
CMEM_cacheInv()
CMEM_cacheWb()
CMEM_cacheWbInvAll()
int CMEM_getVersion ( void  )

Retrieve version from CMEM driver.

Returns
Installed CMEM driver's version number.
Precondition
Must have called CMEM_init()
int CMEM_getBlock ( off_t *  pphys_base,
unsigned long long *  psize 
)

Retrieve memory block bounds from CMEM driver.

Parameters
pphys_basePointer to storage for base physical address of CMEM's memory block
psizePointer to storage for size of CMEM's memory block
Returns
Success (0) or failure (-1).
Precondition
Must have called CMEM_init()
See Also
CMEM_getBlockAttrs()
CMEM_getNumBlocks()
int CMEM_getBlockAttrs ( int  blockid,
CMEM_BlockAttrs pattrs 
)

Retrieve extended memory block attributes from CMEM driver.

Parameters
blockidBlock number
pattrsPointer to CMEM_BlockAttrs struct
Returns
Success (0) or failure (-1).
Remarks
Currently this API returns the same values as CMEM_getBlock().
Precondition
Must have called CMEM_init()
See Also
CMEM_getBlock()
CMEM_getNumBlocks()
int CMEM_getNumBlocks ( int *  pnblocks)

Retrieve number of blocks configured into CMEM driver.

Parameters
pnblocksPointer to storage for holding number of blocks
Returns
Success (0) or failure (-1).
Remarks
Blocks are configured into CMEM through the Linux 'insmod' command.
Precondition
Must have called CMEM_init()
See Also
CMEM_getBlock()
CMEM_getBlockAttrs()
int CMEM_exit ( void  )

Finalize the CMEM module.

Returns
0 for success or -1 for failure.
Remarks
After this function has been called, no other CMEM function may be called (unless CMEM is reinitialized).
Precondition
Must have called CMEM_init()
See Also
CMEM_init()

Variable Documentation

CMEM_AllocParams CMEM_DEFAULTPARAMS
Copyright 2015, Texas Instruments Incorporated