Data Structures | Defines | Typedefs | Enumerations | Functions

SDMA Manager

Data Structures

struct  SDMA_transferState
 State structure shared between SDMAK and SDMA user layers. More...
union  SDMA_requestDmaParams
 SDMAK ioctl input/output parameters. More...
struct  SDMA_ChannelDescriptor
 Descriptor for a channel granted with a SDMA_IOCREQUESTDMA ioctl(). More...

Defines

#define SDMA_VERSION   0x01010000U
#define SDMA_IOCMAGIC   0x0000fb00
 SDMAK ioctl() commands.
#define SDMA_IOCCMDMASK   0x000000ff
#define SDMA_IOCREQUESTDMA   1
#define SDMA_IOCRELEASEDMA   2
#define SDMA_IOCWAITFORCOMPLETION   3
#define SDMA_IOCGETVERSION   4

Typedefs

typedef struct
SDMA_ChannelDescriptor 
SDMA_ChannelDescriptor
 Descriptor for a channel granted with a SDMA_IOCREQUESTDMA ioctl().
typedef enum SDMA_Status SDMA_Status
 Status codes for SDMA API return values.

Enumerations

enum  SDMA_Status {
  SDMA_OK = 0,
  SDMA_EFAIL,
  SDMA_ENOCHANNEL,
  SDMA_ENOINIT
}
 

Status codes for SDMA API return values.

More...

Functions

int SDMA_init (void)
 SDMA initialization API.
int SDMA_exit (void)
 SDMA finalization API.
SDMA_Status SDMA_getChannels (int numChannels, SDMA_ChannelDescriptor chanArray[])
 Returns available logical channels.
SDMA_Status SDMA_freeChannels (int numChannels, SDMA_ChannelDescriptor chanArray[])
 Frees previously requested logical channels.
SDMA_Status SDMA_wait (SDMA_ChannelDescriptor *channel)
 Waits for the transfer corresponding to this descriptor to complete.
SDMA_Status SDMA_check (SDMA_ChannelDescriptor *channel, int *pcompleted)
 Checks the status of the transfer corresponding to this descriptor and returns it in the *pcompleted field.
int SDMA_getVersion (void)
 Retrieve version from SDMA driver.

Detailed Description

This is the API for the SDMA Manager.


Define Documentation

#define SDMA_VERSION   0x01010000U
#define SDMA_IOCMAGIC   0x0000fb00

SDMAK ioctl() commands.

#define SDMA_IOCCMDMASK   0x000000ff
#define SDMA_IOCREQUESTDMA   1
#define SDMA_IOCRELEASEDMA   2
#define SDMA_IOCWAITFORCOMPLETION   3
#define SDMA_IOCGETVERSION   4

Typedef Documentation

Descriptor for a channel granted with a SDMA_IOCREQUESTDMA ioctl().

Remarks:
The address of the transferState member is passed down to the SDMAK module during the SDMA_IOCREQUESTDMA ioctl(). The SDMAK module maps this address and queries and writes to it during the completion ISR activity. It is therefore vital that the address of the descriptor passed to SDMA_getChannels() is in persistent memory that is live for the duration of SDMA channel usage.
See also:
SDMA_getChannels()
SDMA_freeChannels()
SDMA_wait()
SDMA_check()
typedef enum SDMA_Status SDMA_Status

Status codes for SDMA API return values.


Enumeration Type Documentation

Status codes for SDMA API return values.

Enumerator:
SDMA_OK 

OK

SDMA_EFAIL 

general failure

SDMA_ENOCHANNEL 

no channels available

SDMA_ENOINIT 

SDMA_init() not called


Function Documentation

int SDMA_init ( void   )

SDMA initialization API.

int SDMA_exit ( void   )

SDMA finalization API.

SDMA_Status SDMA_getChannels ( int  numChannels,
SDMA_ChannelDescriptor  chanArray[] 
)

Returns available logical channels.

Parameters:
numChannelsnumber of requested channels.
chanArraypointer to SDMA_ChannelDescriptor storage of sufficient size to hold numChannels descriptors. All structure array fields are filled by this API (in other words, no fields need to be filled by the caller prior to the call).
Remarks:
chanArray must be allocated from memory that persists over the life of the channel's usage, since the address of the chanArray will be used by the SDMA kernel driver. This implies that the contents of the passed chanArray should not be copied to another SDMA_ChannelDescriptor that is then used for the subsequent operations.
Fails if the requested number of channels is not available.
See also:
SDMA_freeChannels()
SDMA_Status SDMA_freeChannels ( int  numChannels,
SDMA_ChannelDescriptor  chanArray[] 
)

Frees previously requested logical channels.

Parameters:
numChannelsnumber of requested channels.
chanArraypointer to SDMA_ChannelDescriptor storage of sufficient size to hold numChannels descriptors. This will typically be the same pointer passed to SDMA_getChannels().
See also:
SDMA_getChannels()
SDMA_Status SDMA_wait ( SDMA_ChannelDescriptor channel )

Waits for the transfer corresponding to this descriptor to complete.

Parameters:
channelpointer to the single channel for which to wait.
Remarks:
SDMA_wait() first checks the transferComplete flag of the struct SDMA_transferState in channel. This flag is directly written by the SDMAK module's completion ISR. If this flag is not set to 1, SDMA_wait() will issue a SDMA_IOCWAITFORCOMPLETION ioctl(), which will block inside the SDMAK module and become unblocked by the completion ISR.
See also:
SDMA_check()
SDMA_Status SDMA_check ( SDMA_ChannelDescriptor channel,
int *  pcompleted 
)

Checks the status of the transfer corresponding to this descriptor and returns it in the *pcompleted field.

Parameters:
channelpointer to single channel to check.
pcompletedpointer to completion status.
Remarks:
copies the contents of the transferComplete flag of the struct SDMA_transferState in channel into *pcompleted (does not issue any ioctl()).
See also:
SDMA_wait()
int SDMA_getVersion ( void   )

Retrieve version from SDMA driver.

Returns:
Installed SDMA driver's version number.
Precondition:
Must have called SDMA_init()
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2012, Texas Instruments Incorporated