SDMA Manager

Data Structures

struct  SDMA_transferState
 State structure shared between SDMAK and SDMA user layers. More...
union  SDMA_requestDmaParams
 SDMAK ioctl input/output parameters. More...
struct  SDMA_ChannelDescriptor
 Descriptor for a channel granted with a SDMA_IOCREQUESTDMA ioctl(). More...

Defines

#define SDMA_VERSION   0x01000000U

Enumerations

enum  SDMA_commmands {
  SDMA_IOCREQUESTDMA = 1,
  SDMA_IOCRELEASEDMA,
  SDMA_IOCWAITFORCOMPLETION,
  SDMA_IOCGETVERSION
}
 

SDMAK ioctl() commands.

More...
enum  SDMA_Status {
  SDMA_OK = 0,
  SDMA_EFAIL,
  SDMA_ENOCHANNEL,
  SDMA_ENOINIT
}
 

Status codes for SDMA API return values.

More...

Functions

int SDMA_init (void)
 SDMA initialization API.
int SDMA_exit (void)
 SDMA finalization API.
SDMA_Status SDMA_getChannels (int numChannels, SDMA_ChannelDescriptor chanArray[])
 Returns available logical channels.
SDMA_Status SDMA_freeChannels (int numChannels, SDMA_ChannelDescriptor chanArray[])
 Frees previously requested logical channels.
SDMA_Status SDMA_wait (SDMA_ChannelDescriptor *channel)
 Waits for the transfer corresponding to this descriptor to complete.
SDMA_Status SDMA_check (SDMA_ChannelDescriptor *channel, int *pcompleted)
 Checks the status of the transfer corresponding to this descriptor and returns it in the *pcompleted field.
int SDMA_getVersion (void)
 Retrieve version from SDMA driver.

Detailed Description

This is the API for the SDMA Manager.


Define Documentation

#define SDMA_VERSION   0x01000000U

Enumeration Type Documentation

SDMAK ioctl() commands.

Enumerator:
SDMA_IOCREQUESTDMA 
SDMA_IOCRELEASEDMA 
SDMA_IOCWAITFORCOMPLETION 
SDMA_IOCGETVERSION 

Status codes for SDMA API return values.

Enumerator:
SDMA_OK 

OK

SDMA_EFAIL 

general failure

SDMA_ENOCHANNEL 

no channels available

SDMA_ENOINIT 

SDMA_init() not called


Function Documentation

int SDMA_init ( void   ) 

SDMA initialization API.

int SDMA_exit ( void   ) 

SDMA finalization API.

SDMA_Status SDMA_getChannels ( int  numChannels,
SDMA_ChannelDescriptor  chanArray[] 
)

Returns available logical channels.

Parameters:
numChannels number of requested channels.
chanArray pointer to SDMA_ChannelDescriptor storage of sufficient size to hold numChannels descriptors. All structure array fields are filled by this API (in other words, no fields need to be filled by the caller prior to the call).
Remarks:
chanArray must be allocated from memory that persists over the life of the channel's usage, since the address of the chanArray will be used by the SDMA kernel driver. This implies that the contents of the passed chanArray should not be copied to another SDMA_ChannelDescriptor that is then used for the subsequent operations.
Fails if the requested number of channels is not available.
See also:
SDMA_freeChannels()
SDMA_Status SDMA_freeChannels ( int  numChannels,
SDMA_ChannelDescriptor  chanArray[] 
)

Frees previously requested logical channels.

Parameters:
numChannels number of requested channels.
chanArray pointer to SDMA_ChannelDescriptor storage of sufficient size to hold numChannels descriptors. This will typically be the same pointer passed to SDMA_getChannels().
See also:
SDMA_getChannels()
SDMA_Status SDMA_wait ( SDMA_ChannelDescriptor channel  ) 

Waits for the transfer corresponding to this descriptor to complete.

Parameters:
channel pointer to the single channel for which to wait.
Remarks:
SDMA_wait() first checks the transferComplete flag of the struct SDMA_transferState in channel. This flag is directly written by the SDMAK module's completion ISR. If this flag is not set to 1, SDMA_wait() will issue a SDMA_IOCWAITFORCOMPLETION ioctl(), which will block inside the SDMAK module and become unblocked by the completion ISR.
See also:
SDMA_check()
SDMA_Status SDMA_check ( SDMA_ChannelDescriptor channel,
int *  pcompleted 
)

Checks the status of the transfer corresponding to this descriptor and returns it in the *pcompleted field.

Parameters:
channel pointer to single channel to check.
pcompleted pointer to completion status.
Remarks:
copies the contents of the transferComplete flag of the struct SDMA_transferState in channel into *pcompleted (does not issue any ioctl()).
See also:
SDMA_wait()
int SDMA_getVersion ( void   ) 

Retrieve version from SDMA driver.

Returns:
Installed SDMA driver's version number.
Precondition:
Must have called SDMA_init()
 All Data Structures Files Functions Variables Enumerations Enumerator Defines

Copyright 2010, Texas Instruments Incorporated