#include <sdma.h>
SDMA_IOCREQUESTDMA
ioctl() operation and is registered with the received channel. It is therefore vital that the structure address that is registered with the kernel module points to the actual location that is queried and written during a "wait" operation.
Data Fields | |
volatile int | transferCompleted |
volatile int | checkPending |
volatile int SDMA_transferState::transferCompleted |
flag for channel completion
volatile int SDMA_transferState::checkPending |
completion check hand-shaking flag