module ti.sdo.utils.MultiProc

Processor Id Module Manager

Many IPC modules require identifying processors in a multi-processor environment. The MultiProc module centralizes processor id management into one module. Since this configuration is almost always universally required, most IPC applications require supplying configuration of this module. [ more ... ]
C synopsis target-domain sourced in ti/sdo/utils/MultiProc.xdc
DETAILS
Many IPC modules require identifying processors in a multi-processor environment. The MultiProc module centralizes processor id management into one module. Since this configuration is almost always universally required, most IPC applications require supplying configuration of this module.
Each processor in the MultiProc module may be uniquely identified by either a name string or an integer ranging from 0 to MAXPROCESSORS - 1. Configuration is supplied using the setConfig meta function, the numProcessors and baseIdOfCluster.
The setConfig function tells the MultiProc module:
  • The specific processor for which the application is being built
  • The number of processors in the cluster
A cluster is a set of processors within a system which share some share shared memory and supports notifications. Typically most systems contain one cluster. When there are multiple clusters in the system, the numProcessors and baseIdOfCluster configuration paramaters are required to be set before calling setConfig
For examle in a system with 2 C6678 devices [each C6678 contains 8 homogeneuous cores]. For first C6678 device:
  var MultiProc = xdc.useModule('ti.sdo.utils.MultiProc');
  MultiProc.baseIdOfCluster = 0;
  MultiProc.numProcessors = 16;
  MultiProc.setConfig(null, ["CORE0", "CORE1", "CORE2", "CORE3",
                             "CORE4", "CORE5", "CORE6", "CORE7"]);
For second C6678 device:
  var MultiProc = xdc.useModule('ti.sdo.utils.MultiProc');
  MultiProc.baseIdOfCluster = 8;
  MultiProc.numProcessors = 16;
  MultiProc.setConfig(null, ["CORE0", "CORE1", "CORE2", "CORE3",
                             "CORE4", "CORE5", "CORE6", "CORE7"]);
Using the information supplied using the setConfig meta function and the baseIdOfCluster module configuration, the processor IDs are internally set. Please refer to the documentation for setConfig and baseIdOfCluster for more details.
At runtime, the getId call returns the MultiProc id of those processors within its cluster. At config-time, the getIdMeta call returns the the same value.
 
const MultiProc_INVALIDID

Invalid processor id constant

C synopsis target-domain
#define MultiProc_INVALIDID (UInt16)0xFFFF
 
DETAILS
This constant denotes that the processor id is not valid.
 
enum MultiProc_ProcAddrMode

Enumerate the Processor Addressing Modes

C synopsis target-domain
typedef enum MultiProc_ProcAddrMode {
    MultiProc_ProcAddrMode_Global,
    MultiProc_ProcAddrMode_Cluster
} MultiProc_ProcAddrMode;
 
VALUES
ProcAddrMode_Global — Every processor in the system must be directly addressable. Usually, this requires a resource allocation for each processor. This might require a dedicated hardware resource and/or a memory allocation on behalf of every processor in the sytem. For large systems, this might result in significant memory requirements. Use with caution.
ProcAddrMode_Cluster — Direct addressing is required only for the processors in your cluster. Processors outside of the cluster may share resources. This mode limits the per processor resource allocations to just the processors within your cluster. This address mode is typically used for large processor systems.
DETAILS
This enumeration defines the various processor addressing modes which might impact the behavior and resource allocations of modules that communicate with other processors in the system (i.e. IPC).
It is a way for the system integrator to control the internal behavior and resource allocations of various module to suit the needs of the program. However, it is at the discretion of each module on how to respond to these processor addressing modes.
For example, the NameServer module reflects on this mode when constructing its internal data structures. For the 'Global' mode, it will allocate a resource for every processor in the system. When using 'Cluster' mode, resources are only allocated for processors in the cluster. A side-effect is that when using Cluster mode, name queries cannot be addressed to processors outside of the cluster.
Specify the addressing mode by setting the MultiProc.procAddrMode configuration parameter.
SEE
 
config MultiProc_A_invalidMultiProcId  // module-wide

Assert raised when an invalid processor id is used

C synopsis target-domain
extern const Assert_Id MultiProc_A_invalidMultiProcId;
 
 
config MultiProc_A_invalidProcName  // module-wide

Assert raised when a NULL processor name is encountered

C synopsis target-domain
extern const Assert_Id MultiProc_A_invalidProcName;
 
 
config MultiProc_numProcessors  // module-wide

Number of processors in the system

C synopsis target-domain
extern const UInt16 MultiProc_numProcessors;
 
DETAILS
This configuration should only be set when there is more than one cluster in the system. It must be set before calling setConfig. If the system contains only one cluster, it is internally set by the setConfig meta function to the length of the supplied nameList array. After setConfig has been called, it is possible to retrive the maximum # of processors by reading this module config either at run-time or at config time.
 
config MultiProc_procAddrMode  // module-wide

Define which processor addressing mode is in operation

C synopsis target-domain
extern const MultiProc_ProcAddrMode MultiProc_procAddrMode;
 
DETAILS
This configuration parameter is reflected upon by various system components whose implementation is impacted by the processor addressing mode currently in effect. It allows modules to optimize their behavior and resource allocations for any given processor address mode.
The MultiProc module has no specific behavior associated with this configuration parameter. It is simply a convenient location for such a configuration parameter as most processor aware modules already depend on MultiProc.
SEE
Module-Wide Built-Ins

C synopsis target-domain
Types_ModuleId MultiProc_Module_id();
// Get this module's unique id
 
Bool MultiProc_Module_startupDone();
// Test if this module has completed startup
 
IHeap_Handle MultiProc_Module_heap();
// The heap from which this module allocates memory
 
Bool MultiProc_Module_hasMask();
// Test whether this module has a diagnostics mask
 
Bits16 MultiProc_Module_getMask();
// Returns the diagnostics mask for this module
 
Void MultiProc_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
 
Configuration settings sourced in ti/sdo/utils/MultiProc.xdc
var MultiProc = xdc.useModule('ti.sdo.utils.MultiProc');
module-wide constants & types
 
        const MultiProc.ProcAddrMode_Global;
        const MultiProc.ProcAddrMode_Cluster;
 
    var obj = new MultiProc.ModuleView// ;
        obj.id = UInt16  ...
        obj.numProcessors = UInt16  ...
        obj.nameList = String[]  ...
module-wide config parameters
        msg: "A_invalidMultiProcId: Invalid MultiProc id"
    };
        msg: "A_invalidProcName: NULL MultiProc name encountered"
    };
 
module-wide functions
    MultiProc.getIdMeta// Meta version of getId(String name) returns UInt16
    MultiProc.setConfig// Configure the MultiProc module(String name, String[] nameList) returns Void
 
 
const MultiProc.INVALIDID

Invalid processor id constant

Configuration settings
const MultiProc.INVALIDID = 0xFFFF;
 
DETAILS
This constant denotes that the processor id is not valid.
C SYNOPSIS
 
enum MultiProc.ProcAddrMode

Enumerate the Processor Addressing Modes

Configuration settings
values of type MultiProc.ProcAddrMode
    const MultiProc.ProcAddrMode_Global;
    const MultiProc.ProcAddrMode_Cluster;
 
VALUES
ProcAddrMode_Global — Every processor in the system must be directly addressable. Usually, this requires a resource allocation for each processor. This might require a dedicated hardware resource and/or a memory allocation on behalf of every processor in the sytem. For large systems, this might result in significant memory requirements. Use with caution.
ProcAddrMode_Cluster — Direct addressing is required only for the processors in your cluster. Processors outside of the cluster may share resources. This mode limits the per processor resource allocations to just the processors within your cluster. This address mode is typically used for large processor systems.
DETAILS
This enumeration defines the various processor addressing modes which might impact the behavior and resource allocations of modules that communicate with other processors in the system (i.e. IPC).
It is a way for the system integrator to control the internal behavior and resource allocations of various module to suit the needs of the program. However, it is at the discretion of each module on how to respond to these processor addressing modes.
For example, the NameServer module reflects on this mode when constructing its internal data structures. For the 'Global' mode, it will allocate a resource for every processor in the system. When using 'Cluster' mode, resources are only allocated for processors in the cluster. A side-effect is that when using Cluster mode, name queries cannot be addressed to processors outside of the cluster.
Specify the addressing mode by setting the MultiProc.procAddrMode configuration parameter.
SEE
C SYNOPSIS
 
metaonly struct MultiProc.ModuleView
Configuration settings
var obj = new MultiProc.ModuleView;
 
    obj.id = UInt16  ...
    obj.numProcessors = UInt16  ...
    obj.nameList = String[]  ...
 
 
config MultiProc.A_invalidMultiProcId  // module-wide

Assert raised when an invalid processor id is used

Configuration settings
MultiProc.A_invalidMultiProcId = Assert.Desc {
    msg: "A_invalidMultiProcId: Invalid MultiProc id"
};
 
C SYNOPSIS
 
config MultiProc.A_invalidProcName  // module-wide

Assert raised when a NULL processor name is encountered

Configuration settings
MultiProc.A_invalidProcName = Assert.Desc {
    msg: "A_invalidProcName: NULL MultiProc name encountered"
};
 
C SYNOPSIS
 
config MultiProc.numProcessors  // module-wide

Number of processors in the system

Configuration settings
MultiProc.numProcessors = UInt16 1;
 
DETAILS
This configuration should only be set when there is more than one cluster in the system. It must be set before calling setConfig. If the system contains only one cluster, it is internally set by the setConfig meta function to the length of the supplied nameList array. After setConfig has been called, it is possible to retrive the maximum # of processors by reading this module config either at run-time or at config time.
C SYNOPSIS
 
config MultiProc.procAddrMode  // module-wide

Define which processor addressing mode is in operation

Configuration settings
 
DETAILS
This configuration parameter is reflected upon by various system components whose implementation is impacted by the processor addressing mode currently in effect. It allows modules to optimize their behavior and resource allocations for any given processor address mode.
The MultiProc module has no specific behavior associated with this configuration parameter. It is simply a convenient location for such a configuration parameter as most processor aware modules already depend on MultiProc.
SEE
C SYNOPSIS
 
metaonly config MultiProc.baseIdOfCluster  // module-wide

The base processor ID of the cluster

Configuration settings
MultiProc.baseIdOfCluster = UInt16 0;
 
DETAILS
The ID of each processor in a cluster is computed by adding its position in the name list of setConfig to the base ID of the cluster. When more than one cluster exists in the system, this parameter must be set before calling setConfig.
 
metaonly config MultiProc.common$  // module-wide

Common module configuration parameters

Configuration settings
MultiProc.common$ = Types.Common$ undefined;
 
DETAILS
All modules have this configuration parameter. Its name contains the '$' character to ensure it does not conflict with configuration parameters declared by the module. This allows new configuration parameters to be added in the future without any chance of breaking existing modules.
 
metaonly config MultiProc.rovViewInfo  // module-wide
Configuration settings
MultiProc.rovViewInfo = ViewInfo.Instance ViewInfo.create;
 
 
metaonly MultiProc.getDeviceProcNames()  // module-wide

Returns an array of all possible processor names on the build device

Configuration settings
MultiProc.getDeviceProcNames() returns Any
 
DETAILS
@(return) Array of valid MultiProc processor names
 
metaonly MultiProc.getIdMeta()  // module-wide

Meta version of getId

Configuration settings
MultiProc.getIdMeta(String name) returns UInt16
 
ARGUMENTS
name — MultiProc procName
DETAILS
Statically returns the internally set ID based on configuration supplied via setConfig.
 
metaonly MultiProc.setConfig()  // module-wide

Configure the MultiProc module

Configuration settings
MultiProc.setConfig(String name, String[] nameList) returns Void
 
ARGUMENTS
name — MultiProc name for the local processor
nameList — Array of all processors used by the application
DETAILS
Configuration of the MultiProc module is primarily accomplished using the setConfig API at config time. The setConfig API allows the MultiProc module to identify:
  • Which is the local processor
  • Which processors are being used
  • Which processors can synchronize
The second of these two pieces of information is supplied via the nameList argument. The nameList is a non-empty set of distinct processors valid for the particular device. For a list of valid processor names for a given device, please refer to the : Table of Valid Names for Each Device.
The local processor is identified by using a single name from nameList. A MultiProc id is internally set to the index of 'name' in the supplied 'nameList'. I.e. in the example:
  MultiProc.setConfig("DSP", ["HOST", "DSP", "OTHERCORE"]);
The processors, "HOST", "DSP" and "OTHERCORE" get assigned MultiProc IDs 0, 1, and 2, respectively. The local processor, "DSP" is assigned an ID of '1'.
If the local processor is not known at static time, it is possible to supply a null name. MultiProc will set the local id to INVALIDID until it is set at runtime using MultiProc_setLocalId.
generated on Fri, 21 Aug 2015 19:36:04 GMT