interface ti.sdo.ipc.interfaces.INetworkTransport |
|
|
|
Interface for the network type of transports
interface INetworkTransport { ...
instance: ...
module-wide config parameters
instance:
per-instance creation
per-instance functions
}
metaonly config INetworkTransport.common$ // module-wide |
|
Common module configuration parameters
DETAILS
All modules have this configuration parameter. Its name
contains the '$' character to ensure it does not conflict with
configuration parameters declared by the module. This allows
new configuration parameters to be added in the future without
any chance of breaking existing modules.
Static Instance Creation |
|
create();
// Create an instance-object
INetworkTransport.bind() // instance |
|
Bind a resource for the given queueId
Int bind(UInt32 queueId);
INetworkTransport.put() // instance |
|
Send the message over the given transport instance
INetworkTransport.unbind() // instance |
|
Unbind a resource for the given queueId
Int unbind(UInt32 queueId);
generated on Fri, 21 Aug 2015 19:35:42 GMT