This module implements the
ti.sdo.ipc.interfaces.IGateMPSupport
interface using the Peterson Algorithm in shared memory. This
implementation works for N processors.
Each GatePetersonN instance requires a small piece of
shared memory. The base address of this shared memory is specified as
the 'sharedAddr' argument to the create. The amount of shared memory
consumed by a single instance can be obtained using the
sharedMemReq call.
Shared memory has to conform to the following specification. Padding is
added between certain elements in shared memory if cache alignment is
required for the region in which the instance is placed.
shmBaseAddr -> ------------------------------ bytes
| enteredStage[0] | 4
| (PADDING if aligned) |
|----------------------------|
| enteredStage[1] | 4
| (PADDING if aligned) |
|----------------------------|
. . .
|----------------------------|
| enteredStage[N-1] | 4
| (PADDING if aligned) |
|----------------------------|
| lastProcEnteringStage[1] | 4
| (PADDING if aligned) |
|----------------------------|
. . .
|----------------------------|
| lastProcEnteringStage[N-1]| 4
| (PADDING if aligned) |
|----------------------------|
const GatePetersonN_Q_BLOCKING |
|
Blocking quality
#define GatePetersonN_Q_BLOCKING (Int)1
DETAILS
Gates with this "quality" may cause the calling thread to block;
i.e., suspend execution until another thread leaves the gate.
const GatePetersonN_Q_PREEMPTING |
|
Preempting quality
#define GatePetersonN_Q_PREEMPTING (Int)2
DETAILS
Gates with this "quality" allow other threads to preempt the thread
that has already entered the gate.
config GatePetersonN_MAX_NUM_PROCS // module-wide |
|
extern const UInt GatePetersonN_MAX_NUM_PROCS;
config GatePetersonN_numInstances // module-wide |
|
Maximum number of instances supported by the GatePetersonN module
extern const UInt GatePetersonN_numInstances;
GatePetersonN_query() // module-wide |
|
Runtime test for a particular gate quality
Bool GatePetersonN_query(Int qual);
ARGUMENTS
qual
constant describing a quality
RETURNS
Returns TRUE if the gate has the given quality,
and FALSE otherwise, which includes the case when the gate does not
recognize the constant describing the quality.
GatePetersonN_sharedMemReq() // module-wide |
|
Amount of shared memory required for creation of each instance
ARGUMENTS
params
Pointer to the parameters that will be used in
the create.
DETAILS
The value returned by this function may depend on the cache alignment
requirements for the shared region from which memory will be used.
RETURNS
Number of MAUs needed to create the instance.
Module-Wide Built-Ins |
|
// Get this module's unique id
Bool GatePetersonN_Module_startupDone();
// Test if this module has completed startup
// The heap from which this module allocates memory
Bool GatePetersonN_Module_hasMask();
// Test whether this module has a diagnostics mask
Bits16 GatePetersonN_Module_getMask();
// Returns the diagnostics mask for this module
Void GatePetersonN_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
Instance Object Types |
|
typedef struct GatePetersonN_Object GatePetersonN_Object;
// Opaque internal representation of an instance object
// Client reference to an instance object
typedef struct GatePetersonN_Struct GatePetersonN_Struct;
// Opaque client structure large enough to hold an instance object
// Convert this instance structure pointer into an instance handle
// Convert this instance handle into an instance structure pointer
Instance Config Parameters |
|
typedef struct GatePetersonN_Params {
// Instance config-params structure
// Common per-instance configs
UInt resourceId;
// Logical resource id
Ptr sharedAddr;
// Physical address of the shared memory
} GatePetersonN_Params;
// Initialize this config-params structure with supplier-specified defaults before instance creation
config GatePetersonN_Params.resourceId // instance |
|
Logical resource id
config GatePetersonN_Params.sharedAddr // instance |
|
Physical address of the shared memory
DETAILS
This parameter is only used by GateMP delegates that use shared memory
Runtime Instance Creation |
|
// Allocate and initialize a new instance object and return its handle
// Initialize a new instance object inside the provided structure
ARGUMENTS
localGate
Gate to use for local protection.
params
per-instance config params, or NULL to select default values (target-domain only)
eb
active error-handling block, or NULL to select default policy (target-domain only)
DETAILS
A Non-NULL gate for local protection must be passed to the create
call. If no local protection is desired, a
xdc.runtime.GateNull handle must be passed in.
Instance Deletion |
|
// Finalize and free this previously allocated instance object, setting the referenced handle to NULL
// Finalize the instance object inside the provided structure
Instance Convertors |
|
// unconditionally move one level up the inheritance hierarchy
// conditionally move one level down the inheritance hierarchy; NULL upon failure
// unconditionally move 2 levels up the inheritance hierarchy
// conditionally move 2 levels down the inheritance hierarchy; NULL upon failure
Instance Built-Ins |
|
Int GatePetersonN_Object_count();
// The number of statically-created instance objects
// The handle of the i-th statically-created instance object (array == NULL)
// The handle of the first dynamically-created instance object, or NULL
// The handle of the next dynamically-created instance object, or NULL
// The heap used to allocate dynamically-created instance objects
// The label associated with this instance object
// The name of this instance object
const GatePetersonN.Q_BLOCKING |
|
Blocking quality
const GatePetersonN.Q_BLOCKING = 1;
DETAILS
Gates with this "quality" may cause the calling thread to block;
i.e., suspend execution until another thread leaves the gate.
C SYNOPSIS
const GatePetersonN.Q_PREEMPTING |
|
Preempting quality
const GatePetersonN.Q_PREEMPTING = 2;
DETAILS
Gates with this "quality" allow other threads to preempt the thread
that has already entered the gate.
C SYNOPSIS
config GatePetersonN.MAX_NUM_PROCS // module-wide |
|
GatePetersonN.MAX_NUM_PROCS = UInt 8;
C SYNOPSIS
config GatePetersonN.numInstances // module-wide |
|
Maximum number of instances supported by the GatePetersonN module
GatePetersonN.numInstances = UInt 512;
C SYNOPSIS
metaonly config GatePetersonN.common$ // module-wide |
|
Common module configuration parameters
DETAILS
All modules have this configuration parameter. Its name
contains the '$' character to ensure it does not conflict with
configuration parameters declared by the module. This allows
new configuration parameters to be added in the future without
any chance of breaking existing modules.
metaonly GatePetersonN.getNumResources() // module-wide |
|
Returns the number of resources offered by the GateMP delegate
GatePetersonN.getNumResources() returns UInt
metaonly GatePetersonN.queryMeta() // module-wide |
|
Configuration time test for a particular gate quality
GatePetersonN.queryMeta(Int qual) returns Bool
ARGUMENTS
qual
constant describing a quality
RETURNS
Returns TRUE if the gate has the given quality,
and FALSE otherwise, which includes the case when the gate does not
recognize the constant describing the quality.
Instance Config Parameters |
|
var params = new GatePetersonN.Params;
// Instance config-params object
params.resourceId = UInt 0;
// Logical resource id
params.sharedAddr = Ptr null;
// Physical address of the shared memory
config GatePetersonN.Params.resourceId // instance |
|
Logical resource id
var params = new GatePetersonN.Params;
...
params.resourceId = UInt 0;
C SYNOPSIS
config GatePetersonN.Params.sharedAddr // instance |
|
Physical address of the shared memory
var params = new GatePetersonN.Params;
...
params.sharedAddr = Ptr null;
DETAILS
This parameter is only used by GateMP delegates that use shared memory
C SYNOPSIS
Static Instance Creation |
|
var params =
new GatePetersonN.
Params;
// Allocate instance config-params
params.config = ...
// Assign individual configs
// Create an instance-object
ARGUMENTS
localGate
Gate to use for local protection.
params
per-instance config params, or NULL to select default values (target-domain only)
eb
active error-handling block, or NULL to select default policy (target-domain only)
DETAILS
A Non-NULL gate for local protection must be passed to the create
call. If no local protection is desired, a
xdc.runtime.GateNull handle must be passed in.