const GateMPSupportNull_Q_BLOCKING |
|
Blocking quality
#define GateMPSupportNull_Q_BLOCKING (Int)1
DETAILS
Gates with this "quality" may cause the calling thread to block;
i.e., suspend execution until another thread leaves the gate.
const GateMPSupportNull_Q_PREEMPTING |
|
Preempting quality
#define GateMPSupportNull_Q_PREEMPTING (Int)2
DETAILS
Gates with this "quality" allow other threads to preempt the thread
that has already entered the gate.
enum GateMPSupportNull_Action |
|
Error codes returned by certain calls in GateMP
typedef enum GateMPSupportNull_Action {
GateMPSupportNull_Action_NONE,
GateMPSupportNull_Action_ASSERT
} GateMPSupportNull_Action;
config GateMPSupportNull_A_invalidAction // module-wide |
|
Assert raised when trying to use GateMPSupportNull's enter or leave
extern const Assert_Id GateMPSupportNull_A_invalidAction;
config GateMPSupportNull_action // module-wide |
|
Assert if the enter and/or leave is called
GateMPSupportNull_query() // module-wide |
|
Runtime test for a particular gate quality
Bool GateMPSupportNull_query(Int qual);
ARGUMENTS
qual
constant describing a quality
RETURNS
Returns TRUE if the gate has the given quality,
and FALSE otherwise, which includes the case when the gate does not
recognize the constant describing the quality.
GateMPSupportNull_sharedMemReq() // module-wide |
|
Amount of shared memory required for creation of each instance
ARGUMENTS
params
Pointer to the parameters that will be used in
the create.
DETAILS
The value returned by this function may depend on the cache alignment
requirements for the shared region from which memory will be used.
RETURNS
Number of MAUs needed to create the instance.
Module-Wide Built-Ins |
|
// Get this module's unique id
Bool GateMPSupportNull_Module_startupDone();
// Test if this module has completed startup
// The heap from which this module allocates memory
Bool GateMPSupportNull_Module_hasMask();
// Test whether this module has a diagnostics mask
Bits16 GateMPSupportNull_Module_getMask();
// Returns the diagnostics mask for this module
Void GateMPSupportNull_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
Instance Object Types |
|
typedef struct GateMPSupportNull_Object GateMPSupportNull_Object;
// Opaque internal representation of an instance object
// Client reference to an instance object
typedef struct GateMPSupportNull_Struct GateMPSupportNull_Struct;
// Opaque client structure large enough to hold an instance object
// Convert this instance structure pointer into an instance handle
// Convert this instance handle into an instance structure pointer
Instance Config Parameters |
|
typedef struct GateMPSupportNull_Params {
// Instance config-params structure
// Common per-instance configs
UInt resourceId;
// Logical resource id
Ptr sharedAddr;
// Physical address of the shared memory
} GateMPSupportNull_Params;
// Initialize this config-params structure with supplier-specified defaults before instance creation
config GateMPSupportNull_Params.resourceId // instance |
|
Logical resource id
config GateMPSupportNull_Params.sharedAddr // instance |
|
Physical address of the shared memory
DETAILS
This parameter is only used by GateMP delegates that use shared memory
Runtime Instance Creation |
|
// Allocate and initialize a new instance object and return its handle
// Initialize a new instance object inside the provided structure
ARGUMENTS
localGate
Gate to use for local protection.
params
per-instance config params, or NULL to select default values (target-domain only)
eb
active error-handling block, or NULL to select default policy (target-domain only)
DETAILS
A Non-NULL gate for local protection must be passed to the create
call. If no local protection is desired, a
xdc.runtime.GateNull handle must be passed in.
Instance Deletion |
|
// Finalize and free this previously allocated instance object, setting the referenced handle to NULL
// Finalize the instance object inside the provided structure
Instance Convertors |
|
// unconditionally move one level up the inheritance hierarchy
// conditionally move one level down the inheritance hierarchy; NULL upon failure
// unconditionally move 2 levels up the inheritance hierarchy
// conditionally move 2 levels down the inheritance hierarchy; NULL upon failure
Instance Built-Ins |
|
Int GateMPSupportNull_Object_count();
// The number of statically-created instance objects
// The handle of the i-th statically-created instance object (array == NULL)
// The handle of the first dynamically-created instance object, or NULL
// The handle of the next dynamically-created instance object, or NULL
// The heap used to allocate dynamically-created instance objects
// The label associated with this instance object
// The name of this instance object
const GateMPSupportNull.Q_BLOCKING |
|
Blocking quality
const GateMPSupportNull.Q_BLOCKING = 1;
DETAILS
Gates with this "quality" may cause the calling thread to block;
i.e., suspend execution until another thread leaves the gate.
C SYNOPSIS
const GateMPSupportNull.Q_PREEMPTING |
|
Preempting quality
const GateMPSupportNull.Q_PREEMPTING = 2;
DETAILS
Gates with this "quality" allow other threads to preempt the thread
that has already entered the gate.
C SYNOPSIS
enum GateMPSupportNull.Action |
|
Error codes returned by certain calls in GateMP
values of type GateMPSupportNull.Action
const GateMPSupportNull.Action_NONE;
const GateMPSupportNull.Action_ASSERT;
C SYNOPSIS
config GateMPSupportNull.A_invalidAction // module-wide |
|
Assert raised when trying to use GateMPSupportNull's enter or leave
msg: "A_invalidAction: Cannot use ti.sdo.ipc.gates.GateMPSupportNull"
};
C SYNOPSIS
config GateMPSupportNull.action // module-wide |
|
Assert if the enter and/or leave is called
C SYNOPSIS
metaonly config GateMPSupportNull.common$ // module-wide |
|
Common module configuration parameters
DETAILS
All modules have this configuration parameter. Its name
contains the '$' character to ensure it does not conflict with
configuration parameters declared by the module. This allows
new configuration parameters to be added in the future without
any chance of breaking existing modules.
metaonly GateMPSupportNull.getNumResources() // module-wide |
|
Returns the number of resources offered by the GateMP delegate
GateMPSupportNull.getNumResources() returns UInt
metaonly GateMPSupportNull.queryMeta() // module-wide |
|
Configuration time test for a particular gate quality
GateMPSupportNull.queryMeta(Int qual) returns Bool
ARGUMENTS
qual
constant describing a quality
RETURNS
Returns TRUE if the gate has the given quality,
and FALSE otherwise, which includes the case when the gate does not
recognize the constant describing the quality.
Instance Config Parameters |
|
var params = new GateMPSupportNull.Params;
// Instance config-params object
params.resourceId = UInt 0;
// Logical resource id
params.sharedAddr = Ptr null;
// Physical address of the shared memory
config GateMPSupportNull.Params.resourceId // instance |
|
Logical resource id
var params = new GateMPSupportNull.Params;
...
params.resourceId = UInt 0;
C SYNOPSIS
config GateMPSupportNull.Params.sharedAddr // instance |
|
Physical address of the shared memory
var params = new GateMPSupportNull.Params;
...
params.sharedAddr = Ptr null;
DETAILS
This parameter is only used by GateMP delegates that use shared memory
C SYNOPSIS
Static Instance Creation |
|
var params =
new GateMPSupportNull.
Params;
// Allocate instance config-params
params.config = ...
// Assign individual configs
// Create an instance-object
ARGUMENTS
localGate
Gate to use for local protection.
params
per-instance config params, or NULL to select default values (target-domain only)
eb
active error-handling block, or NULL to select default policy (target-domain only)
DETAILS
A Non-NULL gate for local protection must be passed to the create
call. If no local protection is desired, a
xdc.runtime.GateNull handle must be passed in.