const InterruptArp32_NUM_CORES |
|
#define InterruptArp32_NUM_CORES (UInt8)11
const InterruptArp32_NUM_EVES |
|
#define InterruptArp32_NUM_EVES (UInt8)4
const InterruptArp32_NUM_EVE_MBX |
|
#define InterruptArp32_NUM_EVE_MBX (UInt8)12
const InterruptArp32_NUM_SYS_MBX |
|
#define InterruptArp32_NUM_SYS_MBX (UInt8)4
struct InterruptArp32_IntInfo |
|
typedef struct InterruptArp32_IntInfo {
UInt localIntId;
UInt remoteIntId;
UInt intVectorId;
} InterruptArp32_IntInfo;
config InterruptArp32_mailboxBaseAddr // module-wide |
|
InterruptArp32_intClear() // module-wide |
|
Clear interrupt
ARGUMENTS
remoteProcId
Remote MultiProc Id
intInfo
Information needed to configure interrupt line
RETURNS
Value (if any) of the interrupt before
it was cleared
InterruptArp32_intDisable() // module-wide |
|
Disables the interrupt corresponding to intId
ARGUMENTS
remoteProcId
Remote MultiProc Id
intInfo
Information needed to configure interrupt line
InterruptArp32_intEnable() // module-wide |
|
Enables the interrupt corresponding to intId
ARGUMENTS
remoteProcId
Remote MultiProc Id
intInfo
Information needed to configure interrupt line
InterruptArp32_intRegister() // module-wide |
|
Register an interrupt line to a remote processor
Void InterruptArp32_intRegister(
UInt16 remoteProcId,
IInterrupt_IntInfo *
intInfo,
Fxn func,
UArg arg);
ARGUMENTS
remoteProcId
Remote MultiProc Id
intInfo
Information needed to configure interrupt line
func
Function to register.
arg
Argument that will be passed to func
InterruptArp32_intSend() // module-wide |
|
Send interrupt to the remote processor
ARGUMENTS
remoteProcId
Remote MultiProc Id
intInfo
Information needed to configure interrupt line
arg
Argument for sending interrupt.
InterruptArp32_intUnregister() // module-wide |
|
Unregister an interrupt line to a remote processor
ARGUMENTS
remoteProcId
Remote MultiProc Id
intInfo
Information needed to configure interrupt line
Module-Wide Built-Ins |
|
// Get this module's unique id
Bool InterruptArp32_Module_startupDone();
// Test if this module has completed startup
// The heap from which this module allocates memory
Bool InterruptArp32_Module_hasMask();
// Test whether this module has a diagnostics mask
Bits16 InterruptArp32_Module_getMask();
// Returns the diagnostics mask for this module
Void InterruptArp32_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module