Notification manager
This module has a common header that can be found in the
ti.ipc
package. Application code should include the common header file (not the
RTSC-generated one):
#include <ti/ipc/Notify.h>
The RTSC module must be used in the application's RTSC configuration file
(.cfg) if runtime APIs will be used in the application:
Notify = xdc.useModule('ti.sdo.ipc.Notify');
Documentation for all runtime APIs, instance configuration parameters,
error codes macros and type definitions available to the application
integrator can be found in the
Doxygen documenation
for the IPC product. However, the documentation presented on this page
should be referred to for information specific to the RTSC module, such as
module configuration, Errors, and Asserts.
[
more ... ]
#include <ti/sdo/ipc/Notify.h>
Functions |
Void | |
Functions common to all target instances |
|
Notify_handle// Convert this instance structure pointer into an instance handle,
Notify_Handle_label// The label associated with this instance object,
Notify_Handle_name// The name of this instance object,
Notify_Object_count// The number of statically-created instance objects,
Notify_Object_first// The handle of the first dynamically-created instance object, or NULL,
Notify_Object_get// The handle of the i-th statically-created instance object (array == NULL),
Notify_Object_heap// The heap used to allocate dynamically-created instance objects,
Notify_Object_next// The handle of the next dynamically-created instance object, or NULL,
Notify_struct// Convert this instance handle into an instance structure pointer
|
Functions common to all target modules |
|
|
Defines |
#define | |
Typedefs |
| |
typedef struct | |
typedef struct | |
typedef struct | |
Constants |
| |
| |
| |
| |
| |
| |
extern const UInt | |
extern const UInt16 | |
extern const UInt32 | |
DETAILS
This module has a common header that can be found in the
ti.ipc
package. Application code should include the common header file (not the
RTSC-generated one):
#include <ti/ipc/Notify.h>
The RTSC module must be used in the application's RTSC configuration file
(.cfg) if runtime APIs will be used in the application:
Notify = xdc.useModule('ti.sdo.ipc.Notify');
Documentation for all runtime APIs, instance configuration parameters,
error codes macros and type definitions available to the application
integrator can be found in the
Doxygen documenation
for the IPC product. However, the documentation presented on this page
should be referred to for information specific to the RTSC module, such as
module configuration, Errors, and Asserts.
The Notify module typically doesn't require much (if any) configuration at
static time. However, it is possible to reduce the amount of shared memory
used by the Notify subsystem by reducing the value of
numEvents.
const Notify_MAXEVENTS |
|
Maximum number of events supported by the Notify module
#define Notify_MAXEVENTS (UInt)32
config Notify_A_alreadyRegistered // module-wide |
|
Assert raised when trying to re-register for given line and processor
extern const Assert_Id Notify_A_alreadyRegistered;
config Notify_A_internal // module-wide |
|
Assert raised when an internal error is encountered
config Notify_A_invArgument // module-wide |
|
Assert raised when an argument is invalid
config Notify_A_notRegistered // module-wide |
|
Assert raised when trying to use an unregistered Notify instance
extern const Assert_Id Notify_A_notRegistered;
config Notify_A_outOfOrderNesting // module-wide |
|
Assert raised when restore called with improper key
extern const Assert_Id Notify_A_outOfOrderNesting;
config Notify_A_reservedEvent // module-wide |
|
Assert raised when trying to improperly use a reserved event
extern const Assert_Id Notify_A_reservedEvent;
config Notify_numEvents // module-wide |
|
Number of events supported by Notify
extern const UInt Notify_numEvents;
DETAILS
Lowering this value offers the benefit of lower footprint especially in
shared memory.
config Notify_reservedEvents // module-wide |
|
Number of reserved event numbers
extern const UInt16 Notify_reservedEvents;
DETAILS
The first reservedEvents event numbers are reserved for
middleware modules. Attempts to use these reserved events
will result in a
A_reservedEvent assert.
To use the reserved events, the top 16-bits of the eventId must equal
Notify_SYSTEMKEY.
config Notify_sendEventPollCount // module-wide |
|
Poll for specified amount before sendEvent times out
extern const UInt32 Notify_sendEventPollCount;
DETAILS
Setting a finite value for sendEventPollCount will cause
Notify_sendEvent to poll for an amount of time
proportional to this value when the 'waitClear' flag is TRUE.
Module-Wide Built-Ins |
|
// Get this module's unique id
Bool Notify_Module_startupDone();
// Test if this module has completed startup
// The heap from which this module allocates memory
Bool Notify_Module_hasMask();
// Test whether this module has a diagnostics mask
Bits16 Notify_Module_getMask();
// Returns the diagnostics mask for this module
Void Notify_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
Instance Object Types |
|
typedef struct Notify_Object Notify_Object;
// Opaque internal representation of an instance object
// Client reference to an instance object
typedef struct Notify_Struct Notify_Struct;
// Opaque client structure large enough to hold an instance object
// Convert this instance structure pointer into an instance handle
// Convert this instance handle into an instance structure pointer
Instance Config Parameters |
|
typedef struct Notify_Params {
// Instance config-params structure
// Common per-instance configs
} Notify_Params;
// Initialize this config-params structure with supplier-specified defaults before instance creation
Instance Built-Ins |
|
Int Notify_Object_count();
// The number of statically-created instance objects
// The handle of the i-th statically-created instance object (array == NULL)
// The handle of the first dynamically-created instance object, or NULL
// The handle of the next dynamically-created instance object, or NULL
// The heap used to allocate dynamically-created instance objects
// The label associated with this instance object
// The name of this instance object
var Notify = xdc.useModule('ti.sdo.ipc.Notify');
local proxy modules
module-wide constants & types
module-wide config parameters
msg: "A_alreadyRegistered: Notify instance for the processor/line already registered"
};
msg: "A_internal: An internal error has occurred"
};
msg: "A_invArgument: Invalid argument supplied"
};
msg: "A_notRegistered: Notify instance not yet registered for the processor/line"
};
msg: "A_outOfOrderNesting: Out of order nesting"
};
msg: "A_reservedEvent: Improper use of a reserved event"
};
per-instance config parameters
proxy Notify.SetupProxy |
|
Device-specific Notify setup proxy
// some delegate module inheriting the
INotifySetup interface
// explicit access to the currently bound delegate module
const Notify.MAXEVENTS |
|
Maximum number of events supported by the Notify module
const Notify.MAXEVENTS = 32;
C SYNOPSIS
config Notify.A_alreadyRegistered // module-wide |
|
Assert raised when trying to re-register for given line and processor
msg: "A_alreadyRegistered: Notify instance for the processor/line already registered"
};
C SYNOPSIS
config Notify.A_internal // module-wide |
|
Assert raised when an internal error is encountered
msg: "A_internal: An internal error has occurred"
};
C SYNOPSIS
config Notify.A_invArgument // module-wide |
|
Assert raised when an argument is invalid
msg: "A_invArgument: Invalid argument supplied"
};
C SYNOPSIS
config Notify.A_notRegistered // module-wide |
|
Assert raised when trying to use an unregistered Notify instance
msg: "A_notRegistered: Notify instance not yet registered for the processor/line"
};
C SYNOPSIS
config Notify.A_outOfOrderNesting // module-wide |
|
Assert raised when restore called with improper key
msg: "A_outOfOrderNesting: Out of order nesting"
};
C SYNOPSIS
config Notify.A_reservedEvent // module-wide |
|
Assert raised when trying to improperly use a reserved event
msg: "A_reservedEvent: Improper use of a reserved event"
};
C SYNOPSIS
config Notify.numEvents // module-wide |
|
Number of events supported by Notify
Notify.numEvents = UInt 32;
DETAILS
Lowering this value offers the benefit of lower footprint especially in
shared memory.
C SYNOPSIS
config Notify.reservedEvents // module-wide |
|
Number of reserved event numbers
Notify.reservedEvents = UInt16 5;
DETAILS
The first reservedEvents event numbers are reserved for
middleware modules. Attempts to use these reserved events
will result in a
A_reservedEvent assert.
To use the reserved events, the top 16-bits of the eventId must equal
Notify_SYSTEMKEY.
C SYNOPSIS
config Notify.sendEventPollCount // module-wide |
|
Poll for specified amount before sendEvent times out
Notify.sendEventPollCount = UInt32 -1;
DETAILS
Setting a finite value for sendEventPollCount will cause
Notify_sendEvent to poll for an amount of time
proportional to this value when the 'waitClear' flag is TRUE.
C SYNOPSIS
metaonly config Notify.common$ // module-wide |
|
Common module configuration parameters
DETAILS
All modules have this configuration parameter. Its name
contains the '$' character to ensure it does not conflict with
configuration parameters declared by the module. This allows
new configuration parameters to be added in the future without
any chance of breaking existing modules.
metaonly config Notify.rovViewInfo // module-wide |
|
Instance Config Parameters |
|
var params = new Notify.Params;
// Instance config-params object
generated on Fri, 21 Aug 2015 19:35:36 GMT