IPC API  3.10.02.13
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
Data Fields
SharedRegion_Entry Struct Reference

Structure defining a region. More...

#include <SharedRegion.h>

Collaboration diagram for SharedRegion_Entry:
Collaboration graph

Data Fields

Ptr base
 The base address of the region.
SizeT len
 The length of the region.
UInt16 ownerProcId
 The MultiProc id of the owner of the region.
Bool isValid
 Whether the region is valid.
Bool cacheEnable
 Whether to perform cache operations for the region.
SizeT cacheLineSize
 The cache line size of the region.
Bool createHeap
 Whether a heap is created for the region.
String name
 The name of the region.

Detailed Description

Structure defining a region.


Field Documentation

Ptr SharedRegion_Entry::base

The base address of the region.

SizeT SharedRegion_Entry::len

The length of the region.

The length of a region must be the same across all processors in the system.

UInt16 SharedRegion_Entry::ownerProcId

The MultiProc id of the owner of the region.

The owner id for a shared region must be the same across all processors in the system.

Bool SharedRegion_Entry::isValid

Whether the region is valid.

Bool SharedRegion_Entry::cacheEnable

Whether to perform cache operations for the region.

If 'TRUE', a cache invalidate is performed before any read and a cache write back invalidate is performed after any write for the shared region. The cache operations are done for all caches. If 'FALSE', no cache operations are performed.

SizeT SharedRegion_Entry::cacheLineSize

The cache line size of the region.

The cache line size for a region must be the same across all processors in the system. It is used for structure alignment and padding.

Bool SharedRegion_Entry::createHeap

Whether a heap is created for the region.

If 'TRUE', a HeapMemMP instance is created with the size spanning the length of the shared region minus any memory that is reserved in the region. If 'FALSE', no heap is created in the shared region.

String SharedRegion_Entry::name

The name of the region.

The name must be in persistent memory. It is used for displaying in ROV.


The documentation for this struct was generated from the following file:
Copyright 2013, Texas Instruments Incorporated