IPC API
3.10.02.13
|
Multi-processor fixed-size buffer heap implementation.
Heap implementation that manages fixed size buffers that can be used in a multiprocessor system with shared memory.
The HeapBufMP manager provides functions to allocate and free storage from a heap of type HeapBufMP which inherits from IHeap. HeapBufMP manages a single fixed-size buffer, split into equally sized allocatable blocks.
The HeapBufMP manager is intended as a very fast memory manager which can only allocate blocks of a single size. It is ideal for managing a heap that is only used for allocating a single type of object, or for objects that have very similar sizes.
The HeapBufMP module uses a NameServer instance to store instance information when an instance is created. The name supplied must be unique for all HeapBufMP instances.
HeapBufMP_create() initializes the shared memory as needed. Once an instance is created, HeapBufMP_open() can be performed. The open is used to gain access to the same HeapBufMP instance. Generally an instance is created on one processor and opened on the other processor(s).
The open returns a HeapBufMP instance handle like the create, however the open does not modify the shared memory.
The HeapBufMP header should be included in an application as follows:
#include <ti/ipc/GateMP.h>
Go to the source code of this file.
Data Structures | |
struct | HeapBufMP_Params |
Structure defining parameters for the HeapBufMP module. More... | |
struct | HeapBufMP_ExtendedStats |
Stats structure for HeapBufMP_getExtendedStats() More... |
Macros | |
#define | HeapBufMP_S_BUSY 2 |
The resource is still in use. | |
#define | HeapBufMP_S_ALREADYSETUP 1 |
The module has been already setup. | |
#define | HeapBufMP_S_SUCCESS 0 |
Operation is successful. | |
#define | HeapBufMP_E_FAIL -1 |
Generic failure. | |
#define | HeapBufMP_E_INVALIDARG -2 |
Argument passed to function is invalid. | |
#define | HeapBufMP_E_MEMORY -3 |
Operation resulted in memory failure. | |
#define | HeapBufMP_E_ALREADYEXISTS -4 |
The specified entity already exists. | |
#define | HeapBufMP_E_NOTFOUND -5 |
Unable to find the specified entity. | |
#define | HeapBufMP_E_TIMEOUT -6 |
Operation timed out. | |
#define | HeapBufMP_E_INVALIDSTATE -7 |
Module is not initialized. | |
#define | HeapBufMP_E_OSFAILURE -8 |
A failure occurred in an OS-specific call. | |
#define | HeapBufMP_E_RESOURCE -9 |
Specified resource is not available. | |
#define | HeapBufMP_E_RESTART -10 |
Operation was interrupted. Please restart the operation. |
Typedefs | |
typedef struct HeapBufMP_Object * | HeapBufMP_Handle |
HeapBufMP_Handle type. | |
typedef struct HeapBufMP_Params | HeapBufMP_Params |
Structure defining parameters for the HeapBufMP module. | |
typedef struct HeapBufMP_ExtendedStats | HeapBufMP_ExtendedStats |
Stats structure for HeapBufMP_getExtendedStats() |
Functions | |
Int | HeapBufMP_close (HeapBufMP_Handle *handlePtr) |
Close a HeapBufMP instance. | |
HeapBufMP_Handle | HeapBufMP_create (const HeapBufMP_Params *params) |
Create a HeapBufMP instance. | |
Int | HeapBufMP_delete (HeapBufMP_Handle *handlePtr) |
Delete a created HeapBufMP instance. | |
Int | HeapBufMP_open (String name, HeapBufMP_Handle *handlePtr) |
Open a created HeapBufMP instance. | |
Void | HeapBufMP_Params_init (HeapBufMP_Params *params) |
Initialize a HeapBufMP parameters struct. | |
Void * | HeapBufMP_alloc (HeapBufMP_Handle handle, SizeT size, SizeT align) |
Allocate a block of memory of specified size and alignment. | |
Void | HeapBufMP_free (HeapBufMP_Handle handle, Ptr block, SizeT size) |
Frees a block of memory. | |
Void | HeapBufMP_getExtendedStats (HeapBufMP_Handle handle, HeapBufMP_ExtendedStats *stats) |
Get extended memory statistics. | |
Void | HeapBufMP_getStats (HeapBufMP_Handle handle, Ptr stats) |
Get memory statistics. |
#define HeapBufMP_S_BUSY 2 |
The resource is still in use.
#define HeapBufMP_S_ALREADYSETUP 1 |
The module has been already setup.
#define HeapBufMP_S_SUCCESS 0 |
Operation is successful.
#define HeapBufMP_E_FAIL -1 |
Generic failure.
#define HeapBufMP_E_INVALIDARG -2 |
Argument passed to function is invalid.
#define HeapBufMP_E_MEMORY -3 |
Operation resulted in memory failure.
#define HeapBufMP_E_ALREADYEXISTS -4 |
The specified entity already exists.
#define HeapBufMP_E_NOTFOUND -5 |
Unable to find the specified entity.
#define HeapBufMP_E_TIMEOUT -6 |
Operation timed out.
#define HeapBufMP_E_INVALIDSTATE -7 |
Module is not initialized.
#define HeapBufMP_E_OSFAILURE -8 |
A failure occurred in an OS-specific call.
#define HeapBufMP_E_RESOURCE -9 |
Specified resource is not available.
#define HeapBufMP_E_RESTART -10 |
Operation was interrupted. Please restart the operation.
typedef struct HeapBufMP_Object* HeapBufMP_Handle |
HeapBufMP_Handle type.
typedef struct HeapBufMP_Params HeapBufMP_Params |
Structure defining parameters for the HeapBufMP module.
typedef struct HeapBufMP_ExtendedStats HeapBufMP_ExtendedStats |
Stats structure for HeapBufMP_getExtendedStats()
Int HeapBufMP_close | ( | HeapBufMP_Handle * | handlePtr | ) |
Close a HeapBufMP instance.
Closing an instance will free local memory consumed by the opened instance. All opened instances should be closed before the instance is deleted.
[in,out] | handlePtr | Pointer to handle returned from HeapBufMP_open() |
HeapBufMP_Handle HeapBufMP_create | ( | const HeapBufMP_Params * | params | ) |
Create a HeapBufMP instance.
[in] | params | HeapBufMP parameters |
Int HeapBufMP_delete | ( | HeapBufMP_Handle * | handlePtr | ) |
Delete a created HeapBufMP instance.
[in,out] | handlePtr | Pointer to handle to delete. |
Int HeapBufMP_open | ( | String | name, |
HeapBufMP_Handle * | handlePtr | ||
) |
Open a created HeapBufMP instance.
Once an instance is created, an open can be performed. The open is used to gain access to the same HeapBufMP instance. Generally an instance is created on one processor and opened on the other processor.
The open returns a HeapBufMP instance handle like the create, however the open does not initialize the shared memory. The supplied name is used to identify the created instance.
Call HeapBufMP_close when the opened instance is not longer needed.
[in] | name | Name of created HeapBufMP instance |
[out] | handlePtr | Pointer to HeapBufMP handle to be opened |
Void HeapBufMP_Params_init | ( | HeapBufMP_Params * | params | ) |
Initialize a HeapBufMP parameters struct.
[out] | params | Pointer to creation parameters |
Void* HeapBufMP_alloc | ( | HeapBufMP_Handle | handle, |
SizeT | size, | ||
SizeT | align | ||
) |
Allocate a block of memory of specified size and alignment.
The actual block returned may be larger than requested to satisfy alignment requirements. NULL is returned if the allocation fails.
HeapBufMP_alloc() will lock the heap using the HeapBufMP gate while it traverses the list of free blocks to find a large enough block for the request.
Guidelines for using large heaps and multiple alloc() calls.
[in] | handle | Handle to previously created/opened instance. |
[in] | size | Size to be allocated (in MADUs) |
[in] | align | Alignment for allocation (power of 2) |
Void HeapBufMP_free | ( | HeapBufMP_Handle | handle, |
Ptr | block, | ||
SizeT | size | ||
) |
Frees a block of memory.
HeapBufMP_free() places the memory block specified by addr and size back into the free pool of the heap specified. The newly freed block is combined with any adjacent free blocks. The space is then available for future allocations.
HeapBufMP_free() will lock the heap using the HeapBufMP gate if one is specified or the system GateMP if not.
[in] | handle | Handle to previously created/opened instance. |
[in] | block | Block of memory to be freed. |
[in] | size | Size to be freed (in MADUs) |
Void HeapBufMP_getExtendedStats | ( | HeapBufMP_Handle | handle, |
HeapBufMP_ExtendedStats * | stats | ||
) |
Get extended memory statistics.
This function retrieves extended statistics for a HeapBufMP instance. Refer to HeapBufMP_ExtendedStats for more information regarding what information is returned.
In SYS/BIOS, HeapBufMP.trackAllocs needs to be set to 'true' in the configuration to get meaningful extended stats.
[in] | handle | Handle to previously created/opened instance. |
[out] | stats | ExtendedStats structure |
Void HeapBufMP_getStats | ( | HeapBufMP_Handle | handle, |
Ptr | stats | ||
) |
Get memory statistics.
[in] | handle | Handle to previously created/opened instance. |
[out] | stats | Memory statistics structure |