HeapBufMP_ExtendedStats Struct Reference

Stats structure for the HeapBufMP_getExtendedStats API. More...

#include <HeapBufMP.h>

Data Fields

UInt maxAllocatedBlocks
UInt numAllocatedBlocks

Detailed Description

Stats structure for the HeapBufMP_getExtendedStats API.


Field Documentation

The maximum number of blocks allocated from this heap at any point in time during the lifetime of this HeapBufMP instance.

The total number of blocks currently allocated in this HeapBufMP instance.


The documentation for this struct was generated from the following file:

Copyright 2011, Texas Instruments Incorporated