![]() |
![]() |
| GateMP_Params | Structure defining parameters for the GateMP module |
| HeapBufMP_ExtendedStats | Stats structure for the HeapBufMP_getExtendedStats API |
| HeapBufMP_Params | Structure defining parameters for the HeapBufMP module |
| HeapMemMP_ExtendedStats | Stats structure for the HeapMemMP_getExtendedStats API |
| HeapMemMP_Params | Structure defining parameters for the HeapMemMP module |
| HeapMultiBufMP_Bucket | Structure for bucket configuration |
| HeapMultiBufMP_ExtendedStats | Stats structure for the HeapMultiBufMP_getExtendedStats API |
| HeapMultiBufMP_Params | Structure defining parameters for the HeapMultiBufMP module |
| HeapQueueMgr_Params | Structure defining parameters for the HeapQueueMgr module |
| ListMP_Elem | Structure defining a ListMP element |
| ListMP_Params | Structure defining parameter structure for ListMP_create() |
| MessageQ_MsgHeader | Required first field in every message |
| MessageQ_Params | Structure defining parameters for the MessageQ module |
| NameServer_Params | NameServer_Handle type |
| SharedRegion_Entry | Structure defining a region |