SHMBUF_Params Struct Reference
[Shared Memory Buffer Protocol]

SHMBUF specific params. More...

#include <shmbuf.h>

Collaboration diagram for SHMBUF_Params:
Collaboration graph
[legend]

Data Fields

IRESMAN_Params iresConfig
Int bufsize
UInt32 key
UInt32 isScratch

Detailed Description

SHMBUF specific params.

Remarks:
This struct extends IRESMAN_Params. These params are used to initialize the resource.

Field Documentation


The documentation for this struct was generated from the following file:

Copyright 2010, Texas Instruments Incorporated