Descriptor to Logical Resource. More...
#include <ires_common.h>
Data Fields | |
String | resourceName |
struct IRES_ProtocolArgs * | protocolArgs |
IRES_ProtocolRevision * | revision |
struct IRES_Obj * | handle |
Descriptor to Logical Resource.
String containing the package name to identify the resource.
struct IRES_ProtocolArgs* IRES_ResourceDescriptor::protocolArgs [read] |
Pointer to the Resource Protocol Arguments. The Resource Manager selects the appropriate Resource Protocol based on the supplied "resourceName", and uses the protocol to construct the IRES Resource Handle.
The revision of the IRES_ResourceProtocol Interface expected by the client algorithm.
struct IRES_Obj* IRES_ResourceDescriptor::handle [read] |
The handle to the object representing the requested resource. The handle is initially set to 'null' by the requesting algorithm. The 'resource manager' allocates the resource and constructs the handle.