Framework Components Application Programming Interface (API)
fc-v04
|
IRES_Obj holds the private state associated with each logical resource. More...
#include <ires_common.h>
Data Fields | |
Int32 | persistent |
Void(* | getStaticProperties )(struct IRES_Obj *resourceHandle, IRES_Properties *resourceProperties) |
IRES_Obj holds the private state associated with each logical resource.
Int32 IRES_Obj::persistent |
Indicates if the resource has been allocated as persistent.
Void(* IRES_Obj::getStaticProperties) (struct IRES_Obj *resourceHandle, IRES_Properties *resourceProperties) |
Obtain the static properties associated with this resource This could include information like the register layer of the device etc.