Framework Components Application Programming Interface (API)  fc-v04
Data Fields
ECPY_Params Struct Reference

DMA transfer specific parameters. Defines the configuration of a logical channel. More...

#include <ecpy.h>

Collaboration diagram for ECPY_Params:
Collaboration graph

Data Fields

ECPY_TransferType transferType
 
Void * srcAddr
 
Void * dstAddr
 
unsigned short elementSize
 
unsigned short numElements
 
unsigned short numFrames
 
short srcElementIndex
 
short dstElementIndex
 
short srcFrameIndex
 
short dstFrameIndex
 

Detailed Description

DMA transfer specific parameters. Defines the configuration of a logical channel.

Field Documentation

ECPY_TransferType ECPY_Params::transferType

1D1D, 1D2D, 2D1D or 2D2D

Void* ECPY_Params::srcAddr

Source Address of the DMA transfer

Void* ECPY_Params::dstAddr

Destination Address of the DMA transfer

unsigned short ECPY_Params::elementSize

Number of consecutive bytes in each 1D transfer vector (ACNT)

unsigned short ECPY_Params::numElements

Number of 1D vectors in 2D transfers (BCNT)

unsigned short ECPY_Params::numFrames

Number of 1D1D, 1D2D, 2D1D or 2D2D frames to transfer (CCNT)

short ECPY_Params::srcElementIndex

Offset in number of bytes from beginning of each 1D vector to the beginning of the next 1D vector. (SBIDX)

short ECPY_Params::dstElementIndex

Offset in number of bytes from beginning of each 1D vector to the beginning of the next 1D vector. (DBIDX)

short ECPY_Params::srcFrameIndex

Offset in number of bytes from beginning of 1D vector of current (source) frame to the beginning of next frame's first 1D vector. (SCIDX): signed value between -32768 and 32767.

short ECPY_Params::dstFrameIndex

Offset in number of bytes from beginning of 1D vector of current (destination) frame to the beginning of next frame's first 1D vector. (DCIDX): signed value between -32768 and 32767.


The documentation for this struct was generated from the following file:
Copyright 2015, Texas Instruments Incorporated