Framework Components Application Programming Interface (API)
fc-v04
|
IRES generic Resource Manager RMAN Definitions - Generic Resource Manager that manages resource allocation for algorithms that implement the IRES interface.
Go to the source code of this file.
Functions | |
IRES_Status | RMAN_init (Void) |
Initialize the RMAN object with static information from the headers/configuration etc. This function has to return successfully before the other APIs are called. More... | |
IRES_Status | RMAN_exit (Void) |
Delete the generic IRES RMAN and release memory back. More... | |
IRES_Status | RMAN_register (IRESMAN_Fxns *resmanFxns, IRESMAN_Params *initArgs) |
Register the protocol/protocol revision and the device specific resource manager implementation with the Resource Registry of the RMAN. More... | |
IRES_Status | RMAN_unregister (IRESMAN_Fxns *resmanFxns) |
Unregister the protocol and the corresponding resource manager implementation from the Resource Registry. More... | |
IRES_Status | RMAN_assignResources (IALG_Handle algHandle, IRES_Fxns *resFxns, Int scratchGroupId) |
Assign resources to the algorithm indicated by algHandle. The resource requirements can be determined by using the IRES_Fxns implementation. More... | |
IRES_Status | RMAN_allocateResources (Int requestId, IRES_ResourceDescriptor *resDesc, Int numResources, Int scratchGroupId) |
Directly allocate IRES resources by client without implementing IRES_Fxns. More... | |
IRES_Status | RMAN_freeResources (IALG_Handle algHandle, IRES_Fxns *resFxns, Int scratchGroupId) |
Free resources held by the algorithm resource handle. More... | |
IRES_Status | RMAN_freeAllocatedResources (Int requestId, IRES_ResourceDescriptor *resDesc, Int numResources, Int scratchGroupId) |
Free resources held by the algorithm resource handle. More... | |
IRES_Status | RMAN_activateResource (IALG_Handle algHandle, IRES_Handle resourceHandle, IRES_Fxns *resFxns, Int scratchGroupId) |
Activate resource identified by the resourceHandle held by the algorithm. More... | |
IRES_Status | RMAN_activateAllResources (IALG_Handle algHandle, IRES_Fxns *resFxns, Int scratchGroupId) |
Activate all resources held by the algorithm. More... | |
IRES_Status | RMAN_deactivateResource (IALG_Handle algHandle, IRES_Handle resourceHandle, IRES_Fxns *resFxns, Int scratchGroupId) |
Deactivate resource identified by the resourceHandle held by the algorithm. More... | |
IRES_Status | RMAN_deactivateAllResources (IALG_Handle algHandle, IRES_Fxns *resFxns, Int scratchGroupId) |
Deactivate all resources held by the algorithm. More... | |
void | RMAN_yield (IRES_YieldResourceType resource, IRES_YieldContextHandle algYieldContext, IRES_YieldArgs yieldArgs) |
Yield function specifically for use when DSKT2 based algorithms need cooperative preemption and multi-tasking support This function is called by the algorithm at pre-determined points during its execution, to allow another algorithm of same, or higher prioirty to preempt its execution. More... | |
Macros | |
#define | ti_sdo_fc_ires_NOPROTOCOLREV |
#define | RMAN_MODNAME "ti.sdo.fc.rman" |
Name to pass to Diags_setMask() to enable logging for RMAN functions. For example, Diags_setMask(RMAN_MODNAME"+EX1234567"); turns on all Log statements in this module. Diags_setMask() must be called after initialization to take effect. More... | |
#define | RMAN_GTNAME "ti.sdo.fc.rman" |
Name used to identify the GT module. More... | |
#define | RMAN_PROTOCOLNAMESIZE 200 |
Size of the Protocol Name in the Resource Registry Table. More... | |
Data Structures | |
struct | RMAN_Params |
The module configuration structure for RMAN. It is set at design time by the system integrator to register the specific Resource Managers(IRESMAN implementations). More... | |
Typedefs | |
typedef struct Sem_Obj * | RMAN_SemHandle |
Declare abstract handle for Semaphore object. More... | |
typedef IRES_YieldArgs(* | ti_sdo_fc_rman_RMAN_YieldArgsFxn) (Int scratchId, Bool yieldFlag) |
Type declaration for the "yield fxn" which is required if if RMAN has been configured to yield execution to same/higher priority algorithms. More... | |
typedef struct RMAN_Params | RMAN_Params |
The module configuration structure for RMAN. It is set at design time by the system integrator to register the specific Resource Managers(IRESMAN implementations). More... | |
Variables | |
__FAR__ RMAN_Params | RMAN_PARAMS |
Initialization parameters for the generic Resource Manager. More... | |
__FAR__ IRESMAN_Fxns * | RMAN_TABLE [] |
RMAN Table to hold IRESMAN registrations. More... | |
__FAR__ short | RMAN_FREE_ENTRIES [] |
Free Table to hold entries freed from RMAN Table. More... | |
__FAR__ short | RMAN_numRegistryEntries |
Number of entries statically configured for the Resource Registry table. Set this variable to zero if no static configuration is required. More... | |
__FAR__ IRESMAN_Fxns ** | RMAN_registryEntries |
To allow for static configuration of the Resource Registry table this can be set to a valid configuration table or to NULL. Set this variable to NULL if no static configuration is required. More... | |
__FAR__ IRESMAN_Params ** | RMAN_registryResmanArgs |
Initialization arguments for the entries to be registered Set this variable to NULL if no static configuration is required. More... | |
__FAR__ unsigned int ** | RMAN_iresVTable |
Table that holds the mapping from algorithms IALG_Fxns to IRES_Fxns. More... | |
__FAR__ unsigned int | ti_sdo_fc_rman_RMAN_MAXALGS |
Maximum number of algorithm instances that will use RMAN. More... | |
UInt32 | ti_sdo_fc_rman_RMAN_ipcKey |
Base key value ofr RMAN Linux IPC Objects. More... | |
ti_sdo_fc_rman_RMAN_YieldArgsFxn | ti_sdo_fc_rman_RMAN_setYieldArgs |
Function to set yield arguments to pass to yield function set in RMAN_PARAMS. More... | |
#define ti_sdo_fc_ires_NOPROTOCOLREV |