Framework Components Application Programming Interface (API)
fc-v02
|
Configuration Parameters required by the Resource Manager implementation. These can be extended by individual resource managers if required. More...
#include <iresman.h>
Data Fields | |
Int32 | size |
IRESMAN_PersistentAllocFxn * | allocFxn |
Function to allocate memory required by the resource manager implementation and the protocol. More... | |
IRESMAN_PersistentFreeFxn * | freeFxn |
Function to free memory released by the resource manager implementation and the protocol. More... | |
Configuration Parameters required by the Resource Manager implementation. These can be extended by individual resource managers if required.
Int32 IRESMAN_Params::size |
Size of this structure
IRESMAN_PersistentAllocFxn* IRESMAN_Params::allocFxn |
Function to allocate memory required by the resource manager implementation and the protocol.
IRESMAN_PersistentFreeFxn* IRESMAN_Params::freeFxn |
Function to free memory released by the resource manager implementation and the protocol.