Framework Components Application Programming Interface (API)  fc-v02
Data Fields
IRES_TILEDMEMORY_ProtocolArgs Struct Reference

TILEDMEMORY Protocol Arguments definition. More...

#include <ires_tiledmemory.h>

Collaboration diagram for IRES_TILEDMEMORY_ProtocolArgs:
Collaboration graph

Data Fields

IRES_ProtocolArgs base
 
XDAS_UInt32 accessDimension
 
XDAS_UInt32 accessUnit
 
int sizeDim0
 
int sizeDim1
 
int alignment
 

Detailed Description

TILEDMEMORY Protocol Arguments definition.

Field Documentation

IRES_ProtocolArgs IRES_TILEDMEMORY_ProtocolArgs::base
XDAS_UInt32 IRES_TILEDMEMORY_ProtocolArgs::accessDimension

Access dimension of requested memory.

See also
IRES_TILEDMEMORY_AccessDimension
XDAS_UInt32 IRES_TILEDMEMORY_ProtocolArgs::accessUnit

Access Unit for memory requested.

See also
IRES_TILEDMEMORY_AccessUnit
int IRES_TILEDMEMORY_ProtocolArgs::sizeDim0

size of 1st Dimension (width) in number of bytes

int IRES_TILEDMEMORY_ProtocolArgs::sizeDim1

size of 2nd Dimension (height) in number of bytes when 2D access type

int IRES_TILEDMEMORY_ProtocolArgs::alignment

alignment in bytes for the memory base address to be allocated


The documentation for this struct was generated from the following file:
Copyright 2015, Texas Instruments Incorporated