Framework Components Application Programming Interface (API)  fc-v02
Data Fields
IRES_TILEDMEMORY_Obj Struct Reference

IRES_TILEDMEMORY_Obj extends the generic IRES_Obj structure that is returned back to the algorithm requesting the resource. More...

#include <ires_tiledmemory.h>

Collaboration diagram for IRES_TILEDMEMORY_Obj:
Collaboration graph

Data Fields

IRES_Obj ires
 
XDAS_Voidinfo
 
XDAS_VoidmemoryBaseAddress
 
XDAS_UInt32 isTiledMemory
 
XDAS_UInt32 accessUnit
 
XDAS_VoidtilerBaseAddress
 
XDAS_VoidsystemSpaceBaseAddress
 

Detailed Description

IRES_TILEDMEMORY_Obj extends the generic IRES_Obj structure that is returned back to the algorithm requesting the resource.

Field Documentation

IRES_Obj IRES_TILEDMEMORY_Obj::ires
XDAS_Void* IRES_TILEDMEMORY_Obj::info

RSVD for future use

XDAS_Void* IRES_TILEDMEMORY_Obj::memoryBaseAddress

Process-specific virtual base address of Tiler memory allocated.

XDAS_UInt32 IRES_TILEDMEMORY_Obj::isTiledMemory

Boolean value that identifies if returned memory is of type TILED memory or not.

Valid values for this field are XDAS_TRUE and XDAS_FALSE.

If XDAS_TRUE, accessUnit will describe the kind of TILED memory allocated.

XDAS_UInt32 IRES_TILEDMEMORY_Obj::accessUnit

Describes the kind of memory actually allocated in the TILER space of type,

Remarks
Requestor MUST check the type of returned memory to ensure it is suitable for its purpose.
See also
IRES_TILEDMEMORY_AccessUnit
XDAS_Void* IRES_TILEDMEMORY_Obj::tilerBaseAddress

Base address of TILER on SOC

XDAS_Void* IRES_TILEDMEMORY_Obj::systemSpaceBaseAddress

Tiler space base address of memory allocated


The documentation for this struct was generated from the following file:
Copyright 2015, Texas Instruments Incorporated