Framework Components Application Programming Interface (API)  fc-v02
Data Fields
IRES_HDVICP_Obj Struct Reference

IRES_HDVICP_Obj extends the generic IRES_Obj structure that is returned back to the algorithm requesting the resource. More...

#include <ires_hdvicp.h>

Collaboration diagram for IRES_HDVICP_Obj:
Collaboration graph

Data Fields

IRES_Obj ires
 
Void * info
 
Int id
 
Void * registerBaseAddress
 
Void * memoryBaseAddress
 
unsigned int pscRegisterSpace
 

Detailed Description

IRES_HDVICP_Obj extends the generic IRES_Obj structure that is returned back to the algorithm requesting the resource.

Field Documentation

IRES_Obj IRES_HDVICP_Obj::ires
Void* IRES_HDVICP_Obj::info

RSVD for future use

Int IRES_HDVICP_Obj::id

ID of the HDVICP being , granted, could be IRES_HDVICP_ID_0 or IRES_HDVICP_ID_1

Void* IRES_HDVICP_Obj::registerBaseAddress

Base address of reg space

Void* IRES_HDVICP_Obj::memoryBaseAddress

Mem address of mem space

unsigned int IRES_HDVICP_Obj::pscRegisterSpace

Base address of the PSC and system module register space


The documentation for this struct was generated from the following file:
Copyright 2015, Texas Instruments Incorporated