Framework Components Application Programming Interface (API)  fc-v02
Data Fields
IRES_EDMA3CHAN_ProtocolArgs Struct Reference

EDMA3 Linked Transfer Protocol Arguments definition. More...

#include <ires_edma3Chan.h>

Collaboration diagram for IRES_EDMA3CHAN_ProtocolArgs:
Collaboration graph

Data Fields

int size
 
IRES_RequestMode mode
 
short numPaRams
 
short paRamIndex
 
short numTccs
 
short tccIndex
 
short qdmaChan
 
short edmaChan
 
short contiguousAllocation
 
short shadowPaRamsAllocation
 

Detailed Description

EDMA3 Linked Transfer Protocol Arguments definition.

Remarks
When requesting resources on a device on which DCHMAP feature does not exist, please follow these rules:
  1. Break up requests into LOGICAL channel requests and requests for PaRams.
  2. Logical Qdma/Edma channel => Q/E channel + PaRam + TCC
  3. Avoid requesting EDMA3 resources of specific number, for most transfers an "ANY" type request should be sufficient
  4. For linked transfers, request a Logical channel in one descriptor, and "N" contiguous Params in another descriptor
  5. If a logical channel request is combined with a request for multiple Params or Tccs, this might result in an inefficient allocation of resources, and in some cases, simplifying assumptions about the resource requests may be made by the allocator.

Field Documentation

int IRES_EDMA3CHAN_ProtocolArgs::size

Size of this structure.

IRES_RequestMode IRES_EDMA3CHAN_ProtocolArgs::mode

Resource request type.

See also
IRES_RequestMode
short IRES_EDMA3CHAN_ProtocolArgs::numPaRams

Number of params requested.

Remarks
Must be between 0 and IRES_EDMA3CHAN_MAXPARAMS - 1 inclusive.
short IRES_EDMA3CHAN_ProtocolArgs::paRamIndex

Describe type of paRams required.

Remarks
If numParams > 1 and requesting contiguous Params, this field indicates the start index of the PaRam block. Otherwise, set this field to IRES_EDMA3CHAN_PARAM_ANY.
short IRES_EDMA3CHAN_ProtocolArgs::numTccs

Number of Tcc(s) requested.

Remarks
Must be between 0 and IRES_EDMA3CHAN_MAXTCCS -1 inclusive.
short IRES_EDMA3CHAN_ProtocolArgs::tccIndex

The type of tccs requested.

Remarks
If numParams > 1 and requesting contiguous Params, this field indicates the start index of the Tcc block. Otherwise, set this field to IRES_EDMA3CHAN_TCC_ANY.
short IRES_EDMA3CHAN_ProtocolArgs::qdmaChan

QDMA channel required, if any.

Remarks
If a QDMA channel is not needed, set this field to IRES_EDMA3CHAN_CHAN_NONE.
short IRES_EDMA3CHAN_ProtocolArgs::edmaChan

Edma channel required if any.

Remarks
If a QDMA channel is not needed, set this field to IRES_EDMA3CHAN_CHAN_NONE.
If a single EDMA channel is requested with a single Tcc in one resource descriptor, then resource allocator will attempt to allocate EDMA Channel # N = Tcc # N, and will fail if that is unavailable.
short IRES_EDMA3CHAN_ProtocolArgs::contiguousAllocation

Flag indicating if contiguous allocation of PaRams and Tccs is required.

short IRES_EDMA3CHAN_ProtocolArgs::shadowPaRamsAllocation

Flag indicating if shadow PaRams need to be allocated.


The documentation for this struct was generated from the following file:
Copyright 2015, Texas Instruments Incorporated