Framework Components Application Programming Interface (API)  fc-v02
Data Fields
IRES_EDMA3CHAN_Properties Struct Reference

Static Resource Properties. More...

#include <ires_edma3Chan.h>

Collaboration diagram for IRES_EDMA3CHAN_Properties:
Collaboration graph

Data Fields

unsigned int numDmaChannels
 
unsigned int numQdmaChannels
 
unsigned int numTccs
 
unsigned int numPaRAMSets
 
unsigned int numEvtQueue
 
unsigned int numTcs
 
unsigned int numRegions
 
unsigned short dmaChPaRAMMapExists
 Channel mapping existence. More...
 
unsigned short memProtectionExists
 
IRES_EDMA3CHAN_EDMA3RegisterLayerglobalRegs
 

Detailed Description

Static Resource Properties.

Field Documentation

unsigned int IRES_EDMA3CHAN_Properties::numDmaChannels

Total number of DMA Channel supported by the EDMA3

unsigned int IRES_EDMA3CHAN_Properties::numQdmaChannels

Total number of QDMA Channels supported by the EDMA3 Controller.

unsigned int IRES_EDMA3CHAN_Properties::numTccs

Total number of Tccs supported by the EDMA3.

unsigned int IRES_EDMA3CHAN_Properties::numPaRAMSets

Total number of PaRAM Sets supported by the EDMA3.

unsigned int IRES_EDMA3CHAN_Properties::numEvtQueue

Total number of Event Queues in the EDMA3.

unsigned int IRES_EDMA3CHAN_Properties::numTcs

Total number of Transfer Controllers (TCs) in the EDMA3 Controller.

unsigned int IRES_EDMA3CHAN_Properties::numRegions

Number of Regions on the EDMA3 controller.

unsigned short IRES_EDMA3CHAN_Properties::dmaChPaRAMMapExists

Channel mapping existence.

A value of 0 (No channel mapping) implies that there is fixed association for a channel number to a parameter entry number or, in other words, PaRAM entry n corresponds to channel n.

unsigned short IRES_EDMA3CHAN_Properties::memProtectionExists

Existence of memory protection feature.

IRES_EDMA3CHAN_EDMA3RegisterLayer* IRES_EDMA3CHAN_Properties::globalRegs

Pointer to Global Register region of CC Registers.


The documentation for this struct was generated from the following file:
Copyright 2015, Texas Instruments Incorporated