Framework Components Application Programming Interface (API)  fc-v02
Data Fields
IRES_EDMA3CHAN_EDMA3DraeRegister Struct Reference

Defines the Region Enable register part of the EDMA3 CC Register Layer. More...

#include <ires_edma3Chan.h>

Collaboration diagram for IRES_EDMA3CHAN_EDMA3DraeRegister:
Collaboration graph

Data Fields

volatile unsigned int DRAE
 
volatile unsigned int DRAEH
 

Detailed Description

Defines the Region Enable register part of the EDMA3 CC Register Layer.

Field Documentation

volatile unsigned int IRES_EDMA3CHAN_EDMA3DraeRegister::DRAE
volatile unsigned int IRES_EDMA3CHAN_EDMA3DraeRegister::DRAEH

The documentation for this struct was generated from the following file:
Copyright 2015, Texas Instruments Incorporated