Data Fields

IRES_VICP2_Obj Struct Reference
[IRES VICP2 Protocol]

IRES_VICP2_Obj extends the generic IRES_Obj structure that is returned back to the algorithm requesting the resource. More...

#include <ires_vicp2.h>

Collaboration diagram for IRES_VICP2_Obj:
Collaboration graph
[legend]

Data Fields

IRES_Obj ires
short assignedIMX0
short assignedIMX1
short assignedMJCP
short assignedNSF
unsigned int assignedIMCOPBuffers [16]
short numMemBufs
unsigned int assignedMemAddrs [16]
unsigned int assignedMemSizes [16]
unsigned int configBaseAddress
unsigned int dmaViewConfigBaseAddr
unsigned int pscRegisterSpace

Detailed Description

IRES_VICP2_Obj extends the generic IRES_Obj structure that is returned back to the algorithm requesting the resource.


Field Documentation

Value of 1 to indicate resource was granted, 0 otherwise

Addresses of Named buffers granted, index array with IMCOP_BUFFER_<>

Number of individual memory buffers assigned

Addresses of buffers assigned, only the first numBufs will hold valid addresses

Base address of config space

Base address of DMA view of VICP buffers

Base address of the PSC and system module register space


The documentation for this struct was generated from the following file:
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2013, Texas Instruments Incorporated