Data Fields

IRES_TILEDMEMORY_ProtocolArgs Struct Reference
[IRES TILEDMEMORY Protocol (Beta)]

TILEDMEMORY Protocol Arguments definition. More...

#include <ires_tiledmemory.h>

Collaboration diagram for IRES_TILEDMEMORY_ProtocolArgs:
Collaboration graph
[legend]

Data Fields

IRES_ProtocolArgs base
XDAS_UInt32 accessDimension
XDAS_UInt32 accessUnit
int sizeDim0
int sizeDim1
int alignment

Detailed Description

TILEDMEMORY Protocol Arguments definition.


Field Documentation

Access dimension of requested memory.

See also:
IRES_TILEDMEMORY_AccessDimension

Access Unit for memory requested.

See also:
IRES_TILEDMEMORY_AccessUnit

size of 1st Dimension (width) in number of bytes

size of 2nd Dimension (height) in number of bytes when 2D access type

alignment in bytes for the memory base address to be allocated


The documentation for this struct was generated from the following file:
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2013, Texas Instruments Incorporated