Data Fields

IRES_EDMA3CHAN_ProtocolArgs Struct Reference
[IRES EDMA3 Protocol]

EDMA3 Linked Transfer Protocol Arguments definition. More...

#include <ires_edma3Chan.h>

Data Fields

int size
IRES_RequestMode mode
short numPaRams
short paRamIndex
short numTccs
short tccIndex
short qdmaChan
short edmaChan
short contiguousAllocation
short shadowPaRamsAllocation

Detailed Description

EDMA3 Linked Transfer Protocol Arguments definition.

Remarks:
When requesting resources on a device on which DCHMAP feature does not exist, please follow these rules:
  1. Break up requests into LOGICAL channel requests and requests for PaRams.
  2. Logical Qdma/Edma channel => Q/E channel + PaRam + TCC
  3. Avoid requesting EDMA3 resources of specific number, for most transfers an "ANY" type request should be sufficient
  4. For linked transfers, request a Logical channel in one descriptor, and "N" contiguous Params in another descriptor
  5. If a logical channel request is combined with a request for multiple Params or Tccs, this might result in an inefficient allocation of resources, and in some cases, simplifying assumptions about the resource requests may be made by the allocator.

Field Documentation

Size of this structure.

Resource request type.

See also:
IRES_RequestMode

Number of params requested.

Remarks:
Must be between 0 and IRES_EDMA3CHAN_MAXPARAMS - 1 inclusive.

Describe type of paRams required.

Remarks:
If numParams > 1 and requesting contiguous Params, this field indicates the start index of the PaRam block. Otherwise, set this field to IRES_EDMA3CHAN_PARAM_ANY.

Number of Tcc(s) requested.

Remarks:
Must be between 0 and IRES_EDMA3CHAN_MAXTCCS -1 inclusive.

The type of tccs requested.

Remarks:
If numParams > 1 and requesting contiguous Params, this field indicates the start index of the Tcc block. Otherwise, set this field to IRES_EDMA3CHAN_TCC_ANY.

QDMA channel required, if any.

Remarks:
If a QDMA channel is not needed, set this field to IRES_EDMA3CHAN_CHAN_NONE.

Edma channel required if any.

Remarks:
If a QDMA channel is not needed, set this field to IRES_EDMA3CHAN_CHAN_NONE.
If a single EDMA channel is requested with a single Tcc in one resource descriptor, then resource allocator will attempt to allocate EDMA Channel # N = Tcc # N, and will fail if that is unavailable.

Flag indicating if contiguous allocation of PaRams and Tccs is required.

Flag indicating if shadow PaRams need to be allocated.


The documentation for this struct was generated from the following file:
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2013, Texas Instruments Incorporated