Functions | Data Structures | Typedefs | Variables

IRESMAN EDMA3 -

Functions

String IRESMAN_EDMA3CHAN_getProtocolName ()
 Function to return the name of the protocol.
IRES_ProtocolRevisionIRESMAN_EDMA3CHAN_getProtocolRevision ()
 Function to return the revision of the protocol.
IRES_Status IRESMAN_EDMA3CHAN_init (IRESMAN_Params *initArgs)
 Function to initialize the device specific resource manager implementation.
IRES_Status IRESMAN_EDMA3CHAN_exit ()
 Function called when RESMAN is no longer needed. Use it to free memory allocated etc.
IRES_Handle IRESMAN_EDMA3CHAN_getHandles (IALG_Handle algHandle, IRES_ResourceDescriptor *resDesc, Int scratchGroupId, IRES_Status *status)
 Function that returns the IRES_Handle to the resource requested using the IRES_ResourceProtocolArgs.
IRES_Status IRESMAN_EDMA3CHAN_freeHandle (IALG_Handle algHandle, IRES_Handle algResourceHandle, IRES_ResourceDescriptor *resDesc, Int scratchGroupId)
 Frees handles back to the resource pool.

Data Structures

struct  IRESMAN_Edma3ChanParams
 Configuration parameters for Edma3Chan resman implementation. More...

Typedefs

typedef struct
IRESMAN_Edma3ChanParams 
IRESMAN_Edma3ChanParams
 Configuration parameters for Edma3Chan resman implementation.

Variables

__FAR__ IRESMAN_PersistentAllocFxn _RMAN_allocPersistent
 Memory allocation functions for all of RMANs and other IRES rotocol's memory requirements.
__FAR__ IRESMAN_PersistentFreeFxn _RMAN_freePersistent
 Memory free functions for all of RMANs and other IRES protocol's memory requirements.
IRESMAN_Fxns IRESMAN_EDMA3CHAN
 IRES RESMAN implementation for EDMA3 Linked transfers.

Detailed Description

EDMA3 specific Resource Manager and corresponding IRES Protocol Implementation


Function Documentation

String IRESMAN_EDMA3CHAN_getProtocolName (  )

Function to return the name of the protocol.

Return values:
Stringname identifying the protocol
IRES_ProtocolRevision* IRESMAN_EDMA3CHAN_getProtocolRevision (  )

Function to return the revision of the protocol.

Return values:
Revisionidentifying the protocol
IRES_Status IRESMAN_EDMA3CHAN_init ( IRESMAN_Params initArgs )

Function to initialize the device specific resource manager implementation.

Parameters:
[in]initArgsInitialization arguments that may be interpreted by the device specific implementation
Return values:
IRES_StatusIRES_OK Success IRES_EEXISTS Already initialized IRES_EFAIL Error
IRES_Status IRESMAN_EDMA3CHAN_exit (  )

Function called when RESMAN is no longer needed. Use it to free memory allocated etc.

Return values:
IRES_StatusIRES_OK Success IRES_ENOINIT Not initialized IRES_EFAIL Error
IRES_Handle IRESMAN_EDMA3CHAN_getHandles ( IALG_Handle  algHandle,
IRES_ResourceDescriptor resDesc,
Int  scratchGroupId,
IRES_Status status 
)

Function that returns the IRES_Handle to the resource requested using the IRES_ResourceProtocolArgs.

Parameters:
[in]algHandleHandle of the algorithm that requests the resources
[in]resDescArguments to be interpreted by the IRES_Manager implementation to determine which actual physical resources to obtain
[in]scratchGroupIdGroup Id required if scratch resources are requested, -1 otherwise
[out]statusStatus of this call
Return values:
IRES_HandleValid handle corresponding to the resource requested on success, or NULL on error.
IRES_Status IRESMAN_EDMA3CHAN_freeHandle ( IALG_Handle  algHandle,
IRES_Handle  algResourceHandle,
IRES_ResourceDescriptor resDesc,
Int  scratchGroupId 
)

Frees handles back to the resource pool.

Parameters:
[in]algHandleHandle of the algorithm that frees the resources
[in]algResourceHandleHandle that is to be released
[in]resDescArguments that help determine which resources to free
[in]scratchGroupIdGroup Id required if scratch resources are requested, -1 otherwise
Return values:
IRES_StatusIRES_OK Success IRES_EFAIL Failure

Typedef Documentation

Configuration parameters for Edma3Chan resman implementation.


Variable Documentation

Memory allocation functions for all of RMANs and other IRES rotocol's memory requirements.

Memory free functions for all of RMANs and other IRES protocol's memory requirements.

IRES RESMAN implementation for EDMA3 Linked transfers.

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2013, Texas Instruments Incorporated