Data Fields

IRES_VICP_Obj Struct Reference
[IRES VICP Protocol]

IRES_VICP_Obj extends the generic IRES_Obj structure that is returned back to the algorithm requesting the resource. More...

#include <ires_vicp.h>

Collaboration diagram for IRES_VICP_Obj:
Collaboration graph
[legend]

Data Fields

IRES_Obj ires
short assignedIMX
short assignedVLCD
short assignedSEQ

Detailed Description

IRES_VICP_Obj extends the generic IRES_Obj structure that is returned back to the algorithm requesting the resource.


Field Documentation


The documentation for this struct was generated from the following file:
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2012, Texas Instruments Incorporated