Data Fields

IRES_Properties Struct Reference

Abstract Resource Properties structure/pointer definition. Actual resource protocol will supply the concrete property definitions. The list of attributes for the actual resource will expose the relevant features that needs to be known to a client to use the resource, such as: resource register base addresses and offsets, critical register and memory region addresses, ... More...

#include <ires_common.h>

Data Fields

Int32 size

Detailed Description

Abstract Resource Properties structure/pointer definition. Actual resource protocol will supply the concrete property definitions. The list of attributes for the actual resource will expose the relevant features that needs to be known to a client to use the resource, such as: resource register base addresses and offsets, critical register and memory region addresses, ...


Field Documentation

Size of this structure.


The documentation for this struct was generated from the following file:
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2012, Texas Instruments Incorporated