Data Fields

RcmServer_Params Struct Reference
[RcmServer]

RcmServer Instance create parameters. More...

#include <RcmServer.h>

Collaboration diagram for RcmServer_Params:
Collaboration graph
[legend]

Data Fields

Thread_Priority priority
 Server thread priority.
Int osPriority
 Server thread priority (OS-specific).
SizeT stackSize
 The stack size in bytes of the server thread.
String stackSeg
 The server thread stack placement.
RcmServer_ThreadPoolDesc defaultPool
 The default thread pool used for anonymous messages.
RcmServer_ThreadPoolDescAry workerPools
 Array of thread pool descriptors.
RcmServer_FxnDescAry fxns
 Array of function names to install into the server.

Detailed Description

RcmServer Instance create parameters.


Field Documentation

Thread_Priority RcmServer_Params::priority

Server thread priority.

This value is Operating System independent. It determines the execution priority of the server thread. The server thread reads the incoming message and then either executes the message function (in-band execution) or dispatches the message to a thread pool (out-of-band execution). The server thread then wait on the next message.

Server thread priority (OS-specific).

This value is Operating System specific. It determines the execution priority of the server thread. If this attribute is set, it takes precedence over the priority attribute below. The server thread reads the incoming message and then either executes the message function (in-band execution) or dispatches the message to a thread pool (out-of-band execution). The server thread then wait on the next message.

The stack size in bytes of the server thread.

The server thread stack placement.

The default thread pool used for anonymous messages.

Array of thread pool descriptors.

The worker pools declared with this instance parameter are statically bound to the server, they persist for the life of the server. They cannot be removed with a call to RcmServer_deletePool(). However, worker threads may be created or deleted at runtime.

Array of function names to install into the server.

The functions declared with this instance parameter are statically bound to the server, they persist for the life of the server. They cannot be removed with a call to RcmServer_removeSymbol().

To specify a function address, use the & character in the string as in the following example.

  RcmServer_FxnDesc serverFxnAry[] = {
      { "LED_on",         LED_on  },
      { "LED_off",        LED_off }
  };

  #define serverFxnAryLen (sizeof serverFxnAry / sizeof serverFxnAry[0])

  RcmServer_FxnDescAry Server_fxnTab = {
      serverFxnAryLen,
      serverFxnAry
  };

  RcmServer_Params rcmServerP;
  RcmServer_Params_init(&rcmServerP);
  rcmServerP.fxns.length = Server_fxnTab.length;
  rcmServerP.fxns.elem = Server_fxnTab.elem;

  RcmServer_Handle rcmServerH;
  rval = RcmServer_create("ServerA", &rcmServerP, &(rcmServerH));

The documentation for this struct was generated from the following file:
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2011, Texas Instruments Incorporated